Messaging
Connect APIs and handlers for sending and receiving messages. More...
         Macros | 
       |
| #define | EMBER_MAX_UNSECURED_APPLICATION_PAYLOAD_LENGTH 111 | 
| #define | EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH 102 | 
| #define | EMBER_MAX_ENDPOINT 0xF | 
| 
         The maximum allowed endpoint value.
         
          More...
         
          | 
       |
         Functions | 
       |
| EmberStatus | emberMessageSend ( EmberNodeId destination, uint8_t endpoint, uint8_t messageTag, EmberMessageLength messageLength, uint8_t *message, EmberMessageOptions options) | 
| 
         Send a message to the passed destination short ID.
         
          More...
         
          | 
       |
| EmberStatus | emberMacMessageSend ( EmberMacFrame *macFrame, uint8_t messageTag, EmberMessageLength messageLength, uint8_t *message, EmberMessageOptions options) | 
| 
         Create a MAC level frame and sends it to the passed destination. This API can only be used for nodes of
         
          EMBER_MAC_MODE_DEVICE
         
         node type or
         
          EMBER_MAC_MODE_SLEEPY_DEVICE
         
         node type.
         
          More...
         
          | 
       |
| EmberStatus | emberPollForData (void) | 
| 
         Send a data request command to the parent node. Note that if the node short ID is a value of
         
          EMBER_USE_LONG_ADDRESS
         
         , the node shall use its long ID as source address.
         
          More...
         
          | 
       |
| EmberStatus | emberSetPollDestinationAddress ( EmberMacAddress *destination) | 
| 
         Set data polls destination address for nodes of
         
          EMBER_MAC_MODE_DEVICE
         
         node type or
         
          EMBER_MAC_MODE_SLEEPY_DEVICE
         
         node type.
         
          More...
         
          | 
       |
| uint8_t | emberGetMaximumPayloadLength ( EmberMacAddressMode srcAddressMode, EmberMacAddressMode dstAddressMode, bool interpan, bool secured) | 
| 
         Return the maximum payload according to the passed source and destination addressing modes, the passed secured flag, and the current configuration of the node.
         
          More...
         
          | 
       |
         Handlers | 
       |
| 
          The Application Framework implements all handlers, directly calling their associated callbacks. By default, Connect projects declare such callbacks as stubs in flex-callbacks-stubs.c. Hence, to use an enabled Connect feature, applications should replace the stub with their own implementation of the associated callback (typically in flex-callbacks.c). See UG235.04 for more info.  | 
       |
| void | emberMessageSentHandler ( EmberStatus status, EmberOutgoingMessage *message) | 
| 
         This handler is invoked when the stack has completed sending a message.
         
          More...
         
          | 
       |
| void | emberMacMessageSentHandler ( EmberStatus status, EmberOutgoingMacMessage *message) | 
| 
         This handler is invoked when a node of
         
          EMBER_MAC_MODE_DEVICE
         
         type or
         
          EMBER_MAC_MODE_SLEEPY_DEVICE
         
         type has completed sending a MAC frame.
         
          More...
         
          | 
       |
| void | emberIncomingMessageHandler ( EmberIncomingMessage *message) | 
| 
         This handler is invoked when a packet has been received from a node type other than
         
          EMBER_MAC_MODE_DEVICE
         
         or
         
          EMBER_MAC_MODE_SLEEPY_DEVICE
         
         .
         
          More...
         
          | 
       |
| void | emberIncomingMacMessageHandler ( EmberIncomingMacMessage *message) | 
| 
         This handler is invoked when a node of
         
          EMBER_MAC_MODE_DEVICE
         
         type or
         
          EMBER_MAC_MODE_SLEEPY_DEVICE
         
         has received a MAC frame.
         
          More...
         
          | 
       |
Detailed Description
Connect APIs and handlers for sending and receiving messages.
t_stack
Note that MAC mode and Extended star/direct mode use different APIs for messaging.
      See
      
       message.h
      
      for source code.
     
Macro Definition Documentation
◆ EMBER_MAX_ENDPOINT
| #define EMBER_MAX_ENDPOINT 0xF | 
The maximum allowed endpoint value.
        Definition at line
        
         58
        
        of file
        
         message.h
        
        .
       
◆ EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH
| #define EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH 102 | 
- Deprecated:
 - The maximum length in bytes of the application payload for a secured message. This define has been deprecated, you should use the emberGetMaximumPayloadLength API instead.
 
        Definition at line
        
         54
        
        of file
        
         message.h
        
        .
       
◆ EMBER_MAX_UNSECURED_APPLICATION_PAYLOAD_LENGTH
| #define EMBER_MAX_UNSECURED_APPLICATION_PAYLOAD_LENGTH 111 | 
- Deprecated:
 - The maximum length in bytes of the application payload for an unsecured message. This define has been deprecated, you should use the emberGetMaximumPayloadLength API instead.
 
        Definition at line
        
         48
        
        of file
        
         message.h
        
        .
       
Function Documentation
◆ emberGetMaximumPayloadLength()
| uint8_t emberGetMaximumPayloadLength | ( | EmberMacAddressMode | 
           
            srcAddressMode,
           
           | 
         
| EmberMacAddressMode | 
           
            dstAddressMode,
           
           | 
         ||
| bool | 
           
            interpan,
           
           | 
         ||
| bool | 
           
            secured
           
           | 
         ||
| ) | 
Return the maximum payload according to the passed source and destination addressing modes, the passed secured flag, and the current configuration of the node.
- Parameters
 - 
         
[in] srcAddressModeAn EmberMacAddressMode value indicating the mode of the source address. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . [in] dstAddressModeAn EmberMacAddressMode value indicating the mode of the destination address. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . [in] interpanIndicates whether the frame is an interpan frame or not. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE . [in] securedIndicates whether the frame should be secured or not.  
- Returns
 - The maximum payload length in bytes achievable according to the passed parameters or 0xFF if the node is currently active on a network or any of the passed parameters are invalid.
 
◆ emberIncomingMacMessageHandler()
| void emberIncomingMacMessageHandler | ( | EmberIncomingMacMessage * | 
           
            message
           
           | 
          ) | 
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE has received a MAC frame.
- Parameters
 - 
         
[in] messageAn EmberIncomingMacMessage describing the incoming packet.  
- Warning
 - Implement associated callback emberAfIncomingMacMessageCallback() to use. See Handlers for additional information.
 
◆ emberIncomingMessageHandler()
| void emberIncomingMessageHandler | ( | EmberIncomingMessage * | 
           
            message
           
           | 
          ) | 
This handler is invoked when a packet has been received from a node type other than EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE .
- Parameters
 - 
         
[in] messageAn EmberIncomingMessage describing the incoming packet.  
- Warning
 - Implement associated callback emberAfIncomingMessageCallback() to use. See Handlers for additional information.
 
◆ emberMacMessageSend()
| EmberStatus emberMacMessageSend | ( | EmberMacFrame * | 
           
            macFrame,
           
           | 
         
| uint8_t | 
           
            messageTag,
           
           | 
         ||
| EmberMessageLength | 
           
            messageLength,
           
           | 
         ||
| uint8_t * | 
           
            message,
           
           | 
         ||
| EmberMessageOptions | 
           
            options
           
           | 
         ||
| ) | 
Create a MAC level frame and sends it to the passed destination. This API can only be used for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
- Parameters
 - 
         
[in] macFrameA pointer to an EmberMacFrame struct that specifies the source and destination addresses and the source and destination PAN IDs for the message to be sent. Note that if the source/destination PAN ID is not specified, it defaults to the node's PAN ID. Also, the destination address mode must be either EMBER_MAC_ADDRESS_MODE_SHORT or EMBER_MAC_ADDRESS_MODE_LONG . [in] messageTagA value chosen by the application. This value will be passed in the corresponding emberMacMessageSentHandler() call. [in] messageLengthThe size in bytes of the message payload. The application can use the emberGetMaximumPayloadLength() API to determine the maximum allowable payload, given a permutation of source and destination addressing and other TX options. [in] messageA pointer to an array of bytes containing the message payload. [in] optionsSpecifies the EmberMessageOptions for the outgoing message.  
- Returns
 - 
         an
         
EmberStatusvalue of:- EMBER_SUCCESS if the message was accepted by the stack. If a success status is returned, the emberMacMessageSentHandler() callback will be invoked by the stack to indicate whether the message was successfully delivered or the reason for failure.
 - EMBER_INVALID_CALL if the node is of a node type other than EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE .
 - EMBER_BAD_ARGUMENT if the packet length is 0, the passed TX options indicates some feature that is not supported or the destination address mode is set to EMBER_MAC_ADDRESS_MODE_NONE .
 - EMBER_MESSAGE_TOO_LONG if the message does not fit in a single frame.
 - EMBER_PHY_TX_BUSY if the message cannot be sent since the node does not support MAC queuing and the radio is currently busy.
 - EMBER_MAC_TRANSMIT_QUEUE_FULL if the outgoing MAC queue is currently full.
 - EMBER_NO_BUFFERS if the stack could not allocate enough RAM to store the submitted message.
 - EMBER_MAC_SECURITY_NOT_SUPPORTED if the message was requested to be sent out with a security but no security plugin was enabled.
 - EMBER_MAC_BUSY if the message was not accepted because the MAC is currently performing a critical operation.
 
 
◆ emberMacMessageSentHandler()
| void emberMacMessageSentHandler | ( | EmberStatus | 
           
            status,
           
           | 
         
| EmberOutgoingMacMessage * | 
           
            message
           
           | 
         ||
| ) | 
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE type has completed sending a MAC frame.
- Parameters
 - 
         
[in] statusAn EmberStatusvalue of:- EMBER_SUCCESS if an ACK was received from the destination or no ACK was requested.
 - EMBER_MAC_NO_ACK_RECEIVED if an ACK was requested and no ACK was received.
 - EMBER_MAC_INDIRECT_TIMEOUT if the MAC frame was sent out via the indirect queue and the it timed-out before a data request was received.
 - EMBER_MAC_INDIRECT_MESSAGE_PURGED if the MAC frame was sent out via the indirect queue and it was removed prior to a data request being received. See emberPurgeIndirectMessages() .
 - EMBER_MAC_SECURITY_FAILED if the stack failed to encrypt the message. This typically occurs when a node is sending a message using short source addressing with an address other than the node's short address and the no mapping to a corresponding address was found in the short-to-long address mapping table. The application should use the emberMacAddShortToLongAddressMapping to populate such table.
 - EMBER_PHY_TX_CCA_FAIL if the node failed all the clear channel assessment attempts.
 - EMBER_PHY_TX_INCOMPLETE if the transmission was not completed correctly.
 
[in] messageAn EmberOutgoingMacMessage describing the outgoing MAC frame.  
- Warning
 - Implement associated callback emberAfMacMessageSentCallback() to use. See Handlers for additional information.
 
◆ emberMessageSend()
| EmberStatus emberMessageSend | ( | EmberNodeId | 
           
            destination,
           
           | 
         
| uint8_t | 
           
            endpoint,
           
           | 
         ||
| uint8_t | 
           
            messageTag,
           
           | 
         ||
| EmberMessageLength | 
           
            messageLength,
           
           | 
         ||
| uint8_t * | 
           
            message,
           
           | 
         ||
| EmberMessageOptions | 
           
            options
           
           | 
         ||
| ) | 
Send a message to the passed destination short ID.
- Parameters
 - 
         
[in] destinationThe destination node short ID. [in] endpointThe destination endpoint of the outgoing message. This value can't exceed EMBER_MAX_ENDPOINT . [in] messageTagA value chosen by the application. This value will be passed in the corresponding emberMessageSentHandler() call. [in] messageLengthThe size of the message payload in bytes. Use the emberGetMaximumPayloadLength() API to determine the maximum message length allowed. [in] messageA pointer to an array of bytes containing the message payload. [in] optionsSpecifies the EmberMessageOptions for the outgoing message.  
- Returns
 - 
         an
         
EmberStatusvalue of:- EMBER_SUCCESS if the message was accepted by the stack. If a success status is returned, the emberMessageSentHandler() callback is invoked by the stack to indicate whether the message was successfully delivered or the reason for failure.
 - EMBER_INVALID_CALL if the node is not joined to a network or the node is of EMBER_MAC_MODE_DEVICE device type or EMBER_MAC_MODE_SLEEPY_DEVICE (use emberMacMessageSend instead).
 - EMBER_BAD_ARGUMENT if the packet length is 0, the passed TX options indicates some feature that is not supported, the passed endpoint exceeds EMBER_MAX_ENDPOINT
 - EMBER_MESSAGE_TOO_LONG if the message does not fit in a single frame.
 - EMBER_PHY_TX_BUSY if the message cannot be sent since the node does not support MAC queuing and the radio is currently busy.
 - EMBER_MAC_TRANSMIT_QUEUE_FULL if the outgoing MAC queue is currently full.
 - EMBER_NO_BUFFERS if the stack could not allocate enough RAM to store the submitted message.
 - EMBER_MAC_UNKNOWN_DESTINATION if the node is part of a star network and the destination node does not appear in the node's routing table.
 - EMBER_MAC_SECURITY_NOT_SUPPORTED if the message was requested to be sent out secured and either the local node does not support security or the destination node is known to not support security.
 - EMBER_MAC_BUSY if the message was not accepted because the MAC is currently performing some critical operation.
 
 
◆ emberMessageSentHandler()
| void emberMessageSentHandler | ( | EmberStatus | 
           
            status,
           
           | 
         
| EmberOutgoingMessage * | 
           
            message
           
           | 
         ||
| ) | 
This handler is invoked when the stack has completed sending a message.
- Parameters
 - 
         
[in] statusAn EmberStatusvalue of:- EMBER_SUCCESS if an ACK was received from the destination or no ACK was requested.
 - EMBER_MAC_NO_ACK_RECEIVED if an ACK was requested and no ACK was received.
 - EMBER_MAC_INDIRECT_TIMEOUT if the destination is a sleepy node and the packet timed-out before the sleepy node sent a data request.
 - EMBER_MAC_INDIRECT_MESSAGE_PURGED if the destination is a sleepy node and it was removed from the child table while the packet was stored in the indirect queue.
 - EMBER_PHY_TX_CCA_FAIL if the node failed all the clear channel assessment attempts.
 - EMBER_PHY_TX_INCOMPLETE if the transmission was not completed correctly.
 
[in] messageAn EmberOutgoingMessage describing the outgoing packet.  
- Warning
 - Implement associated callback emberAfMessageSentCallback() to use. See Handlers for additional information.
 
◆ emberPollForData()
| EmberStatus emberPollForData | ( | void | 
           
           
           | 
          ) | 
Send a data request command to the parent node. Note that if the node short ID is a value of EMBER_USE_LONG_ADDRESS , the node shall use its long ID as source address.
- Returns
 - 
         and
         
EmberStatusvalue of:- EMBER_SUCCESS if the data poll was accepted by the MAC layer.
 - EMBER_INVALID_CALL if the node is not joined to a network, the node is not an end device, an EMBER_MAC_MODE_DEVICE or an EMBER_MAC_MODE_SLEEPY_DEVICE , or the node is of EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE node type, is not joined to a coordinator and the poll destination was not correctly set via the emberSetPollDestinationAddress() API.
 - EMBER_MAC_BUSY if the MAC is currently performing a critical operation.
 
 
◆ emberSetPollDestinationAddress()
| EmberStatus emberSetPollDestinationAddress | ( | EmberMacAddress * | 
           
            destination
           
           | 
          ) | 
Set data polls destination address for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
- Returns
 - 
         and
         
EmberStatusvalue of EMBER_SUCCESS if the data poll destination was correctly set, or anotherEmberStatusvalue indicating the reason of failure.