EmberEventData_S Struct Reference
Complete events with a control and a handler procedure. More...
#include <
ember-types.h
>
Data Fields | |
EmberEventControl * | control |
void(* | handler )(void) |
Complete events with a control and a handler procedure.
An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.
Definition at line 597
of file ember-types.h
.
Field Documentation
◆ control
EmberEventControl* EmberEventData_S::control |
The control structure for the event.
Definition at line 599
of file ember-types.h
.
◆ handler
void(* EmberEventData_S::handler) (void) |
The procedure to call when the event fires.
Definition at line 601
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h