/***************************************************************************/
#ifndef RADIO_STREAM_H
#define RADIO_STREAM_H
EmberStatus emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel);
EmberStatus emberStopTxStream(void);
#endif
Functions#
emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel)
Start a continuous TX stream to test RF.
emberStopTxStream(void)
Stop an RF stream in progress.
Function Documentation#
emberStartTxStream#
EmberStatus emberStartTxStream (EmberTxStreamParameters parameters, uint16_t channel)
Start a continuous TX stream to test RF.
Parameters
[in] | parameters | Stream mode. See EmberTxStreamParameters. |
[in] | channel | RF channel. |
Returns
EMBER_INVALID_CALL if the stack can not process the request EMBER_BAD_ARGUMENT if the parameters are wrong EMBER_SUCCESS if the stream can be started
Definition at line
50
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/radio-stream.h
emberStopTxStream#
EmberStatus emberStopTxStream (void )
Stop an RF stream in progress.
Parameters
N/A |
Returns
EMBER_INVALID_CALL if no stream is in progress EMBER_SUCCESS otherwise
Definition at line
58
of file /mnt/raid/workspaces/ws.SZ9MaSA5u/overlay/gsdk/protocol/flex/stack/include/radio-stream.h