Hold network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit and the Radio Configurator Guide (AN971).
Public Attribute Documentation#
panId#
uint16_t EmberNetworkParameters::panId
The network's PAN identifier.
Definition at line
187
of file /mnt/raid/workspaces/ws.Q8qnkBLX2/overlay/gsdk/protocol/flex/stack/include/ember-types.h
radioTxPower#
int16_t EmberNetworkParameters::radioTxPower
The transmit power setting, in deci-dBm.
Definition at line
189
of file /mnt/raid/workspaces/ws.Q8qnkBLX2/overlay/gsdk/protocol/flex/stack/include/ember-types.h
radioChannel#
uint16_t EmberNetworkParameters::radioChannel
The radio channel. Be sure to specify a channel supported by the radio.
Definition at line
191
of file /mnt/raid/workspaces/ws.Q8qnkBLX2/overlay/gsdk/protocol/flex/stack/include/ember-types.h