Radio Stream#

Radio stream API.

License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

Connect API managing radio stream for RF testing purpose

See radio-stream.h for source code.

Functions#

emberStartTxStream(EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Stop an RF stream in progress.

Function Documentation#

emberStartTxStream#

EmberStatus emberStartTxStream (EmberTxStreamParameters parameters, uint16_t channel)

Start a continuous TX stream to test RF.

Parameters
TypeDirectionArgument NameDescription
EmberTxStreamParameters[in]parameters

Stream mode. See EmberTxStreamParameters.

uint16_t[in]channel

RF channel.

Returns

  • EMBER_INVALID_CALL if the stack can not process the request EMBER_BAD_ARGUMENT if the parameters are wrong EMBER_SUCCESS if the stream can be started


Definition at line 50 of file /mnt/raid/workspaces/ws.GB1qsZ2Je/overlay/gsdk/protocol/flex/stack/include/radio-stream.h

emberStopTxStream#

EmberStatus emberStopTxStream (void )

Stop an RF stream in progress.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • EMBER_INVALID_CALL if no stream is in progress EMBER_SUCCESS otherwise


Definition at line 58 of file /mnt/raid/workspaces/ws.GB1qsZ2Je/overlay/gsdk/protocol/flex/stack/include/radio-stream.h