License#
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
This notice may not be removed or altered from any source distribution.
/***************************************************************************/
#ifndef __MESSAGE_H__
#define __MESSAGE_H__
#define EMBER_MAX_UNSECURED_APPLICATION_PAYLOAD_LENGTH 111
#define EMBER_MAX_SECURED_APPLICATION_PAYLOAD_LENGTH 102
#define EMBER_MAX_ENDPOINT 0xF
void emberMessageSentHandler(EmberStatus status, EmberOutgoingMessage *message);
void emberMacMessageSentHandler(EmberStatus status,
EmberOutgoingMacMessage *message);
void emberIncomingMessageHandler(EmberIncomingMessage *message);
void emberIncomingMacMessageHandler(EmberIncomingMacMessage *message);
EmberStatus emberMessageSend(EmberNodeId destination,
uint8_t endpoint,
uint8_t messageTag,
EmberMessageLength messageLength,
uint8_t *message,
EmberMessageOptions options);
EmberStatus emberMacMessageSend(EmberMacFrame *macFrame,
uint8_t messageTag,
EmberMessageLength messageLength,
uint8_t *message,
EmberMessageOptions options);
EmberStatus emberPollForData(void);
EmberStatus emberSetPollDestinationAddress(EmberMacAddress *destination);
EmberStatus emberPurgeIndirectMessages(void);
EmberStatus emberSetIndirectQueueTimeout(uint32_t timeoutMs);
uint16_t emberGetMaximumPayloadLength(EmberMacAddressMode srcAddressMode,
EmberMacAddressMode dstAddressMode,
bool interpan,
bool secured);
bool emberUsingLongMessages(void);
EmberStatus emberNcpSetLongMessagesUse(bool useLongMessages);
#endif //__MESSAGE_H__
Handlers#
The Application Framework implements all handlers, directly calling their associated callbacks. By default, Connect projects declare such callbacks as stubs in flex-callbacks-stubs.c. Hence, to use an enabled Connect feature, applications should replace the stub with their own implementation of the associated callback (typically in flex-callbacks.c). See UG235.04 for more info.
This handler is invoked when the stack has completed sending a message.
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE type has completed sending a MAC frame.
This handler is invoked when a packet has been received from a node type other than EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE.
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE has received a MAC frame.
Send a message to the passed destination short ID.
Create a MAC level frame and sends it to the passed destination. This API can only be used for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
Send a data request command to the parent node. Note that if the node short ID is a value of EMBER_USE_LONG_ADDRESS, the node shall use its long ID as source address.
Set data polls destination address for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
Purge all indirect transmissions from the indirect message queue.
Set indirect queue timeout value. The indirect queue timeout is set by default to EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS.
Return the maximum payload according to the passed source and destination addressing modes, the passed secured flag, and the current configuration of the node.
Indicates if the stack is currently using long messages or not.
Set the current message length that the stack uses.
Macros#
DeprecatedThe maximum length in bytes of the application payload for an unsecured message. This define has been deprecated, you should use the emberGetMaximumPayloadLength API instead.
DeprecatedThe maximum length in bytes of the application payload for a secured message. This define has been deprecated, you should use the emberGetMaximumPayloadLength API instead.
The maximum allowed endpoint value.
Handlers Documentation#
emberMessageSentHandler#
void emberMessageSentHandler (EmberStatus status, EmberOutgoingMessage * message)
This handler is invoked when the stack has completed sending a message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberStatus | [in] | status | An EmberStatus value of:
|
| EmberOutgoingMessage * | [in] | message | An EmberOutgoingMessage describing the outgoing packet. |
Warnings
Implement associated callback emberAfMessageSentCallback() to use. See Handlers for additional information.
emberMacMessageSentHandler#
void emberMacMessageSentHandler (EmberStatus status, EmberOutgoingMacMessage * message)
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE type has completed sending a MAC frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberStatus | [in] | status | An EmberStatus value of:
|
| EmberOutgoingMacMessage * | [in] | message | An EmberOutgoingMacMessage describing the outgoing MAC frame. |
Warnings
Implement associated callback emberAfMacMessageSentCallback() to use. See Handlers for additional information.
emberIncomingMessageHandler#
void emberIncomingMessageHandler (EmberIncomingMessage * message)
This handler is invoked when a packet has been received from a node type other than EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberIncomingMessage * | [in] | message | An EmberIncomingMessage describing the incoming packet. |
Warnings
Implement associated callback emberAfIncomingMessageCallback() to use. See Handlers for additional information.
emberIncomingMacMessageHandler#
void emberIncomingMacMessageHandler (EmberIncomingMacMessage * message)
This handler is invoked when a node of EMBER_MAC_MODE_DEVICE type or EMBER_MAC_MODE_SLEEPY_DEVICE has received a MAC frame.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberIncomingMacMessage * | [in] | message | An EmberIncomingMacMessage describing the incoming packet. |
Warnings
Implement associated callback emberAfIncomingMacMessageCallback() to use. See Handlers for additional information.
emberMessageSend#
EmberStatus emberMessageSend (EmberNodeId destination, uint8_t endpoint, uint8_t messageTag, EmberMessageLength messageLength, uint8_t * message, EmberMessageOptions options)
Send a message to the passed destination short ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | [in] | destination | The destination node short ID. |
| uint8_t | [in] | endpoint | The destination endpoint of the outgoing message. This value can't exceed EMBER_MAX_ENDPOINT. |
| uint8_t | [in] | messageTag | A value chosen by the application. This value will be passed in the corresponding emberMessageSentHandler() call. |
| EmberMessageLength | [in] | messageLength | The size of the message payload in bytes. Use the emberGetMaximumPayloadLength() API to determine the maximum message length allowed. |
| uint8_t * | [in] | message | A pointer to an array of bytes containing the message payload. |
| EmberMessageOptions | [in] | options | Specifies the EmberMessageOptions for the outgoing message. |
Returns
an EmberStatus value of:
EMBER_SUCCESS if the message was accepted by the stack. If a success status is returned, the emberMessageSentHandler() callback is invoked by the stack to indicate whether the message was successfully delivered or the reason for failure.
EMBER_INVALID_CALL if the node is not joined to a network or the node is of EMBER_MAC_MODE_DEVICE device type or EMBER_MAC_MODE_SLEEPY_DEVICE (use emberMacMessageSend instead).
EMBER_BAD_ARGUMENT if the packet length is 0, the passed TX options indicates some feature that is not supported, the passed endpoint exceeds EMBER_MAX_ENDPOINT
EMBER_MESSAGE_TOO_LONG if the message does not fit in a single frame.
EMBER_PHY_TX_BUSY if the message cannot be sent since the node does not support MAC queuing and the radio is currently busy.
EMBER_MAC_TRANSMIT_QUEUE_FULL if the outgoing MAC queue is currently full.
EMBER_NO_BUFFERS if the stack could not allocate enough RAM to store the submitted message.
EMBER_MAC_UNKNOWN_DESTINATION if the node is part of a star network and the destination node does not appear in the node's routing table.
EMBER_MAC_SECURITY_NOT_SUPPORTED if the message was requested to be sent out secured and either the local node does not support security or the destination node is known to not support security.
EMBER_MAC_BUSY if the message was not accepted because the MAC is currently performing some critical operation.
emberMacMessageSend#
EmberStatus emberMacMessageSend (EmberMacFrame * macFrame, uint8_t messageTag, EmberMessageLength messageLength, uint8_t * message, EmberMessageOptions options)
Create a MAC level frame and sends it to the passed destination. This API can only be used for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMacFrame * | [in] | macFrame | A pointer to an EmberMacFrame struct that specifies the source and destination addresses and the source and destination PAN IDs for the message to be sent. Note that if the source/destination PAN ID is not specified, it defaults to the node's PAN ID. Also, the destination address mode must be either EMBER_MAC_ADDRESS_MODE_SHORT or EMBER_MAC_ADDRESS_MODE_LONG. |
| uint8_t | [in] | messageTag | A value chosen by the application. This value will be passed in the corresponding emberMacMessageSentHandler() call. |
| EmberMessageLength | [in] | messageLength | The size in bytes of the message payload. The application can use the emberGetMaximumPayloadLength() API to determine the maximum allowable payload, given a permutation of source and destination addressing and other TX options. |
| uint8_t * | [in] | message | A pointer to an array of bytes containing the message payload. |
| EmberMessageOptions | [in] | options | Specifies the EmberMessageOptions for the outgoing message. |
Returns
an EmberStatus value of:
EMBER_SUCCESS if the message was accepted by the stack. If a success status is returned, the emberMacMessageSentHandler() callback will be invoked by the stack to indicate whether the message was successfully delivered or the reason for failure.
EMBER_INVALID_CALL if the node is of a node type other than EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE.
EMBER_BAD_ARGUMENT if the packet length is 0, the passed TX options indicates some feature that is not supported or the destination address mode is set to EMBER_MAC_ADDRESS_MODE_NONE.
EMBER_MESSAGE_TOO_LONG if the message does not fit in a single frame.
EMBER_PHY_TX_BUSY if the message cannot be sent since the node does not support MAC queuing and the radio is currently busy.
EMBER_MAC_TRANSMIT_QUEUE_FULL if the outgoing MAC queue is currently full.
EMBER_NO_BUFFERS if the stack could not allocate enough RAM to store the submitted message.
EMBER_MAC_SECURITY_NOT_SUPPORTED if the message was requested to be sent out with a security but no security plugin was enabled.
EMBER_MAC_BUSY if the message was not accepted because the MAC is currently performing a critical operation.
emberPollForData#
EmberStatus emberPollForData (void )
Send a data request command to the parent node. Note that if the node short ID is a value of EMBER_USE_LONG_ADDRESS, the node shall use its long ID as source address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
and EmberStatus value of:
EMBER_SUCCESS if the data poll was accepted by the MAC layer.
EMBER_INVALID_CALL if the node is not joined to a network, the node is not an end device, an EMBER_MAC_MODE_DEVICE or an EMBER_MAC_MODE_SLEEPY_DEVICE, or the node is of EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE node type, is not joined to a coordinator and the poll destination was not correctly set via the emberSetPollDestinationAddress() API.
EMBER_MAC_BUSY if the MAC is currently performing a critical operation.
emberSetPollDestinationAddress#
EmberStatus emberSetPollDestinationAddress (EmberMacAddress * destination)
Set data polls destination address for nodes of EMBER_MAC_MODE_DEVICE node type or EMBER_MAC_MODE_SLEEPY_DEVICE node type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMacAddress * | N/A | destination |
Returns
and EmberStatus value of EMBER_SUCCESS if the data poll destination was correctly set, or another EmberStatus value indicating the reason of failure.
emberPurgeIndirectMessages#
EmberStatus emberPurgeIndirectMessages (void )
Purge all indirect transmissions from the indirect message queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
an EmberStatus value of EMBER_SUCCESS if all indirect messages were purged, or another EmberStatus value indicating the reason of failure.
emberSetIndirectQueueTimeout#
EmberStatus emberSetIndirectQueueTimeout (uint32_t timeoutMs)
Set indirect queue timeout value. The indirect queue timeout is set by default to EMBER_INDIRECT_TRANSMISSION_TIMEOUT_MS.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | timeoutMs | The timeout in milliseconds to be set. |
Returns
an EmberStatus value of EMBER_SUCCESS if the passed timeout was successfully set, or a value of EMBER_BAD_ARGUMENT if the passed value is invalid.
emberGetMaximumPayloadLength#
uint16_t emberGetMaximumPayloadLength (EmberMacAddressMode srcAddressMode, EmberMacAddressMode dstAddressMode, bool interpan, bool secured)
Return the maximum payload according to the passed source and destination addressing modes, the passed secured flag, and the current configuration of the node.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberMacAddressMode | [in] | srcAddressMode | An EmberMacAddressMode value indicating the mode of the source address. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE. |
| EmberMacAddressMode | [in] | dstAddressMode | An EmberMacAddressMode value indicating the mode of the destination address. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE. |
| bool | [in] | interpan | Indicates whether the frame is an interpan frame or not. Note, this parameter is only meaningful if the node was started as EMBER_MAC_MODE_DEVICE or EMBER_MAC_MODE_SLEEPY_DEVICE. |
| bool | [in] | secured | Indicates whether the frame should be secured or not. |
Returns
The maximum payload length in bytes achievable according to the passed parameters or 0xFF if the node is currently active on a network or any of the passed parameters are invalid.
emberUsingLongMessages#
bool emberUsingLongMessages (void )
Indicates if the stack is currently using long messages or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
True if the stack currently uses long messages (length stored in a uint16_t) or false if it is not the case (length stored in a uint8_t).
emberNcpSetLongMessagesUse#
EmberStatus emberNcpSetLongMessagesUse (bool useLongMessages)
Set the current message length that the stack uses.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | useLongMessages | True to use long messages (length stored in a uint16_t), false to use short messages (length stored in a uint8_t). |
Note
This API is here to assure retro compatibility with old NCP Host lib versions. In NCP Host lib versions that do not support OFDM features (v1.1 and older), only short messaging is supported. For the NCP, short messages are used by default. The Host lib needs to call this API with useLongMessages set to true if it supports OFDM.
Warnings
This API changes the behavior of the Connect Serialization Protocol. It only has effect when using a RTOS or the NCP. Changing it may result in packets being incorrectly transfered through CSP when using a SUN-OFDM or SUN-FSK PHY.