A structure that stores an 802.15.4 address.
Public Attributes#
uint8_t
Long (EUI-64) address. Valid if mode
is EMBER_MAC_ADDRESS_MODE_LONG.
uint16_t
Short address (node ID). Valid if mode
is EMBER_MAC_ADDRESS_MODE_SHORT.
union EmberMacAddress::@3
Public Attribute Documentation#
longAddress#
uint8_t EmberMacAddress::longAddress[EUI64_SIZE]
Long (EUI-64) address. Valid if mode
is EMBER_MAC_ADDRESS_MODE_LONG.
Definition at line
361
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h
shortAddress#
uint16_t EmberMacAddress::shortAddress
Short address (node ID). Valid if mode
is EMBER_MAC_ADDRESS_MODE_SHORT.
Definition at line
366
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h
addr#
union EmberMacAddress::@3 EmberMacAddress::addr
Definition at line
367
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h
mode#
EmberMacAddressMode EmberMacAddress::mode
Addressing mode
Definition at line
369
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h