Control structure for tasks.
This structure should not be accessed directly.
Public Attribute Documentation#
nextEventTime#
uint32_t EmberTaskControl::nextEventTime
The time when the next event associated with this task will fire
Definition at line
614
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h
events#
EmberEventData* EmberTaskControl::events
The list of events associated with this task
Definition at line
616
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h
busy#
bool EmberTaskControl::busy
A flag that indicates the task has something to do other than events
Definition at line
618
of file /mnt/raid/workspaces/ws.2dqDELv9z/overlay/gsdk/protocol/flex/stack/include/ember-types.h