Complete events with a control and a handler procedure.
An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.
Public Attribute Documentation#
control#
EmberEventControl* EmberEventData_S::control
The control structure for the event.
Definition at line
603
of file /mnt/raid/workspaces/ws.S2kiimDMR/overlay/gsdk/protocol/flex/stack/include/ember-types.h
handler#
void(* EmberEventData_S::handler) (void)
The procedure to call when the event fires.
Definition at line
605
of file /mnt/raid/workspaces/ws.S2kiimDMR/overlay/gsdk/protocol/flex/stack/include/ember-types.h