Stack Counters#
Stack counters API.
Functions#
emberGetCounter(EmberCounterType counterType, uint32_t *count)
Retrieve the stack counter corresponding to the passed counter type.
Function Documentation#
emberGetCounter#
EmberStatus emberGetCounter (EmberCounterType counterType, uint32_t * count)
Retrieve the stack counter corresponding to the passed counter type.
Parameters
[in] | counterType | An EmberCounterType value indicating the stack counter to be retrieved. |
[out] | count | The counter of the requested |
Returns
An EmberStatus value of EMBER_SUCCESS if the stack counter was successfully retrieved. An EmberStatus value of EMBER_INVALID_CALL if the passed counterType is invalid. An EmberStatus value of EMBER_LIBRARY_NOT_PRESENT if the stack counter library is not present.
Definition at line
578
of file /mnt/raid/workspaces/ws.S2kiimDMR/overlay/gsdk/protocol/flex/stack/include/stack-info.h