IAR PLATFORM_HEADER Configuration#
Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler.
Note
iar.h should be included first in all source files by setting the preprocessor macro PLATFORM_HEADER to point to it. iar.h automatically includes platform-common.h.
See iar.h and platform-common.h for source code.
Master Variable Types#
LEGACY_PHY_BUILDThese are a set of typedefs to make the size of all variable declarations explicitly known.
A typedef to make the size of the variable explicitly known.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Use the Master Program Memory Declarations from platform-common.h.
Miscellaneous Macros#
A prototype definition for use by the assert macro. (see hal/micro/micro.h)
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
A friendlier name for the compiler's intrinsic for not stripping.
A friendlier name for the compiler's intrinsic for eeprom reference.
The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed(). (see hal/micro/micro.h)
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Declare a variable as unused to avoid a warning. Has no effect in IAR builds.
Some platforms need to cast enum values that have the high bit set.
Define the magic value that is interpreted by IAR C-SPY's Stack View.
Define a generic RAM function identifier to a compiler specific one.
Define a generic no operation identifier to a compiler specific one.
A convenience macro that makes it easy to change the field of a register to any unsigned value.
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.
Stub for code not running in simulation.
Stub for code not running in simulation.
Stub for code not running in simulation.
Use the Divide and Modulus Operations from platform-common.h.
Provide a portable way to specify the segment where a variable lives.
Convinience macro for turning a token into a string.
Provide a portable way to align data.
Provide a portable way to specify a symbol as weak.
Provide a portable way to specify a non initialized symbol.
Provide a portable way to specify a compile time assert.
External Declarations#
If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.These are routines that are defined in certain header files that we don't want to include, e.g. stdlib.h
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
Include platform-common.h last to pick up defaults and common definitions.
The kind of arguments the main function takes.
Include platform-common.h last to pick up defaults and common definitions.
Portable segment names#
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Functions#
Master Variable Types Documentation#
boolean#
typedef bool boolean
A typedef to make the size of the variable explicitly known.
82
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int8u#
typedef unsigned char int8u
Denotes that this platform supports 64-bit data-types.
83
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int8s#
typedef signed char int8s
Denotes that this platform supports 64-bit data-types.
84
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int16u#
typedef unsigned short int16u
Denotes that this platform supports 64-bit data-types.
85
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int16s#
typedef signed short int16s
Denotes that this platform supports 64-bit data-types.
86
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int32u#
typedef unsigned int int32u
Denotes that this platform supports 64-bit data-types.
87
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int32s#
typedef signed int int32s
Denotes that this platform supports 64-bit data-types.
88
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int64u#
typedef unsigned long long int64u
Denotes that this platform supports 64-bit data-types.
89
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int64s#
typedef signed long long int64s
Denotes that this platform supports 64-bit data-types.
90
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
PointerType#
typedef unsigned int PointerType
Denotes that this platform supports 64-bit data-types.
91
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
Miscellaneous Macros Documentation#
halInternalAssertFailed#
void halInternalAssertFailed (const char * filename, int linenumber)
A prototype definition for use by the assert macro. (see hal/micro/micro.h)
Type | Direction | Argument Name | Description |
---|---|---|---|
const char * | N/A | filename | |
int | N/A | linenumber |
152
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
halInternalResetWatchDog#
void halInternalResetWatchDog (void )
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
184
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
External Declarations Documentation#
abs#
int abs (int I)
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
Type | Direction | Argument Name | Description |
---|---|---|---|
int | N/A | I | An integer. |
Returns
A nonnegative integer.
527
of file /mnt/raid/workspaces/ws.tfWcRzYcf/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h