Button Control
Sample API functions for using push-buttons.
See button.h for source code.
Button State Definitions#
A set of numerical definitions for use with the button APIs indicating the state of a button.
Button state is pressed.
Button state is released.
Functions#
Initializes the buttons. This function is automatically called by halInit().
Returns the current state (pressed or released) of a button.
Returns the current state (pressed or released) of the pin associated with a button.
A callback called in interrupt context whenever a button changes its state.
Button State Definitions Documentation#
BUTTON_PRESSED
#define BUTTON_PRESSEDValue:
1
Button state is pressed.
32
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h
BUTTON_RELEASED
#define BUTTON_RELEASEDValue:
0
Button state is released.
36
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h
Function Documentation#
halInternalInitButton
void halInternalInitButton (void )
Initializes the buttons. This function is automatically called by halInit().
N/A |
43
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h
halButtonState
uint8_t halButtonState (uint8_t button)
Returns the current state (pressed or released) of a button.
N/A | button | The button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER. |
Note
This function is correlated with halButtonIsr() and so returns the shadow state rather than reading the actual state of the pin.
Returns
BUTTON_PRESSED if the button is pressed or BUTTON_RELEASED if the button is not pressed.
56
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h
halButtonPinState
uint8_t halButtonPinState (uint8_t button)
Returns the current state (pressed or released) of the pin associated with a button.
N/A | button | The button being queried, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER. |
This reads the actual state of the pin and can be used on startup to determine the initial position of the buttons.
Returns
BUTTON_PRESSED if the button is pressed or BUTTON_RELEASED if the button is not pressed.
70
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h
halButtonIsr
void halButtonIsr (uint8_t button, uint8_t state)
A callback called in interrupt context whenever a button changes its state.
N/A | button | The button which has changed state, either BUTTON0 or BUTTON1 as defined in the appropriate BOARD_HEADER. |
N/A | state | The new state of the button referenced by the button parameter, either BUTTON_PRESSED if the button has been pressed or BUTTON_RELEASED if the button has been released. |
Application Usage:\n Must be implemented by the application. This function should#
contain the functionality to be executed in response to changes of state in each of the buttons, or callbacks to the appropriate functionality.
86
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/button.h