The static part of an event. Each event can be used with only one event queue.
Public Attribute Documentation#
queue#
struct EventQueue_s* EventActions::queue
Definition at line
554
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/protocol/flex/stack/include/ember-types.h
handler#
void(* EventActions::handler) (struct Event_s *)
Definition at line
555
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/protocol/flex/stack/include/ember-types.h
marker#
void(* EventActions::marker) (struct Event_s *)
Definition at line
556
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/protocol/flex/stack/include/ember-types.h
name#
const char* EventActions::name
Definition at line
557
of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/protocol/flex/stack/include/ember-types.h