IAR PLATFORM_HEADER Configuration#

Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler.

Note

  • iar.h should be included first in all source files by setting the preprocessor macro PLATFORM_HEADER to point to it. iar.h automatically includes platform-common.h.

See iar.h and platform-common.h for source code.

Master Variable Types#

LEGACY_PHY_BUILDThese are a set of typedefs to make the size of all variable declarations explicitly known.

typedef bool

A typedef to make the size of the variable explicitly known.

typedef unsigned char

Denotes that this platform supports 64-bit data-types.

typedef signed char

Denotes that this platform supports 64-bit data-types.

typedef unsigned short

Denotes that this platform supports 64-bit data-types.

typedef signed short

Denotes that this platform supports 64-bit data-types.

typedef unsigned int

Denotes that this platform supports 64-bit data-types.

typedef signed int

Denotes that this platform supports 64-bit data-types.

typedef unsigned long long

Denotes that this platform supports 64-bit data-types.

typedef signed long long

Denotes that this platform supports 64-bit data-types.

typedef unsigned int

Denotes that this platform supports 64-bit data-types.

#define

Denotes that this platform supports 64-bit data-types.

#define

Use the Master Program Memory Declarations from platform-common.h.

Miscellaneous Macros#

void
halInternalAssertFailed(const char *filename, int linenumber)

A prototype definition for use by the assert macro. (see hal/micro/micro.h)

void

Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.

#define

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

#define
NTOHS (val)

Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.

#define
NTOHL (val)

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

#define

A friendlier name for the compiler's intrinsic for not stripping.

#define
EEPROM errorerror

A friendlier name for the compiler's intrinsic for eeprom reference.

#define

The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.

#define
assert (condition)

A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed(). (see hal/micro/micro.h)

#define

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.

#define

Declare a variable as unused to avoid a warning. Has no effect in IAR builds.

#define

Some platforms need to cast enum values that have the high bit set.

#define
STACK_FILL_VALUE 0xCDCDCDCDU

Define the magic value that is interpreted by IAR C-SPY's Stack View.

#define
RAMFUNC __ramfunc

Define a generic RAM function identifier to a compiler specific one.

#define

Define a generic no operation identifier to a compiler specific one.

#define
SET_REG_FIELD (reg, field, value)

A convenience macro that makes it easy to change the field of a register to any unsigned value.

#define
SET_CMSIS_REG (reg, mask, value)

A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.

#define
SET_CMSIS_REG_FIELD (reg, field, value)

A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.

#define

Stub for code not running in simulation.

#define

Stub for code not running in simulation.

#define

Stub for code not running in simulation.

#define

Use the Divide and Modulus Operations from platform-common.h.

#define
VAR_AT_SEGMENT (__variableDeclaration, __segmentName)

Provide a portable way to specify the segment where a variable lives.

#define

Convinience macro for turning a token into a string.

#define

Provide a portable way to align data.

#define
WEAK (__symbol)

Provide a portable way to specify a symbol as weak.

#define
NO_INIT (__symbol)

Provide a portable way to specify a non initialized symbol.

#define
STATIC_ASSERT (__condition, __errorstr)

Provide a portable way to specify a compile time assert.

External Declarations#

If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.These are routines that are defined in certain header files that we don't want to include, e.g. stdlib.h

int
abs(int I)

Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.

#define

Include platform-common.h last to pick up defaults and common definitions.

#define

The kind of arguments the main function takes.

#define

Include platform-common.h last to pick up defaults and common definitions.

Portable segment names#

#define
__NO_INIT__ ".noinitlegacy"

Portable segment names.

#define
__DEBUG_CHANNEL__ "DEBUG_CHANNEL"

Portable segment names.

#define
__INTVEC__ ".intvec"

Portable segment names.

#define
__CSTACK__ "CSTACK"

Portable segment names.

#define
__RESETINFO__ "RESETINFO"

Portable segment names.

#define
__DATA_INIT__ ".data_init"

Portable segment names.

#define
__DATA__ ".data"

Portable segment names.

#define
__BSS__ ".bss"

Portable segment names.

#define
__CONST__ ".rodata"

Portable segment names.

#define
__TEXT__ ".text"

Portable segment names.

#define
__TEXTRW_INIT__ ".textrw_init"

Portable segment names.

#define
__TEXTRW__ ".textrw"

Portable segment names.

#define
__AAT__ "AAT"

Portable segment names.

#define
__BAT__ "BAT"

Portable segment names.

#define

Portable segment names.

#define
__FAT__ "FAT"

Portable segment names.

#define
__RAT__ "RAT"

Portable segment names.

#define
__SIMEE__ "SIMEE"

Portable segment names.

#define
__PSSTORE__ "PSSTORE"

Portable segment names.

#define
__LONGTOKEN__ "LONGTOKEN"

Portable segment names.

#define
__EMHEAP__ "EMHEAP"

Portable segment names.

#define
__GUARD_REGION__ "GUARD_REGION"

Portable segment names.

#define
__DLIB_PERTHREAD_INIT__ "__DLIB_PERTHREAD_init"

Portable segment names.

#define
__DLIB_PERTHREAD_INITIALIZED_DATA__ "DLIB_PERTHREAD_INITIALIZED_DATA"

Portable segment names.

#define
__DLIB_PERTHREAD_ZERO_DATA__ "DLIB_PERTHREAD_ZERO_DATA"

Portable segment names.

#define
__INTERNAL_STORAGE__ "INTERNAL_STORAGE"

Portable segment names.

#define
__LOCKBITS_IN_MAINFLASH__ "LOCKBITS_IN_MAINFLASH"

Portable segment names.

#define
__UNRETAINED_RAM__ "UNRETAINED_RAM"

Portable segment names.

#define
_NO_INIT_SEGMENT_BEGIN __segment_begin(__NO_INIT__)

Portable segment names.

#define
_DEBUG_CHANNEL_SEGMENT_BEGIN __segment_begin(__DEBUG_CHANNEL__)

Portable segment names.

#define
_INTVEC_SEGMENT_BEGIN __segment_begin(__INTVEC__)

Portable segment names.

#define
_CSTACK_SEGMENT_BEGIN __segment_begin(__CSTACK__)

Portable segment names.

#define
_RESETINFO_SEGMENT_BEGIN __segment_begin(__RESETINFO__)

Portable segment names.

#define
_DATA_INIT_SEGMENT_BEGIN __segment_begin(__DATA_INIT__)

Portable segment names.

#define
_DATA_SEGMENT_BEGIN __segment_begin(__DATA__)

Portable segment names.

#define
_BSS_SEGMENT_BEGIN __segment_begin(__BSS__)

Portable segment names.

#define
_CONST_SEGMENT_BEGIN __segment_begin(__CONST__)

Portable segment names.

#define
_TEXT_SEGMENT_BEGIN __segment_begin(__TEXT__)

Portable segment names.

#define
_TEXTRW_INIT_SEGMENT_BEGIN __segment_begin(__TEXTRW_INIT__)

Portable segment names.

#define
_TEXTRW_SEGMENT_BEGIN __segment_begin(__TEXTRW__)

Portable segment names.

#define
_AAT_SEGMENT_BEGIN __segment_begin(__AAT__)

Portable segment names.

#define
_BAT_SEGMENT_BEGIN __segment_begin(__BAT__)

Portable segment names.

#define
_BAT_INIT_SEGMENT_BEGIN __segment_begin(__BAT_INIT__)

Portable segment names.

#define
_FAT_SEGMENT_BEGIN __segment_begin(__FAT__)

Portable segment names.

#define
_RAT_SEGMENT_BEGIN __segment_begin(__RAT__)

Portable segment names.

#define
_SIMEE_SEGMENT_BEGIN __segment_begin(__SIMEE__)

Portable segment names.

#define
_PSSTORE_SEGMENT_BEGIN __segment_begin(__PSSTORE__)

Portable segment names.

#define
_LONGTOKEN_SEGMENT_BEGIN __segment_begin(__LONGTOKEN__)

Portable segment names.

#define
_EMHEAP_SEGMENT_BEGIN __segment_begin(__EMHEAP__)

Portable segment names.

#define
_GUARD_REGION_SEGMENT_BEGIN __segment_begin(__GUARD_REGION__)

Portable segment names.

#define
_DLIB_PERTHREAD_INIT_SEGMENT_BEGIN __segment_begin(__DLIB_PERTHREAD_INIT__)

Portable segment names.

#define
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN __segment_begin(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.

#define
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN __segment_begin(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.

#define
_INTERNAL_STORAGE_SEGMENT_BEGIN __segment_begin(__INTERNAL_STORAGE__)

Portable segment names.

#define
_LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN __segment_begin(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.

#define
_UNRETAINED_RAM_SEGMENT_BEGIN __segment_begin(__UNRETAINED_RAM__)

Portable segment names.

#define
_NO_INIT_SEGMENT_END __segment_end(__NO_INIT__)

Portable segment names.

#define
_DEBUG_CHANNEL_SEGMENT_END __segment_end(__DEBUG_CHANNEL__)

Portable segment names.

#define
_INTVEC_SEGMENT_END __segment_end(__INTVEC__)

Portable segment names.

#define
_CSTACK_SEGMENT_END __segment_end(__CSTACK__)

Portable segment names.

#define
_RESETINFO_SEGMENT_END __segment_end(__RESETINFO__)

Portable segment names.

#define
_DATA_INIT_SEGMENT_END __segment_end(__DATA_INIT__)

Portable segment names.

#define
_DATA_SEGMENT_END __segment_end(__DATA__)

Portable segment names.

#define
_BSS_SEGMENT_END __segment_end(__BSS__)

Portable segment names.

#define
_CONST_SEGMENT_END __segment_end(__CONST__)

Portable segment names.

#define
_TEXT_SEGMENT_END __segment_end(__TEXT__)

Portable segment names.

#define
_TEXTRW_INIT_SEGMENT_END __segment_end(__TEXTRW_INIT__)

Portable segment names.

#define
_TEXTRW_SEGMENT_END __segment_end(__TEXTRW__)

Portable segment names.

#define
_AAT_SEGMENT_END __segment_end(__AAT__)

Portable segment names.

#define
_BAT_SEGMENT_END __segment_end(__BAT__)

Portable segment names.

#define
_BAT_INIT_SEGMENT_END __segment_end(__BAT_INIT__)

Portable segment names.

#define
_FAT_SEGMENT_END __segment_end(__FAT__)

Portable segment names.

#define
_RAT_SEGMENT_END __segment_end(__RAT__)

Portable segment names.

#define
_SIMEE_SEGMENT_END __segment_end(__SIMEE__)

Portable segment names.

#define
_PSSTORE_SEGMENT_END __segment_end(__PSSTORE__)

Portable segment names.

#define
_LONGTOKEN_SEGMENT_END __segment_end(__LONGTOKEN__)

Portable segment names.

#define
_EMHEAP_SEGMENT_END __segment_end(__EMHEAP__)

Portable segment names.

#define
_GUARD_REGION_SEGMENT_END __segment_end(__GUARD_REGION__)

Portable segment names.

#define
_DLIB_PERTHREAD_INIT_SEGMENT_END __segment_end(__DLIB_PERTHREAD_INIT__)

Portable segment names.

#define
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END __segment_end(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.

#define
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END __segment_end(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.

#define
_INTERNAL_STORAGE_SEGMENT_END __segment_end(__INTERNAL_STORAGE__)

Portable segment names.

#define
_LOCKBITS_IN_MAINFLASH_SEGMENT_END __segment_end(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.

#define
_UNRETAINED_RAM_SEGMENT_END __segment_end(__UNRETAINED_RAM__)

Portable segment names.

#define
_NO_INIT_SEGMENT_SIZE __segment_size(__NO_INIT__)

Portable segment names.

#define
_DEBUG_CHANNEL_SEGMENT_SIZE __segment_size(__DEBUG_CHANNEL__)

Portable segment names.

#define
_INTVEC_SEGMENT_SIZE __segment_size(__INTVEC__)

Portable segment names.

#define
_CSTACK_SEGMENT_SIZE __segment_size(__CSTACK__)

Portable segment names.

#define
_RESETINFO_SEGMENT_SIZE __segment_size(__RESETINFO__)

Portable segment names.

#define
_DATA_INIT_SEGMENT_SIZE __segment_size(__DATA_INIT__)

Portable segment names.

#define
_DATA_SEGMENT_SIZE __segment_size(__DATA__)

Portable segment names.

#define
_BSS_SEGMENT_SIZE __segment_size(__BSS__)

Portable segment names.

#define
_CONST_SEGMENT_SIZE __segment_size(__CONST__)

Portable segment names.

#define
_TEXT_SEGMENT_SIZE __segment_size(__TEXT__)

Portable segment names.

#define
_TEXTRW_INIT_SEGMENT_SIZE __segment_size(__TEXTRW_INIT__)

Portable segment names.

#define
_TEXTRW_SEGMENT_SIZE __segment_size(__TEXTRW__)

Portable segment names.

#define
_AAT_SEGMENT_SIZE __segment_size(__AAT__)

Portable segment names.

#define
_BAT_SEGMENT_SIZE __segment_size(__BAT__)

Portable segment names.

#define
_BAT_INIT_SEGMENT_SIZE __segment_size(__BAT_INIT__)

Portable segment names.

#define
_FAT_SEGMENT_SIZE __segment_size(__FAT__)

Portable segment names.

#define
_RAT_SEGMENT_SIZE __segment_size(__RAT__)

Portable segment names.

#define
_SIMEE_SEGMENT_SIZE __segment_size(__SIMEE__)

Portable segment names.

#define
_PSSTORE_SEGMENT_SIZE __segment_size(__PSSTORE__)

Portable segment names.

#define
_LONGTOKEN_SEGMENT_SIZE __segment_size(__LONGTOKEN__)

Portable segment names.

#define
_EMHEAP_SEGMENT_SIZE __segment_size(__EMHEAP__)

Portable segment names.

#define
_GUARD_REGION_SEGMENT_SIZE __segment_size(__GUARD_REGION__)

Portable segment names.

#define
_DLIB_PERTHREAD_INIT_SEGMENT_SIZE __segment_size(__DLIB_PERTHREAD_INIT__)

Portable segment names.

#define
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE __segment_size(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.

#define
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE __segment_size(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.

#define
_INTERNAL_STORAGE_SEGMENT_SIZE __segment_size(__INTERNAL_STORAGE__)

Portable segment names.

#define
_LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE __segment_size(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.

#define
_UNRETAINED_RAM_SEGMENT_SIZE __segment_size(__UNRETAINED_RAM__)

Portable segment names.

Functions#

Master Variable Types Documentation#

boolean#

typedef bool boolean

A typedef to make the size of the variable explicitly known.


Definition at line 82 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int8u#

typedef unsigned char int8u

Denotes that this platform supports 64-bit data-types.


Definition at line 83 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int8s#

typedef signed char int8s

Denotes that this platform supports 64-bit data-types.


Definition at line 84 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int16u#

typedef unsigned short int16u

Denotes that this platform supports 64-bit data-types.


Definition at line 85 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int16s#

typedef signed short int16s

Denotes that this platform supports 64-bit data-types.


Definition at line 86 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int32u#

typedef unsigned int int32u

Denotes that this platform supports 64-bit data-types.


Definition at line 87 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int32s#

typedef signed int int32s

Denotes that this platform supports 64-bit data-types.


Definition at line 88 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int64u#

typedef unsigned long long int64u

Denotes that this platform supports 64-bit data-types.


Definition at line 89 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

int64s#

typedef signed long long int64s

Denotes that this platform supports 64-bit data-types.


Definition at line 90 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

PointerType#

typedef unsigned int PointerType

Denotes that this platform supports 64-bit data-types.


Definition at line 91 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

HAL_HAS_INT64#

#define HAL_HAS_INT64

Denotes that this platform supports 64-bit data-types.


Definition at line 97 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_HAL_USE_COMMON_PGM_#

#define _HAL_USE_COMMON_PGM_

Use the Master Program Memory Declarations from platform-common.h.


Definition at line 102 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

Miscellaneous Macros Documentation#

halInternalAssertFailed#

void halInternalAssertFailed (const char * filename, int linenumber)

A prototype definition for use by the assert macro. (see hal/micro/micro.h)

Parameters
N/Afilename
N/Alinenumber

Definition at line 152 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

halInternalResetWatchDog#

void halInternalResetWatchDog (void )

Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.

Parameters
N/A

Definition at line 184 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

BIGENDIAN_CPU#

#define BIGENDIAN_CPU
Value:
false

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.


Definition at line 115 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

NTOHS#

#define NTOHS
Value:
(val)

Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.


Definition at line 121 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

NTOHL#

#define NTOHL
Value:
(val)

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.


Definition at line 122 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

NO_STRIPPING#

#define NO_STRIPPING
Value:
__root

A friendlier name for the compiler's intrinsic for not stripping.


Definition at line 128 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

EEPROM#

#define EEPROM
Value:
errorerror

A friendlier name for the compiler's intrinsic for eeprom reference.


Definition at line 134 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__SOURCEFILE__#

#define __SOURCEFILE__
Value:
__FILE__

The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.


Definition at line 143 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

assert#

#define assert

A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed(). (see hal/micro/micro.h)


Definition at line 160 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

halResetWatchdog#

#define halResetWatchdog
Value:
()

A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.


Definition at line 191 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

UNUSED#

#define UNUSED

Declare a variable as unused to avoid a warning. Has no effect in IAR builds.


Definition at line 198 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

SIGNED_ENUM#

#define SIGNED_ENUM

Some platforms need to cast enum values that have the high bit set.


Definition at line 203 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

STACK_FILL_VALUE#

#define STACK_FILL_VALUE
Value:
0xCDCDCDCDU

Define the magic value that is interpreted by IAR C-SPY's Stack View.


Definition at line 208 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

RAMFUNC#

#define RAMFUNC
Value:
__ramfunc

Define a generic RAM function identifier to a compiler specific one.


Definition at line 218 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

NO_OPERATION#

#define NO_OPERATION
Value:
()

Define a generic no operation identifier to a compiler specific one.


Definition at line 224 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

SET_REG_FIELD#

#define SET_REG_FIELD
Value:
do { \
reg = ((reg & (~field##_MASK)) \
| ((((uint32_t) value) << field##_BIT) \
& (field##_MASK))); \
} while (0)

A convenience macro that makes it easy to change the field of a register to any unsigned value.


Definition at line 230 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

SET_CMSIS_REG#

#define SET_CMSIS_REG
Value:
do { \
reg = (((reg) & (~mask)) | (value)); \
} while (0)

A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.


Definition at line 247 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

SET_CMSIS_REG_FIELD#

#define SET_CMSIS_REG_FIELD
Value:
do { \
reg = ((reg & (~_##field##_MASK)) \
| ((value << _##field##_SHIFT) \
& (_##field##_MASK))); \
} while (0)

A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.


Definition at line 258 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

simulatedTimePasses#

#define simulatedTimePasses

Stub for code not running in simulation.


Definition at line 268 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

simulatedTimePassesMs#

#define simulatedTimePassesMs

Stub for code not running in simulation.


Definition at line 273 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

simulatedSerialTimePasses#

#define simulatedSerialTimePasses

Stub for code not running in simulation.


Definition at line 278 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_HAL_USE_COMMON_DIVMOD_#

#define _HAL_USE_COMMON_DIVMOD_

Use the Divide and Modulus Operations from platform-common.h.


Definition at line 283 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

VAR_AT_SEGMENT#

#define VAR_AT_SEGMENT
Value:
(__variableDeclaration, __segmentName)

Provide a portable way to specify the segment where a variable lives.


Definition at line 289 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

STRINGIZE#

#define STRINGIZE
Value:
(X)

Convinience macro for turning a token into a string.


Definition at line 295 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

ALIGNMENT#

#define ALIGNMENT
Value:
(X)

Provide a portable way to align data.


Definition at line 300 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

WEAK#

#define WEAK
Value:
(__symbol)

Provide a portable way to specify a symbol as weak.


Definition at line 306 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

NO_INIT#

#define NO_INIT
Value:
(__symbol)

Provide a portable way to specify a non initialized symbol.


Definition at line 312 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

STATIC_ASSERT#

#define STATIC_ASSERT
Value:
(__condition, __errorstr)

Provide a portable way to specify a compile time assert.


Definition at line 318 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

External Declarations Documentation#

abs#

int abs (int I)

Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.

Parameters
N/AI

An integer.

Returns

  • A nonnegative integer.


Definition at line 527 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

PLATCOMMONOKTOINCLUDE#

#define PLATCOMMONOKTOINCLUDE

Include platform-common.h last to pick up defaults and common definitions.


Definition at line 536 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

MAIN_FUNCTION_PARAMETERS#

#define MAIN_FUNCTION_PARAMETERS
Value:
void

The kind of arguments the main function takes.


Definition at line 543 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

MAIN_FUNCTION_ARGUMENTS#

#define MAIN_FUNCTION_ARGUMENTS

Include platform-common.h last to pick up defaults and common definitions.


Definition at line 544 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

Portable segment names Documentation#

__NO_INIT__#

#define __NO_INIT__
Value:
".noinitlegacy"

Portable segment names.


Definition at line 341 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DEBUG_CHANNEL__#

#define __DEBUG_CHANNEL__
Value:
"DEBUG_CHANNEL"

Portable segment names.


Definition at line 344 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__INTVEC__#

#define __INTVEC__
Value:
".intvec"

Portable segment names.


Definition at line 345 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__CSTACK__#

#define __CSTACK__
Value:
"CSTACK"

Portable segment names.


Definition at line 346 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__RESETINFO__#

#define __RESETINFO__
Value:
"RESETINFO"

Portable segment names.


Definition at line 347 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DATA_INIT__#

#define __DATA_INIT__
Value:
".data_init"

Portable segment names.


Definition at line 348 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DATA__#

#define __DATA__
Value:
".data"

Portable segment names.


Definition at line 349 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__BSS__#

#define __BSS__
Value:
".bss"

Portable segment names.


Definition at line 350 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__CONST__#

#define __CONST__
Value:
".rodata"

Portable segment names.


Definition at line 351 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__TEXT__#

#define __TEXT__
Value:
".text"

Portable segment names.


Definition at line 352 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__TEXTRW_INIT__#

#define __TEXTRW_INIT__
Value:
".textrw_init"

Portable segment names.


Definition at line 353 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__TEXTRW__#

#define __TEXTRW__
Value:
".textrw"

Portable segment names.


Definition at line 354 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__AAT__#

#define __AAT__
Value:
"AAT"

Portable segment names.


Definition at line 355 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__BAT__#

#define __BAT__
Value:
"BAT"

Portable segment names.


Definition at line 356 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__BAT_INIT__#

#define __BAT_INIT__
Value:
"BAT"

Portable segment names.


Definition at line 357 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__FAT__#

#define __FAT__
Value:
"FAT"

Portable segment names.


Definition at line 358 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__RAT__#

#define __RAT__
Value:
"RAT"

Portable segment names.


Definition at line 359 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__SIMEE__#

#define __SIMEE__
Value:
"SIMEE"

Portable segment names.


Definition at line 360 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__PSSTORE__#

#define __PSSTORE__
Value:
"PSSTORE"

Portable segment names.


Definition at line 361 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__LONGTOKEN__#

#define __LONGTOKEN__
Value:
"LONGTOKEN"

Portable segment names.


Definition at line 362 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__EMHEAP__#

#define __EMHEAP__
Value:
"EMHEAP"

Portable segment names.


Definition at line 363 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__GUARD_REGION__#

#define __GUARD_REGION__
Value:
"GUARD_REGION"

Portable segment names.


Definition at line 364 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DLIB_PERTHREAD_INIT__#

#define __DLIB_PERTHREAD_INIT__
Value:
"__DLIB_PERTHREAD_init"

Portable segment names.


Definition at line 365 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DLIB_PERTHREAD_INITIALIZED_DATA__#

#define __DLIB_PERTHREAD_INITIALIZED_DATA__
Value:
"DLIB_PERTHREAD_INITIALIZED_DATA"

Portable segment names.


Definition at line 366 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__DLIB_PERTHREAD_ZERO_DATA__#

#define __DLIB_PERTHREAD_ZERO_DATA__
Value:
"DLIB_PERTHREAD_ZERO_DATA"

Portable segment names.


Definition at line 367 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__INTERNAL_STORAGE__#

#define __INTERNAL_STORAGE__
Value:
"INTERNAL_STORAGE"

Portable segment names.


Definition at line 368 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__LOCKBITS_IN_MAINFLASH__#

#define __LOCKBITS_IN_MAINFLASH__
Value:
"LOCKBITS_IN_MAINFLASH"

Portable segment names.


Definition at line 369 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

__UNRETAINED_RAM__#

#define __UNRETAINED_RAM__
Value:
"UNRETAINED_RAM"

Portable segment names.


Definition at line 370 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_NO_INIT_SEGMENT_BEGIN#

#define _NO_INIT_SEGMENT_BEGIN
Value:
__segment_begin(__NO_INIT__)

Portable segment names.


Definition at line 408 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DEBUG_CHANNEL_SEGMENT_BEGIN#

#define _DEBUG_CHANNEL_SEGMENT_BEGIN
Value:
__segment_begin(__DEBUG_CHANNEL__)

Portable segment names.


Definition at line 409 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTVEC_SEGMENT_BEGIN#

#define _INTVEC_SEGMENT_BEGIN
Value:
__segment_begin(__INTVEC__)

Portable segment names.


Definition at line 410 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CSTACK_SEGMENT_BEGIN#

#define _CSTACK_SEGMENT_BEGIN
Value:
__segment_begin(__CSTACK__)

Portable segment names.


Definition at line 411 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RESETINFO_SEGMENT_BEGIN#

#define _RESETINFO_SEGMENT_BEGIN
Value:
__segment_begin(__RESETINFO__)

Portable segment names.


Definition at line 412 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_INIT_SEGMENT_BEGIN#

#define _DATA_INIT_SEGMENT_BEGIN
Value:
__segment_begin(__DATA_INIT__)

Portable segment names.


Definition at line 413 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_SEGMENT_BEGIN#

#define _DATA_SEGMENT_BEGIN
Value:
__segment_begin(__DATA__)

Portable segment names.


Definition at line 414 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BSS_SEGMENT_BEGIN#

#define _BSS_SEGMENT_BEGIN
Value:
__segment_begin(__BSS__)

Portable segment names.


Definition at line 415 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CONST_SEGMENT_BEGIN#

#define _CONST_SEGMENT_BEGIN
Value:
__segment_begin(__CONST__)

Portable segment names.


Definition at line 416 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXT_SEGMENT_BEGIN#

#define _TEXT_SEGMENT_BEGIN
Value:
__segment_begin(__TEXT__)

Portable segment names.


Definition at line 417 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_INIT_SEGMENT_BEGIN#

#define _TEXTRW_INIT_SEGMENT_BEGIN
Value:
__segment_begin(__TEXTRW_INIT__)

Portable segment names.


Definition at line 418 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_SEGMENT_BEGIN#

#define _TEXTRW_SEGMENT_BEGIN
Value:
__segment_begin(__TEXTRW__)

Portable segment names.


Definition at line 419 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_AAT_SEGMENT_BEGIN#

#define _AAT_SEGMENT_BEGIN
Value:
__segment_begin(__AAT__)

Portable segment names.


Definition at line 420 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_SEGMENT_BEGIN#

#define _BAT_SEGMENT_BEGIN
Value:
__segment_begin(__BAT__)

Portable segment names.


Definition at line 421 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_INIT_SEGMENT_BEGIN#

#define _BAT_INIT_SEGMENT_BEGIN
Value:
__segment_begin(__BAT_INIT__)

Portable segment names.


Definition at line 422 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_FAT_SEGMENT_BEGIN#

#define _FAT_SEGMENT_BEGIN
Value:
__segment_begin(__FAT__)

Portable segment names.


Definition at line 423 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RAT_SEGMENT_BEGIN#

#define _RAT_SEGMENT_BEGIN
Value:
__segment_begin(__RAT__)

Portable segment names.


Definition at line 424 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_SIMEE_SEGMENT_BEGIN#

#define _SIMEE_SEGMENT_BEGIN
Value:
__segment_begin(__SIMEE__)

Portable segment names.


Definition at line 425 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_PSSTORE_SEGMENT_BEGIN#

#define _PSSTORE_SEGMENT_BEGIN
Value:
__segment_begin(__PSSTORE__)

Portable segment names.


Definition at line 426 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LONGTOKEN_SEGMENT_BEGIN#

#define _LONGTOKEN_SEGMENT_BEGIN
Value:
__segment_begin(__LONGTOKEN__)

Portable segment names.


Definition at line 427 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_EMHEAP_SEGMENT_BEGIN#

#define _EMHEAP_SEGMENT_BEGIN
Value:
__segment_begin(__EMHEAP__)

Portable segment names.


Definition at line 428 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_GUARD_REGION_SEGMENT_BEGIN#

#define _GUARD_REGION_SEGMENT_BEGIN
Value:
__segment_begin(__GUARD_REGION__)

Portable segment names.


Definition at line 429 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INIT_SEGMENT_BEGIN#

#define _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN
Value:
__segment_begin(__DLIB_PERTHREAD_INIT__)

Portable segment names.


Definition at line 430 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN#

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN
Value:
__segment_begin(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.


Definition at line 431 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN#

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN
Value:
__segment_begin(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.


Definition at line 432 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTERNAL_STORAGE_SEGMENT_BEGIN#

#define _INTERNAL_STORAGE_SEGMENT_BEGIN
Value:
__segment_begin(__INTERNAL_STORAGE__)

Portable segment names.


Definition at line 433 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN#

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN
Value:
__segment_begin(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.


Definition at line 434 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_UNRETAINED_RAM_SEGMENT_BEGIN#

#define _UNRETAINED_RAM_SEGMENT_BEGIN
Value:
__segment_begin(__UNRETAINED_RAM__)

Portable segment names.


Definition at line 435 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_NO_INIT_SEGMENT_END#

#define _NO_INIT_SEGMENT_END
Value:
__segment_end(__NO_INIT__)

Portable segment names.


Definition at line 437 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DEBUG_CHANNEL_SEGMENT_END#

#define _DEBUG_CHANNEL_SEGMENT_END
Value:
__segment_end(__DEBUG_CHANNEL__)

Portable segment names.


Definition at line 438 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTVEC_SEGMENT_END#

#define _INTVEC_SEGMENT_END
Value:
__segment_end(__INTVEC__)

Portable segment names.


Definition at line 439 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CSTACK_SEGMENT_END#

#define _CSTACK_SEGMENT_END
Value:
__segment_end(__CSTACK__)

Portable segment names.


Definition at line 440 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RESETINFO_SEGMENT_END#

#define _RESETINFO_SEGMENT_END
Value:
__segment_end(__RESETINFO__)

Portable segment names.


Definition at line 441 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_INIT_SEGMENT_END#

#define _DATA_INIT_SEGMENT_END
Value:
__segment_end(__DATA_INIT__)

Portable segment names.


Definition at line 442 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_SEGMENT_END#

#define _DATA_SEGMENT_END
Value:
__segment_end(__DATA__)

Portable segment names.


Definition at line 443 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BSS_SEGMENT_END#

#define _BSS_SEGMENT_END
Value:
__segment_end(__BSS__)

Portable segment names.


Definition at line 444 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CONST_SEGMENT_END#

#define _CONST_SEGMENT_END
Value:
__segment_end(__CONST__)

Portable segment names.


Definition at line 445 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXT_SEGMENT_END#

#define _TEXT_SEGMENT_END
Value:
__segment_end(__TEXT__)

Portable segment names.


Definition at line 446 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_INIT_SEGMENT_END#

#define _TEXTRW_INIT_SEGMENT_END
Value:
__segment_end(__TEXTRW_INIT__)

Portable segment names.


Definition at line 447 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_SEGMENT_END#

#define _TEXTRW_SEGMENT_END
Value:
__segment_end(__TEXTRW__)

Portable segment names.


Definition at line 448 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_AAT_SEGMENT_END#

#define _AAT_SEGMENT_END
Value:
__segment_end(__AAT__)

Portable segment names.


Definition at line 449 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_SEGMENT_END#

#define _BAT_SEGMENT_END
Value:
__segment_end(__BAT__)

Portable segment names.


Definition at line 450 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_INIT_SEGMENT_END#

#define _BAT_INIT_SEGMENT_END
Value:
__segment_end(__BAT_INIT__)

Portable segment names.


Definition at line 451 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_FAT_SEGMENT_END#

#define _FAT_SEGMENT_END
Value:
__segment_end(__FAT__)

Portable segment names.


Definition at line 452 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RAT_SEGMENT_END#

#define _RAT_SEGMENT_END
Value:
__segment_end(__RAT__)

Portable segment names.


Definition at line 453 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_SIMEE_SEGMENT_END#

#define _SIMEE_SEGMENT_END
Value:
__segment_end(__SIMEE__)

Portable segment names.


Definition at line 454 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_PSSTORE_SEGMENT_END#

#define _PSSTORE_SEGMENT_END
Value:
__segment_end(__PSSTORE__)

Portable segment names.


Definition at line 455 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LONGTOKEN_SEGMENT_END#

#define _LONGTOKEN_SEGMENT_END
Value:
__segment_end(__LONGTOKEN__)

Portable segment names.


Definition at line 456 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_EMHEAP_SEGMENT_END#

#define _EMHEAP_SEGMENT_END
Value:
__segment_end(__EMHEAP__)

Portable segment names.


Definition at line 457 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_GUARD_REGION_SEGMENT_END#

#define _GUARD_REGION_SEGMENT_END
Value:
__segment_end(__GUARD_REGION__)

Portable segment names.


Definition at line 458 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INIT_SEGMENT_END#

#define _DLIB_PERTHREAD_INIT_SEGMENT_END
Value:
__segment_end(__DLIB_PERTHREAD_INIT__)

Portable segment names.


Definition at line 459 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END#

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END
Value:
__segment_end(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.


Definition at line 460 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END#

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END
Value:
__segment_end(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.


Definition at line 461 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTERNAL_STORAGE_SEGMENT_END#

#define _INTERNAL_STORAGE_SEGMENT_END
Value:
__segment_end(__INTERNAL_STORAGE__)

Portable segment names.


Definition at line 462 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LOCKBITS_IN_MAINFLASH_SEGMENT_END#

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_END
Value:
__segment_end(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.


Definition at line 463 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_UNRETAINED_RAM_SEGMENT_END#

#define _UNRETAINED_RAM_SEGMENT_END
Value:
__segment_end(__UNRETAINED_RAM__)

Portable segment names.


Definition at line 464 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_NO_INIT_SEGMENT_SIZE#

#define _NO_INIT_SEGMENT_SIZE
Value:
__segment_size(__NO_INIT__)

Portable segment names.


Definition at line 466 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DEBUG_CHANNEL_SEGMENT_SIZE#

#define _DEBUG_CHANNEL_SEGMENT_SIZE
Value:
__segment_size(__DEBUG_CHANNEL__)

Portable segment names.


Definition at line 467 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTVEC_SEGMENT_SIZE#

#define _INTVEC_SEGMENT_SIZE
Value:
__segment_size(__INTVEC__)

Portable segment names.


Definition at line 468 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CSTACK_SEGMENT_SIZE#

#define _CSTACK_SEGMENT_SIZE
Value:
__segment_size(__CSTACK__)

Portable segment names.


Definition at line 469 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RESETINFO_SEGMENT_SIZE#

#define _RESETINFO_SEGMENT_SIZE
Value:
__segment_size(__RESETINFO__)

Portable segment names.


Definition at line 470 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_INIT_SEGMENT_SIZE#

#define _DATA_INIT_SEGMENT_SIZE
Value:
__segment_size(__DATA_INIT__)

Portable segment names.


Definition at line 471 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DATA_SEGMENT_SIZE#

#define _DATA_SEGMENT_SIZE
Value:
__segment_size(__DATA__)

Portable segment names.


Definition at line 472 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BSS_SEGMENT_SIZE#

#define _BSS_SEGMENT_SIZE
Value:
__segment_size(__BSS__)

Portable segment names.


Definition at line 473 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_CONST_SEGMENT_SIZE#

#define _CONST_SEGMENT_SIZE
Value:
__segment_size(__CONST__)

Portable segment names.


Definition at line 474 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXT_SEGMENT_SIZE#

#define _TEXT_SEGMENT_SIZE
Value:
__segment_size(__TEXT__)

Portable segment names.


Definition at line 475 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_INIT_SEGMENT_SIZE#

#define _TEXTRW_INIT_SEGMENT_SIZE
Value:
__segment_size(__TEXTRW_INIT__)

Portable segment names.


Definition at line 476 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_TEXTRW_SEGMENT_SIZE#

#define _TEXTRW_SEGMENT_SIZE
Value:
__segment_size(__TEXTRW__)

Portable segment names.


Definition at line 477 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_AAT_SEGMENT_SIZE#

#define _AAT_SEGMENT_SIZE
Value:
__segment_size(__AAT__)

Portable segment names.


Definition at line 478 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_SEGMENT_SIZE#

#define _BAT_SEGMENT_SIZE
Value:
__segment_size(__BAT__)

Portable segment names.


Definition at line 479 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_BAT_INIT_SEGMENT_SIZE#

#define _BAT_INIT_SEGMENT_SIZE
Value:
__segment_size(__BAT_INIT__)

Portable segment names.


Definition at line 480 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_FAT_SEGMENT_SIZE#

#define _FAT_SEGMENT_SIZE
Value:
__segment_size(__FAT__)

Portable segment names.


Definition at line 481 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_RAT_SEGMENT_SIZE#

#define _RAT_SEGMENT_SIZE
Value:
__segment_size(__RAT__)

Portable segment names.


Definition at line 482 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_SIMEE_SEGMENT_SIZE#

#define _SIMEE_SEGMENT_SIZE
Value:
__segment_size(__SIMEE__)

Portable segment names.


Definition at line 483 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_PSSTORE_SEGMENT_SIZE#

#define _PSSTORE_SEGMENT_SIZE
Value:
__segment_size(__PSSTORE__)

Portable segment names.


Definition at line 484 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LONGTOKEN_SEGMENT_SIZE#

#define _LONGTOKEN_SEGMENT_SIZE
Value:
__segment_size(__LONGTOKEN__)

Portable segment names.


Definition at line 485 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_EMHEAP_SEGMENT_SIZE#

#define _EMHEAP_SEGMENT_SIZE
Value:
__segment_size(__EMHEAP__)

Portable segment names.


Definition at line 486 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_GUARD_REGION_SEGMENT_SIZE#

#define _GUARD_REGION_SEGMENT_SIZE
Value:
__segment_size(__GUARD_REGION__)

Portable segment names.


Definition at line 487 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INIT_SEGMENT_SIZE#

#define _DLIB_PERTHREAD_INIT_SEGMENT_SIZE
Value:
__segment_size(__DLIB_PERTHREAD_INIT__)

Portable segment names.


Definition at line 488 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE#

#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE
Value:
__segment_size(__DLIB_PERTHREAD_INITIALIZED_DATA__)

Portable segment names.


Definition at line 489 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE#

#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE
Value:
__segment_size(__DLIB_PERTHREAD_ZERO_DATA__)

Portable segment names.


Definition at line 490 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_INTERNAL_STORAGE_SEGMENT_SIZE#

#define _INTERNAL_STORAGE_SEGMENT_SIZE
Value:
__segment_size(__INTERNAL_STORAGE__)

Portable segment names.


Definition at line 491 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE#

#define _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE
Value:
__segment_size(__LOCKBITS_IN_MAINFLASH__)

Portable segment names.


Definition at line 492 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

_UNRETAINED_RAM_SEGMENT_SIZE#

#define _UNRETAINED_RAM_SEGMENT_SIZE
Value:
__segment_size(__UNRETAINED_RAM__)

Portable segment names.


Definition at line 493 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h

Function Documentation#

_executeBarrierInstructions#

void _executeBarrierInstructions (void )
Parameters
N/A

Definition at line 501 of file /mnt/raid/workspaces/ws.myu1z4nKP/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h