Control structure for events.
This structure should not be accessed directly. It holds the event status (one of the EMBER_EVENT_ values) and the time left before the event fires.
Public Attribute Documentation#
status#
EmberEventUnits EmberEventControl::status
The event's status, either inactive or the units for timeToExecute.
Definition at line
585
of file /mnt/raid/workspaces/ws.Iq463TQni/overlay/gsdk/protocol/flex/stack/include/ember-types.h
taskid#
EmberTaskId EmberEventControl::taskid
The task ID this event belongs to.
Definition at line
587
of file /mnt/raid/workspaces/ws.Iq463TQni/overlay/gsdk/protocol/flex/stack/include/ember-types.h
timeToExecute#
uint32_t EmberEventControl::timeToExecute
How long before the event fires. Units are always in milliseconds.
Definition at line
591
of file /mnt/raid/workspaces/ws.Iq463TQni/overlay/gsdk/protocol/flex/stack/include/ember-types.h