IAR PLATFORM_HEADER Configuration#
Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler.
Note
iar.h should be included first in all source files by setting the preprocessor macro PLATFORM_HEADER to point to it. iar.h automatically includes platform-common.h.
See iar.h and platform-common.h for source code.
Master Variable Types#
LEGACY_PHY_BUILDThese are a set of typedefs to make the size of all variable declarations explicitly known.
A typedef to make the size of the variable explicitly known.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Denotes that this platform supports 64-bit data-types.
Use the Master Program Memory Declarations from platform-common.h.
Miscellaneous Macros#
A prototype definition for use by the assert macro. (see hal/micro/micro.h)
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
A friendlier name for the compiler's intrinsic for not stripping.
A friendlier name for the compiler's intrinsic for eeprom reference.
The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed(). (see hal/micro/micro.h)
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Declare a variable as unused to avoid a warning. Has no effect in IAR builds.
Some platforms need to cast enum values that have the high bit set.
Define the magic value that is interpreted by IAR C-SPY's Stack View.
Define a generic RAM function identifier to a compiler specific one.
Define a generic no operation identifier to a compiler specific one.
A convenience macro that makes it easy to change the field of a register to any unsigned value.
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.
Stub for code not running in simulation.
Stub for code not running in simulation.
Stub for code not running in simulation.
Use the Divide and Modulus Operations from platform-common.h.
Provide a portable way to specify the segment where a variable lives.
Convinience macro for turning a token into a string.
Provide a portable way to align data.
Provide a portable way to specify a symbol as weak.
Provide a portable way to specify a non initialized symbol.
Provide a portable way to specify a compile time assert.
External Declarations#
If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.These are routines that are defined in certain header files that we don't want to include, e.g. stdlib.h
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
Include platform-common.h last to pick up defaults and common definitions.
The kind of arguments the main function takes.
Include platform-common.h last to pick up defaults and common definitions.
Portable segment names#
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Portable segment names.
Functions#
Master Variable Types Documentation#
boolean#
typedef bool boolean
A typedef to make the size of the variable explicitly known.
82
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int8u#
typedef unsigned char int8u
Denotes that this platform supports 64-bit data-types.
83
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int8s#
typedef signed char int8s
Denotes that this platform supports 64-bit data-types.
84
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int16u#
typedef unsigned short int16u
Denotes that this platform supports 64-bit data-types.
85
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int16s#
typedef signed short int16s
Denotes that this platform supports 64-bit data-types.
86
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int32u#
typedef unsigned int int32u
Denotes that this platform supports 64-bit data-types.
87
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int32s#
typedef signed int int32s
Denotes that this platform supports 64-bit data-types.
88
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int64u#
typedef unsigned long long int64u
Denotes that this platform supports 64-bit data-types.
89
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
int64s#
typedef signed long long int64s
Denotes that this platform supports 64-bit data-types.
90
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
PointerType#
typedef unsigned int PointerType
Denotes that this platform supports 64-bit data-types.
91
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
HAL_HAS_INT64#
#define HAL_HAS_INT64
Denotes that this platform supports 64-bit data-types.
97
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_HAL_USE_COMMON_PGM_#
#define _HAL_USE_COMMON_PGM_
Use the Master Program Memory Declarations from platform-common.h.
102
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
Miscellaneous Macros Documentation#
halInternalAssertFailed#
void halInternalAssertFailed (const char * filename, int linenumber)
A prototype definition for use by the assert macro. (see hal/micro/micro.h)
N/A | filename | |
N/A | linenumber |
152
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
halInternalResetWatchDog#
void halInternalResetWatchDog (void )
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.
N/A |
184
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
BIGENDIAN_CPU#
#define BIGENDIAN_CPUValue:
false
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
115
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
NTOHS#
#define NTOHSValue:
(val)
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.
121
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
NTOHL#
#define NTOHLValue:
(val)
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
122
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
NO_STRIPPING#
#define NO_STRIPPINGValue:
__root
A friendlier name for the compiler's intrinsic for not stripping.
128
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
EEPROM#
#define EEPROMValue:
errorerror
A friendlier name for the compiler's intrinsic for eeprom reference.
134
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__SOURCEFILE__#
#define __SOURCEFILE__Value:
__FILE__
The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.
143
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
assert#
#define assert
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function halInternalAssertFailed(). (see hal/micro/micro.h)
160
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
halResetWatchdog#
#define halResetWatchdogValue:
()
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
191
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
UNUSED#
#define UNUSED
Declare a variable as unused to avoid a warning. Has no effect in IAR builds.
198
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
SIGNED_ENUM#
#define SIGNED_ENUM
Some platforms need to cast enum values that have the high bit set.
203
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
STACK_FILL_VALUE#
#define STACK_FILL_VALUEValue:
0xCDCDCDCDU
Define the magic value that is interpreted by IAR C-SPY's Stack View.
208
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
RAMFUNC#
#define RAMFUNCValue:
__ramfunc
Define a generic RAM function identifier to a compiler specific one.
218
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
NO_OPERATION#
#define NO_OPERATIONValue:
()
Define a generic no operation identifier to a compiler specific one.
224
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
SET_REG_FIELD#
#define SET_REG_FIELDValue:
A convenience macro that makes it easy to change the field of a register to any unsigned value.
230
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
SET_CMSIS_REG#
#define SET_CMSIS_REGValue:
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.
247
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
SET_CMSIS_REG_FIELD#
#define SET_CMSIS_REG_FIELDValue:
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.
258
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
simulatedTimePasses#
#define simulatedTimePasses
Stub for code not running in simulation.
268
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
simulatedTimePassesMs#
#define simulatedTimePassesMs
Stub for code not running in simulation.
273
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
simulatedSerialTimePasses#
#define simulatedSerialTimePasses
Stub for code not running in simulation.
278
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_HAL_USE_COMMON_DIVMOD_#
#define _HAL_USE_COMMON_DIVMOD_
Use the Divide and Modulus Operations from platform-common.h.
283
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
VAR_AT_SEGMENT#
#define VAR_AT_SEGMENTValue:
(__variableDeclaration, __segmentName)
Provide a portable way to specify the segment where a variable lives.
289
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
STRINGIZE#
#define STRINGIZEValue:
(X)
Convinience macro for turning a token into a string.
295
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
ALIGNMENT#
#define ALIGNMENTValue:
(X)
Provide a portable way to align data.
300
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
WEAK#
#define WEAKValue:
(__symbol)
Provide a portable way to specify a symbol as weak.
306
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
NO_INIT#
#define NO_INITValue:
(__symbol)
Provide a portable way to specify a non initialized symbol.
312
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
STATIC_ASSERT#
#define STATIC_ASSERTValue:
(__condition, __errorstr)
Provide a portable way to specify a compile time assert.
318
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
External Declarations Documentation#
abs#
int abs (int I)
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
N/A | I | An integer. |
Returns
A nonnegative integer.
527
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
PLATCOMMONOKTOINCLUDE#
#define PLATCOMMONOKTOINCLUDE
Include platform-common.h last to pick up defaults and common definitions.
536
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
MAIN_FUNCTION_PARAMETERS#
#define MAIN_FUNCTION_PARAMETERSValue:
void
The kind of arguments the main function takes.
543
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
MAIN_FUNCTION_ARGUMENTS#
#define MAIN_FUNCTION_ARGUMENTS
Include platform-common.h last to pick up defaults and common definitions.
544
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
Portable segment names Documentation#
__NO_INIT__#
#define __NO_INIT__Value:
".noinitlegacy"
Portable segment names.
341
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DEBUG_CHANNEL__#
#define __DEBUG_CHANNEL__Value:
"DEBUG_CHANNEL"
Portable segment names.
344
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__INTVEC__#
#define __INTVEC__Value:
".intvec"
Portable segment names.
345
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__CSTACK__#
#define __CSTACK__Value:
"CSTACK"
Portable segment names.
346
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__RESETINFO__#
#define __RESETINFO__Value:
"RESETINFO"
Portable segment names.
347
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DATA_INIT__#
#define __DATA_INIT__Value:
".data_init"
Portable segment names.
348
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DATA__#
#define __DATA__Value:
".data"
Portable segment names.
349
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__BSS__#
#define __BSS__Value:
".bss"
Portable segment names.
350
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__CONST__#
#define __CONST__Value:
".rodata"
Portable segment names.
351
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__TEXT__#
#define __TEXT__Value:
".text"
Portable segment names.
352
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__TEXTRW_INIT__#
#define __TEXTRW_INIT__Value:
".textrw_init"
Portable segment names.
353
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__TEXTRW__#
#define __TEXTRW__Value:
".textrw"
Portable segment names.
354
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__AAT__#
#define __AAT__Value:
"AAT"
Portable segment names.
355
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__BAT__#
#define __BAT__Value:
"BAT"
Portable segment names.
356
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__BAT_INIT__#
#define __BAT_INIT__Value:
"BAT"
Portable segment names.
357
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__FAT__#
#define __FAT__Value:
"FAT"
Portable segment names.
358
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__RAT__#
#define __RAT__Value:
"RAT"
Portable segment names.
359
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__SIMEE__#
#define __SIMEE__Value:
"SIMEE"
Portable segment names.
360
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__PSSTORE__#
#define __PSSTORE__Value:
"PSSTORE"
Portable segment names.
361
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__LONGTOKEN__#
#define __LONGTOKEN__Value:
"LONGTOKEN"
Portable segment names.
362
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__EMHEAP__#
#define __EMHEAP__Value:
"EMHEAP"
Portable segment names.
363
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__GUARD_REGION__#
#define __GUARD_REGION__Value:
"GUARD_REGION"
Portable segment names.
364
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DLIB_PERTHREAD_INIT__#
#define __DLIB_PERTHREAD_INIT__Value:
"__DLIB_PERTHREAD_init"
Portable segment names.
365
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DLIB_PERTHREAD_INITIALIZED_DATA__#
#define __DLIB_PERTHREAD_INITIALIZED_DATA__Value:
"DLIB_PERTHREAD_INITIALIZED_DATA"
Portable segment names.
366
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__DLIB_PERTHREAD_ZERO_DATA__#
#define __DLIB_PERTHREAD_ZERO_DATA__Value:
"DLIB_PERTHREAD_ZERO_DATA"
Portable segment names.
367
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__INTERNAL_STORAGE__#
#define __INTERNAL_STORAGE__Value:
"INTERNAL_STORAGE"
Portable segment names.
368
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__LOCKBITS_IN_MAINFLASH__#
#define __LOCKBITS_IN_MAINFLASH__Value:
"LOCKBITS_IN_MAINFLASH"
Portable segment names.
369
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
__UNRETAINED_RAM__#
#define __UNRETAINED_RAM__Value:
"UNRETAINED_RAM"
Portable segment names.
370
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_NO_INIT_SEGMENT_BEGIN#
#define _NO_INIT_SEGMENT_BEGINValue:
__segment_begin(__NO_INIT__)
Portable segment names.
408
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DEBUG_CHANNEL_SEGMENT_BEGIN#
#define _DEBUG_CHANNEL_SEGMENT_BEGINValue:
__segment_begin(__DEBUG_CHANNEL__)
Portable segment names.
409
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTVEC_SEGMENT_BEGIN#
#define _INTVEC_SEGMENT_BEGINValue:
__segment_begin(__INTVEC__)
Portable segment names.
410
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CSTACK_SEGMENT_BEGIN#
#define _CSTACK_SEGMENT_BEGINValue:
__segment_begin(__CSTACK__)
Portable segment names.
411
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RESETINFO_SEGMENT_BEGIN#
#define _RESETINFO_SEGMENT_BEGINValue:
__segment_begin(__RESETINFO__)
Portable segment names.
412
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_INIT_SEGMENT_BEGIN#
#define _DATA_INIT_SEGMENT_BEGINValue:
__segment_begin(__DATA_INIT__)
Portable segment names.
413
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_SEGMENT_BEGIN#
#define _DATA_SEGMENT_BEGINValue:
__segment_begin(__DATA__)
Portable segment names.
414
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BSS_SEGMENT_BEGIN#
#define _BSS_SEGMENT_BEGINValue:
__segment_begin(__BSS__)
Portable segment names.
415
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CONST_SEGMENT_BEGIN#
#define _CONST_SEGMENT_BEGINValue:
__segment_begin(__CONST__)
Portable segment names.
416
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXT_SEGMENT_BEGIN#
#define _TEXT_SEGMENT_BEGINValue:
__segment_begin(__TEXT__)
Portable segment names.
417
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_INIT_SEGMENT_BEGIN#
#define _TEXTRW_INIT_SEGMENT_BEGINValue:
__segment_begin(__TEXTRW_INIT__)
Portable segment names.
418
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_SEGMENT_BEGIN#
#define _TEXTRW_SEGMENT_BEGINValue:
__segment_begin(__TEXTRW__)
Portable segment names.
419
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_AAT_SEGMENT_BEGIN#
#define _AAT_SEGMENT_BEGINValue:
__segment_begin(__AAT__)
Portable segment names.
420
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_SEGMENT_BEGIN#
#define _BAT_SEGMENT_BEGINValue:
__segment_begin(__BAT__)
Portable segment names.
421
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_INIT_SEGMENT_BEGIN#
#define _BAT_INIT_SEGMENT_BEGINValue:
__segment_begin(__BAT_INIT__)
Portable segment names.
422
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_FAT_SEGMENT_BEGIN#
#define _FAT_SEGMENT_BEGINValue:
__segment_begin(__FAT__)
Portable segment names.
423
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RAT_SEGMENT_BEGIN#
#define _RAT_SEGMENT_BEGINValue:
__segment_begin(__RAT__)
Portable segment names.
424
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_SIMEE_SEGMENT_BEGIN#
#define _SIMEE_SEGMENT_BEGINValue:
__segment_begin(__SIMEE__)
Portable segment names.
425
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_PSSTORE_SEGMENT_BEGIN#
#define _PSSTORE_SEGMENT_BEGINValue:
__segment_begin(__PSSTORE__)
Portable segment names.
426
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LONGTOKEN_SEGMENT_BEGIN#
#define _LONGTOKEN_SEGMENT_BEGINValue:
__segment_begin(__LONGTOKEN__)
Portable segment names.
427
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_EMHEAP_SEGMENT_BEGIN#
#define _EMHEAP_SEGMENT_BEGINValue:
__segment_begin(__EMHEAP__)
Portable segment names.
428
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_GUARD_REGION_SEGMENT_BEGIN#
#define _GUARD_REGION_SEGMENT_BEGINValue:
__segment_begin(__GUARD_REGION__)
Portable segment names.
429
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INIT_SEGMENT_BEGIN#
#define _DLIB_PERTHREAD_INIT_SEGMENT_BEGINValue:
__segment_begin(__DLIB_PERTHREAD_INIT__)
Portable segment names.
430
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN#
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGINValue:
__segment_begin(__DLIB_PERTHREAD_INITIALIZED_DATA__)
Portable segment names.
431
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN#
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGINValue:
__segment_begin(__DLIB_PERTHREAD_ZERO_DATA__)
Portable segment names.
432
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTERNAL_STORAGE_SEGMENT_BEGIN#
#define _INTERNAL_STORAGE_SEGMENT_BEGINValue:
__segment_begin(__INTERNAL_STORAGE__)
Portable segment names.
433
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN#
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGINValue:
__segment_begin(__LOCKBITS_IN_MAINFLASH__)
Portable segment names.
434
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_UNRETAINED_RAM_SEGMENT_BEGIN#
#define _UNRETAINED_RAM_SEGMENT_BEGINValue:
__segment_begin(__UNRETAINED_RAM__)
Portable segment names.
435
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_NO_INIT_SEGMENT_END#
#define _NO_INIT_SEGMENT_ENDValue:
__segment_end(__NO_INIT__)
Portable segment names.
437
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DEBUG_CHANNEL_SEGMENT_END#
#define _DEBUG_CHANNEL_SEGMENT_ENDValue:
__segment_end(__DEBUG_CHANNEL__)
Portable segment names.
438
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTVEC_SEGMENT_END#
#define _INTVEC_SEGMENT_ENDValue:
__segment_end(__INTVEC__)
Portable segment names.
439
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CSTACK_SEGMENT_END#
#define _CSTACK_SEGMENT_ENDValue:
__segment_end(__CSTACK__)
Portable segment names.
440
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RESETINFO_SEGMENT_END#
#define _RESETINFO_SEGMENT_ENDValue:
__segment_end(__RESETINFO__)
Portable segment names.
441
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_INIT_SEGMENT_END#
#define _DATA_INIT_SEGMENT_ENDValue:
__segment_end(__DATA_INIT__)
Portable segment names.
442
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_SEGMENT_END#
#define _DATA_SEGMENT_ENDValue:
__segment_end(__DATA__)
Portable segment names.
443
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BSS_SEGMENT_END#
#define _BSS_SEGMENT_ENDValue:
__segment_end(__BSS__)
Portable segment names.
444
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CONST_SEGMENT_END#
#define _CONST_SEGMENT_ENDValue:
__segment_end(__CONST__)
Portable segment names.
445
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXT_SEGMENT_END#
#define _TEXT_SEGMENT_ENDValue:
__segment_end(__TEXT__)
Portable segment names.
446
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_INIT_SEGMENT_END#
#define _TEXTRW_INIT_SEGMENT_ENDValue:
__segment_end(__TEXTRW_INIT__)
Portable segment names.
447
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_SEGMENT_END#
#define _TEXTRW_SEGMENT_ENDValue:
__segment_end(__TEXTRW__)
Portable segment names.
448
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_AAT_SEGMENT_END#
#define _AAT_SEGMENT_ENDValue:
__segment_end(__AAT__)
Portable segment names.
449
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_SEGMENT_END#
#define _BAT_SEGMENT_ENDValue:
__segment_end(__BAT__)
Portable segment names.
450
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_INIT_SEGMENT_END#
#define _BAT_INIT_SEGMENT_ENDValue:
__segment_end(__BAT_INIT__)
Portable segment names.
451
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_FAT_SEGMENT_END#
#define _FAT_SEGMENT_ENDValue:
__segment_end(__FAT__)
Portable segment names.
452
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RAT_SEGMENT_END#
#define _RAT_SEGMENT_ENDValue:
__segment_end(__RAT__)
Portable segment names.
453
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_SIMEE_SEGMENT_END#
#define _SIMEE_SEGMENT_ENDValue:
__segment_end(__SIMEE__)
Portable segment names.
454
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_PSSTORE_SEGMENT_END#
#define _PSSTORE_SEGMENT_ENDValue:
__segment_end(__PSSTORE__)
Portable segment names.
455
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LONGTOKEN_SEGMENT_END#
#define _LONGTOKEN_SEGMENT_ENDValue:
__segment_end(__LONGTOKEN__)
Portable segment names.
456
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_EMHEAP_SEGMENT_END#
#define _EMHEAP_SEGMENT_ENDValue:
__segment_end(__EMHEAP__)
Portable segment names.
457
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_GUARD_REGION_SEGMENT_END#
#define _GUARD_REGION_SEGMENT_ENDValue:
__segment_end(__GUARD_REGION__)
Portable segment names.
458
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INIT_SEGMENT_END#
#define _DLIB_PERTHREAD_INIT_SEGMENT_ENDValue:
__segment_end(__DLIB_PERTHREAD_INIT__)
Portable segment names.
459
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END#
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_ENDValue:
__segment_end(__DLIB_PERTHREAD_INITIALIZED_DATA__)
Portable segment names.
460
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END#
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_ENDValue:
__segment_end(__DLIB_PERTHREAD_ZERO_DATA__)
Portable segment names.
461
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTERNAL_STORAGE_SEGMENT_END#
#define _INTERNAL_STORAGE_SEGMENT_ENDValue:
__segment_end(__INTERNAL_STORAGE__)
Portable segment names.
462
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LOCKBITS_IN_MAINFLASH_SEGMENT_END#
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_ENDValue:
__segment_end(__LOCKBITS_IN_MAINFLASH__)
Portable segment names.
463
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_UNRETAINED_RAM_SEGMENT_END#
#define _UNRETAINED_RAM_SEGMENT_ENDValue:
__segment_end(__UNRETAINED_RAM__)
Portable segment names.
464
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_NO_INIT_SEGMENT_SIZE#
#define _NO_INIT_SEGMENT_SIZEValue:
__segment_size(__NO_INIT__)
Portable segment names.
466
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DEBUG_CHANNEL_SEGMENT_SIZE#
#define _DEBUG_CHANNEL_SEGMENT_SIZEValue:
__segment_size(__DEBUG_CHANNEL__)
Portable segment names.
467
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTVEC_SEGMENT_SIZE#
#define _INTVEC_SEGMENT_SIZEValue:
__segment_size(__INTVEC__)
Portable segment names.
468
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CSTACK_SEGMENT_SIZE#
#define _CSTACK_SEGMENT_SIZEValue:
__segment_size(__CSTACK__)
Portable segment names.
469
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RESETINFO_SEGMENT_SIZE#
#define _RESETINFO_SEGMENT_SIZEValue:
__segment_size(__RESETINFO__)
Portable segment names.
470
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_INIT_SEGMENT_SIZE#
#define _DATA_INIT_SEGMENT_SIZEValue:
__segment_size(__DATA_INIT__)
Portable segment names.
471
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DATA_SEGMENT_SIZE#
#define _DATA_SEGMENT_SIZEValue:
__segment_size(__DATA__)
Portable segment names.
472
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BSS_SEGMENT_SIZE#
#define _BSS_SEGMENT_SIZEValue:
__segment_size(__BSS__)
Portable segment names.
473
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_CONST_SEGMENT_SIZE#
#define _CONST_SEGMENT_SIZEValue:
__segment_size(__CONST__)
Portable segment names.
474
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXT_SEGMENT_SIZE#
#define _TEXT_SEGMENT_SIZEValue:
__segment_size(__TEXT__)
Portable segment names.
475
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_INIT_SEGMENT_SIZE#
#define _TEXTRW_INIT_SEGMENT_SIZEValue:
__segment_size(__TEXTRW_INIT__)
Portable segment names.
476
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_TEXTRW_SEGMENT_SIZE#
#define _TEXTRW_SEGMENT_SIZEValue:
__segment_size(__TEXTRW__)
Portable segment names.
477
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_AAT_SEGMENT_SIZE#
#define _AAT_SEGMENT_SIZEValue:
__segment_size(__AAT__)
Portable segment names.
478
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_SEGMENT_SIZE#
#define _BAT_SEGMENT_SIZEValue:
__segment_size(__BAT__)
Portable segment names.
479
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_BAT_INIT_SEGMENT_SIZE#
#define _BAT_INIT_SEGMENT_SIZEValue:
__segment_size(__BAT_INIT__)
Portable segment names.
480
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_FAT_SEGMENT_SIZE#
#define _FAT_SEGMENT_SIZEValue:
__segment_size(__FAT__)
Portable segment names.
481
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_RAT_SEGMENT_SIZE#
#define _RAT_SEGMENT_SIZEValue:
__segment_size(__RAT__)
Portable segment names.
482
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_SIMEE_SEGMENT_SIZE#
#define _SIMEE_SEGMENT_SIZEValue:
__segment_size(__SIMEE__)
Portable segment names.
483
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_PSSTORE_SEGMENT_SIZE#
#define _PSSTORE_SEGMENT_SIZEValue:
__segment_size(__PSSTORE__)
Portable segment names.
484
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LONGTOKEN_SEGMENT_SIZE#
#define _LONGTOKEN_SEGMENT_SIZEValue:
__segment_size(__LONGTOKEN__)
Portable segment names.
485
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_EMHEAP_SEGMENT_SIZE#
#define _EMHEAP_SEGMENT_SIZEValue:
__segment_size(__EMHEAP__)
Portable segment names.
486
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_GUARD_REGION_SEGMENT_SIZE#
#define _GUARD_REGION_SEGMENT_SIZEValue:
__segment_size(__GUARD_REGION__)
Portable segment names.
487
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INIT_SEGMENT_SIZE#
#define _DLIB_PERTHREAD_INIT_SEGMENT_SIZEValue:
__segment_size(__DLIB_PERTHREAD_INIT__)
Portable segment names.
488
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE#
#define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZEValue:
__segment_size(__DLIB_PERTHREAD_INITIALIZED_DATA__)
Portable segment names.
489
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE#
#define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZEValue:
__segment_size(__DLIB_PERTHREAD_ZERO_DATA__)
Portable segment names.
490
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_INTERNAL_STORAGE_SEGMENT_SIZE#
#define _INTERNAL_STORAGE_SEGMENT_SIZEValue:
__segment_size(__INTERNAL_STORAGE__)
Portable segment names.
491
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE#
#define _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZEValue:
__segment_size(__LOCKBITS_IN_MAINFLASH__)
Portable segment names.
492
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h
_UNRETAINED_RAM_SEGMENT_SIZE#
#define _UNRETAINED_RAM_SEGMENT_SIZEValue:
__segment_size(__UNRETAINED_RAM__)
Portable segment names.
493
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/platform/base/hal/micro/cortexm3/compiler/iar.h