Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token.
Public Attribute Documentation#
panId#
uint16_t tokTypeStackNodeData::panId
The PanId of the device
Definition at line
249
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h
radioTxPower#
int16_t tokTypeStackNodeData::radioTxPower
The TX power configured for the device in deci-dBm
Definition at line
250
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h
radioFreqChannel#
uint16_t tokTypeStackNodeData::radioFreqChannel
The radio channel configured for the device
Definition at line
251
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h
nodeType#
uint8_t tokTypeStackNodeData::nodeType
The EmberNodeType configured for the device
Definition at line
252
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h
nodeId#
uint16_t tokTypeStackNodeData::nodeId
The NodeId (short address) of the device
Definition at line
253
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h
parentId#
uint16_t tokTypeStackNodeData::parentId
The NodeId of the device's parent, if any
Definition at line
254
of file /mnt/raid/workspaces/ws.r4wf6JzLX/overlay/gsdk/protocol/flex/stack/config/token-stack.h