Mailbox Client Plugin#

APIs for mailbox client.

Mailbox protocol is designed for devices that can't be online on the network all the time. The most common example for this is a sleepy end device.

Mailbox clients and the server can submit messages into the mailbox, which is stored in RAM on the mailbox server. Clients can then query the mailbox server for available messages.

The mailbox server will notify clients who submit messages when a message was delivered or when it couldn't be delivered due to an error.

Mailbox uses a plugin-configurable protocol endpoint, which is 15 by default.

The server can also configure the size of the mailbox (in number of packets, 25 by default) and the packet timeout, after which the server drops the message and notifies the source of the error.

The mailbox protocol uses standard data messages, so in case of sleepy end devices, it will use the indirect queue. This means that if a sleepy end device sends a request to a mailbox server, the end device should poll for the response.

Note

  • Mailbox is not available in MAC mode due to the lack of endpoints.

See mailbox-client.h and mailbox-client.c for source code.

Callbacks#

void
emberAfPluginMailboxClientMessageSubmitCallback(EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t tag)

Mailbox Client Message Submit Callback.

void
emberAfPluginMailboxClientMessageDeliveredCallback(EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t tag)

Mailbox Client Message Delivered Callback.

void
emberAfPluginMailboxClientCheckInboxCallback(EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageSource, uint8_t *message, EmberMessageLength messageLength, uint8_t tag, bool moreMessages)

Mailbox Client Check Inbox Callback.

Functions#

emberAfPluginMailboxClientMessageSubmit(EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t *message, EmberMessageLength messageLength, uint8_t tag, bool useSecurity)

Submit a data message to a mailbox server. If this API returns an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS, the corresponding asynchronous callback emberAfPluginMailboxClientMessageSubmitCallback() will be invoked to indicate whether the message was successfully submitted to the mailbox server or to inform the application of the reason of failure.

emberAfPluginMailboxClientCheckInbox(EmberNodeId mailboxServer, bool useSecurity)

Query a mailbox server for pending messages. If this API returns an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS, the corresponding asynchronous callback emberAfPluginMailboxClientCheckInboxCallback() will be invoked either to provide the retrieved message or to indicate the reason for failure.

Callbacks Documentation#

emberAfPluginMailboxClientMessageSubmitCallback#

void emberAfPluginMailboxClientMessageSubmitCallback (EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t tag)

Mailbox Client Message Submit Callback.

Parameters
TypeDirectionArgument NameDescription
EmberAfMailboxStatus[in]status

An EmberAfMailboxStatus value of:

EmberNodeId[in]mailboxServer

The node ID of the mailbox server.

EmberNodeId[in]messageDestination

The node ID of the destination.

uint8_tN/Atag

The tag value passed in the emberAfPluginMailboxClientMessageSubmit() API.

A callback invoked when a message arrived to the mailbox server after a call of emberAfPluginMailboxClientMessageSubmit().

Note

  • Receiving this callback requires the reception of a mailbox command message, which is only possible by polling if the message was submitted on a EMBER_STAR_SLEEPY_END_DEVICE.


Definition at line 168 of file /mnt/raid/workspaces/ws.OJKVohJa4/overlay/gsdk/protocol/flex/mailbox/mailbox-client/mailbox-client.h

emberAfPluginMailboxClientMessageDeliveredCallback#

void emberAfPluginMailboxClientMessageDeliveredCallback (EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t tag)

Mailbox Client Message Delivered Callback.

Parameters
TypeDirectionArgument NameDescription
EmberAfMailboxStatus[in]status

An EmberAfMailboxStatus value of:

EmberNodeId[in]mailboxServer

The node ID of the mailbox server where the message was submitted to.

EmberNodeId[in]messageDestination

The node ID of the destination.

uint8_t[in]tag

The tag value passed in the emberAfPluginMailboxClientMessageSubmit() API.

A callback that may be invoked on the submitter of the message either if the message that was submitted to a mailbox server reached its final destination or it timed-out. Note that the callback is not always called. If the status message from the server is lost, the callback won't be called.

Note

  • Receiving this callback requires the reception of a mailbox command message, which is only possible by polling if the message was submitted on a EMBER_STAR_SLEEPY_END_DEVICE.


Definition at line 199 of file /mnt/raid/workspaces/ws.OJKVohJa4/overlay/gsdk/protocol/flex/mailbox/mailbox-client/mailbox-client.h

emberAfPluginMailboxClientCheckInboxCallback#

void emberAfPluginMailboxClientCheckInboxCallback (EmberAfMailboxStatus status, EmberNodeId mailboxServer, EmberNodeId messageSource, uint8_t * message, EmberMessageLength messageLength, uint8_t tag, bool moreMessages)

Mailbox Client Check Inbox Callback.

Parameters
TypeDirectionArgument NameDescription
EmberAfMailboxStatus[in]status

An EmberAfMailboxStatus value of:

EmberNodeId[in]mailboxServer

The node id of the mailbox server responding.

EmberNodeId[in]messageSource

The source node ID of the retrieved message. Note that this parameter is meaningful only if the status parameter has an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS.

uint8_t *[in]message

A pointer to the retrieved message payload. Note that this parameter is meaningful only if the status parameter has an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS.

EmberMessageLength[in]messageLength

The length in bytes of the retrieved message payload. Note that this parameter is meaningful only if the status parameter has an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS.

uint8_t[in]tag

The tag value passed in the emberAfPluginMailboxClientMessageSubmit() API. Note that this parameter is meaningful only if the status parameter has an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS.

bool[in]moreMessages

This flag is true if the mailbox server has more pending messages for this mailbox client. Note that this parameter is meaningful only if the status parameter has an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS.

This callback is invoked after a successful call to the emberAfPluginMailboxClientCheckInbox() API. If a message was retrieved from the mailbox server, this callback passes it to the application. Otherwise, it indicates the reason for failure to the application.

Note

  • Receiving this callback requires the reception of a mailbox command message, which is only possible by polling if the message was submitted on a EMBER_STAR_SLEEPY_END_DEVICE.


Definition at line 250 of file /mnt/raid/workspaces/ws.OJKVohJa4/overlay/gsdk/protocol/flex/mailbox/mailbox-client/mailbox-client.h

Function Documentation#

emberAfPluginMailboxClientMessageSubmit#

EmberAfMailboxStatus emberAfPluginMailboxClientMessageSubmit (EmberNodeId mailboxServer, EmberNodeId messageDestination, uint8_t * message, EmberMessageLength messageLength, uint8_t tag, bool useSecurity)

Submit a data message to a mailbox server. If this API returns an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS, the corresponding asynchronous callback emberAfPluginMailboxClientMessageSubmitCallback() will be invoked to indicate whether the message was successfully submitted to the mailbox server or to inform the application of the reason of failure.

Parameters
TypeDirectionArgument NameDescription
EmberNodeId[in]mailboxServer

The node ID of the mailbox server.

EmberNodeId[in]messageDestination

The node ID of the destination for this data message.

uint8_t *[in]message

A pointer to the message to be sent.

EmberMessageLength[in]messageLength

The length in bytes of the message to be sent.

uint8_t[in]tag

A tag value which will be returned in all of the corresponding callbacks: emberAfPluginMailboxClientMessageSubmitCallback(), emberAfPluginMailboxClientMessageDeliveredCallback() and emberAfPluginMailboxClientCheckInboxCallback(). The application can use it to match the callbacks with the call.

bool[in]useSecurity

Set it true if the data message should be sent to the server using security.

Returns

Note

See Also


Definition at line 92 of file /mnt/raid/workspaces/ws.OJKVohJa4/overlay/gsdk/protocol/flex/mailbox/mailbox-client/mailbox-client.h

emberAfPluginMailboxClientCheckInbox#

EmberAfMailboxStatus emberAfPluginMailboxClientCheckInbox (EmberNodeId mailboxServer, bool useSecurity)

Query a mailbox server for pending messages. If this API returns an EmberAfMailboxStatus value of EMBER_MAILBOX_STATUS_SUCCESS, the corresponding asynchronous callback emberAfPluginMailboxClientCheckInboxCallback() will be invoked either to provide the retrieved message or to indicate the reason for failure.

Parameters
TypeDirectionArgument NameDescription
EmberNodeId[in]mailboxServer

The node ID of the mailbox server.

bool[in]useSecurity

Set it true if the request command and the responses to it should be sent secured. If a pending message was sent to a server securely, it will be always retrieved securely. This option only affects the request command and the pending messages that were sent without security to the server.

Returns

Note


Definition at line 128 of file /mnt/raid/workspaces/ws.OJKVohJa4/overlay/gsdk/protocol/flex/mailbox/mailbox-client/mailbox-client.h