Connect Stack Version#
Macros to determine the stack version.
Note that the Connect Stack version might not match the version of Flex SDK.
See config.h for source code.
Macros#
The major version of the release. First digit of A.B.C.D.
The minor version of the release. Second digit of A.B.C.D.
The patch version of the release. Third digit of A.B.C.D.
Special version of the release. Fourth digit of A.B.C.D.
Build number of the release. Should be stored on 2 bytes.
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
Version type of the release. EMBER_VERSION_TYPE_GA means generally available.
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
Macro Definition Documentation#
EMBER_MAJOR_VERSION#
#define EMBER_MAJOR_VERSIONValue:
4
The major version of the release. First digit of A.B.C.D.
EMBER_MINOR_VERSION#
#define EMBER_MINOR_VERSIONValue:
0
The minor version of the release. Second digit of A.B.C.D.
EMBER_PATCH_VERSION#
#define EMBER_PATCH_VERSIONValue:
0
The patch version of the release. Third digit of A.B.C.D.
Patch versions are fully backwards compatible as long as the major and minor version matches.
EMBER_SPECIAL_VERSION#
#define EMBER_SPECIAL_VERSIONValue:
0
Special version of the release. Fourth digit of A.B.C.D.
EMBER_BUILD_NUMBER#
#define EMBER_BUILD_NUMBERValue:
0
Build number of the release. Should be stored on 2 bytes.
EMBER_FULL_VERSION#
#define EMBER_FULL_VERSIONValue:
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
EMBER_VERSION_TYPE#
#define EMBER_VERSION_TYPEValue:
EMBER_VERSION_TYPE_GA
Version type of the release. EMBER_VERSION_TYPE_GA means generally available.
SOFTWARE_VERSION#
#define SOFTWARE_VERSIONValue:
EMBER_FULL_VERSION
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.