Connect Stack Version#
Macros to determine the stack version.
Note that the Connect Stack version might not match the version of Flex SDK.
See config.h for source code.
Macros#
#define
EMBER_MAJOR_VERSION 4
The major version of the release. First digit of A.B.C.D.
#define
EMBER_MINOR_VERSION 0
The minor version of the release. Second digit of A.B.C.D.
#define
EMBER_PATCH_VERSION 2
The patch version of the release. Third digit of A.B.C.D.
#define
EMBER_SPECIAL_VERSION 0
Special version of the release. Fourth digit of A.B.C.D.
#define
EMBER_BUILD_NUMBER 0
Build number of the release. Should be stored on 2 bytes.
#define
EMBER_FULL_VERSION undefined
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.
#define
EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA
Version type of the release. EMBER_VERSION_TYPE_GA means generally available.
#define
SOFTWARE_VERSION EMBER_FULL_VERSION
Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.