License#

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.

  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.

  3. This notice may not be removed or altered from any source distribution.

/***************************************************************************/
#define EMBER_MAJOR_VERSION   4

#define EMBER_MINOR_VERSION   1

#define EMBER_PATCH_VERSION   2

#define EMBER_SPECIAL_VERSION   0

#define EMBER_BUILD_NUMBER   0

#define EMBER_FULL_VERSION (  ((uint16_t)EMBER_MAJOR_VERSION << 12)   \
                              | ((uint16_t)EMBER_MINOR_VERSION <<  8) \
                              | ((uint16_t)EMBER_PATCH_VERSION <<  4) \
                              | ((uint16_t)EMBER_SPECIAL_VERSION))

#define EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA

#define SOFTWARE_VERSION EMBER_FULL_VERSION

Macros#

#define

The major version of the release. First digit of A.B.C.D.

#define

The minor version of the release. Second digit of A.B.C.D.

#define

The patch version of the release. Third digit of A.B.C.D.

#define

Special version of the release. Fourth digit of A.B.C.D.

#define

Build number of the release. Should be stored on 2 bytes.

#define

Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.

#define
EMBER_VERSION_TYPE EMBER_VERSION_TYPE_GA

Version type of the release. EMBER_VERSION_TYPE_GA means generally available.

#define
SOFTWARE_VERSION EMBER_FULL_VERSION

Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.

Macro Definition Documentation#

EMBER_MAJOR_VERSION#

#define EMBER_MAJOR_VERSION
Value:
4

The major version of the release. First digit of A.B.C.D.


EMBER_MINOR_VERSION#

#define EMBER_MINOR_VERSION
Value:
1

The minor version of the release. Second digit of A.B.C.D.


EMBER_PATCH_VERSION#

#define EMBER_PATCH_VERSION
Value:
2

The patch version of the release. Third digit of A.B.C.D.

Patch versions are fully backwards compatible as long as the major and minor version matches.


EMBER_SPECIAL_VERSION#

#define EMBER_SPECIAL_VERSION
Value:
0

Special version of the release. Fourth digit of A.B.C.D.


EMBER_BUILD_NUMBER#

#define EMBER_BUILD_NUMBER
Value:
0

Build number of the release. Should be stored on 2 bytes.


EMBER_FULL_VERSION#

#define EMBER_FULL_VERSION
Value:
( ((uint16_t)EMBER_MAJOR_VERSION << 12) \
| ((uint16_t)EMBER_MINOR_VERSION << 8) \
| ((uint16_t)EMBER_PATCH_VERSION << 4) \
| ((uint16_t)EMBER_SPECIAL_VERSION))

Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.


EMBER_VERSION_TYPE#

#define EMBER_VERSION_TYPE
Value:
EMBER_VERSION_TYPE_GA

Version type of the release. EMBER_VERSION_TYPE_GA means generally available.


SOFTWARE_VERSION#

#define SOFTWARE_VERSION
Value:
EMBER_FULL_VERSION

Full version number stored on 2 bytes, with each of the four digits stored on 4 bits.