Sl_bgapi_trace#

BGAPI trace utility for tracing BGAPI commands and events.

The functions provided by this component are automatically called by the BGAPI protocol implementation when a command is processed or an event is delivered to the application. The application does not need to and must not call these functions directly.

Enumerations#

enum
sli_bgapi_trace_message_type_command = 0x0
sli_bgapi_trace_message_type_response = 0x1
sli_bgapi_trace_message_type_event = 0x2
}

Specifies the full type of a BGAPI message.

Functions#

void
sli_bgapi_trace_output_message(sli_bgapi_trace_message_type_t type, uint32_t header, const void *data)

Enumeration Documentation#

sli_bgapi_trace_message_type_t#

sli_bgapi_trace_message_type_t

Specifies the full type of a BGAPI message.

Enumerator
sli_bgapi_trace_message_type_command

(0x0) The message is a BGAPI command

sli_bgapi_trace_message_type_response

(0x1) The message is a BGAPI response

sli_bgapi_trace_message_type_event

(0x2) The message is a BGAPI event


Function Documentation#

sli_bgapi_trace_init#

void sli_bgapi_trace_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize BGAPI tracing.


sli_bgapi_trace_output_message#

void sli_bgapi_trace_output_message (sli_bgapi_trace_message_type_t type, uint32_t header, const void * data)
Parameters
TypeDirectionArgument NameDescription
sli_bgapi_trace_message_type_t[in]type

The BGAPI message type

uint32_t[in]header

The BGAPI message header

const void *[in]data

The BGAPI message payload data

Output a BGAPI message to the trace channel.