TREL - Thread Stack#
This module defines Thread Radio Encapsulation Link (TREL) APIs for Thread Over Infrastructure.
The functions in this module require OPENTHREAD_CONFIG_RADIO_LINK_TREL_ENABLE
to be enabled.
Modules#
Typedefs#
Represents a TREL peer.
Represents an iterator for iterating over TREL peer table entries.
Represents a group of TREL related counters.
Functions#
Enables or disables TREL operation.
Indicates whether the TREL operation is enabled.
Initializes a peer table iterator.
Iterates over the peer table entries and get the next entry from the table.
Returns the number of TREL peers.
Sets the filter mode (enables/disables filtering).
Indicates whether or not the filter mode is enabled.
Gets the TREL counters.
Resets the TREL counters.
Typedef Documentation#
otTrelPeerIterator#
typedef uint16_t otTrelPeerIterator
Represents an iterator for iterating over TREL peer table entries.
otTrelCounters#
typedef otPlatTrelCounters otTrelCounters
Represents a group of TREL related counters.
Function Documentation#
otTrelSetEnabled#
void otTrelSetEnabled (otInstance * aInstance, bool aEnable)
Enables or disables TREL operation.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
bool | [in] | aEnable | A boolean to enable/disable the TREL operation. |
When aEnable
is true, this function initiates an ongoing DNS-SD browse on the service name "_trel._udp" within the local browsing domain to discover other devices supporting TREL. Device also registers a new service to be advertised using DNS-SD, with the service name is "_trel._udp" indicating its support for TREL. Device is then ready to receive TREL messages from peers.
When aEnable
is false, this function stops the DNS-SD browse on the service name "_trel._udp", stops advertising TREL DNS-SD service, and clears the TREL peer table.
Note
By default the OpenThread stack enables the TREL operation on start.
otTrelIsEnabled#
bool otTrelIsEnabled (otInstance * aInstance)
Indicates whether the TREL operation is enabled.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance. |
otTrelInitPeerIterator#
void otTrelInitPeerIterator (otInstance * aInstance, otTrelPeerIterator * aIterator)
Initializes a peer table iterator.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance. |
otTrelPeerIterator * | [in] | aIterator | The iterator to initialize. |
otTrelGetNextPeer#
const otTrelPeer * otTrelGetNextPeer (otInstance * aInstance, otTrelPeerIterator * aIterator)
Iterates over the peer table entries and get the next entry from the table.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance. |
otTrelPeerIterator * | [in] | aIterator | The iterator. MUST be initialized. |
Returns
A pointer to the next
otTrelPeer
entry orNULL
if no more entries in the table.
otTrelGetNumberOfPeers#
uint16_t otTrelGetNumberOfPeers (otInstance * aInstance)
Returns the number of TREL peers.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
The number of TREL peers.
otTrelSetFilterEnabled#
void otTrelSetFilterEnabled (otInstance * aInstance, bool aEnable)
Sets the filter mode (enables/disables filtering).
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance. |
bool | [in] | aEnable | TRUE to enable filter mode, FALSE to disable filter mode. |
When filter mode is enabled, any rx and tx traffic through TREL interface is silently dropped. This is mainly intended for use during testing.
Unlike otTrel{Enable/Disable}()
which fully starts/stops the TREL operation, when filter mode is enabled the TREL interface continues to be enabled.
otTrelIsFilterEnabled#
bool otTrelIsFilterEnabled (otInstance * aInstance)
Indicates whether or not the filter mode is enabled.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | The OpenThread instance. |
otTrelGetCounters#
const otTrelCounters * otTrelGetCounters (otInstance * aInstance)
Gets the TREL counters.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
A pointer to the TREL counters.
otTrelResetCounters#
void otTrelResetCounters (otInstance * aInstance)
Resets the TREL counters.
Type | Direction | Argument Name | Description |
---|---|---|---|
otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |