Core API, inititalizing of SE Manager and SE command context (Core) ... Description 0 Ignore ... Configure sl_se_command_context_t with sl_se_set_yield to yield the CPU core when the SE ...
You should avoid using it in production. ... sl_iostream_rtt_handle sl_iostream_instance_info_t sl_iostream_instance_rtt_info ... sl_iostream_instance_info_t sl_iostream_instance_rtt_info
ProductMicrocontrollersResource TypeSoftware API documentation
Gecko Platform 3.0.0.2 GA Gecko SDK Suite 3.0 July 29, 2020 ... Gecko Bootloader Added rollback prevention feature ... Added Power Manager service in platform/service.
3.Standard debug lock can transit to permanent debug lock by disabling the Device ... Command Key 3 Signed by ... 0 = No action on the corresponding debug option if it was locked (i.e., 1)