ASSERT - Assert#
Assert/error checking module.
By default, library assert usage is not included to reduce footprint and processing overhead. Further, assert usage is decoupled from ISO C assert handling (NDEBUG usage) to allow using ISO C assert without including assert statements.
Below are available defines for controlling assert inclusion. The defines are typically for a project to be used by the preprocessor.
If DEBUG_EFM is defined, the internal library assert handling will be used. This is implemented as a simple while(true) loop. DEBUG_EFM is not defined by default.
If DEBUG_EFM_USER is defined, the user must provide custom implementation of the assertEFM() function.
If both DEBUG_EFM and DEBUG_EFM_USER are undefined, all EFM_ASSERT() statements are not operational.
Note
The internal assert is documented because DEBUG_EFM is defined in the doxygen configuration.
Macros#
Default assertion is not operational.
Function Documentation#
assertEFM#
void assertEFM (const char * file, int line)
Assert function for EFM.
Type | Direction | Argument Name | Description |
---|---|---|---|
const char * | [in] | file | - path and file name of the assert. |
int | [in] | line | - line number, in the file. |