LEUART driver instance initialization structure.
LEUART driver instance initialization structure. Contains a number of UARTDRV configuration options. It is required to initialize a driver instance. This structure is passed to UARTDRV_InitLeuart() when initializing a UARTDRV instance.
Public Attributes#
LEUART_TypeDef *
The peripheral used for LEUART.
uint32_t
UART baud rate.
uint8_t
Location number for LEUART pins.
LEUART_Stopbits_TypeDef
Number of stop bits.
LEUART_Parity_TypeDef
Parity configuration.
Flow control mode.
GPIO_Port_TypeDef
CTS pin port number.
uint8_t
CTS pin number.
GPIO_Port_TypeDef
RTS pin port number.
uint8_t
RTS pin number.
Receive operation queue.
Transmit operation queue.