CORE - Core Interrupt#
Introduction#
CORE interrupt API provides a simple and safe means to disable and enable interrupts to protect sections of code.
This is often referred to as "critical sections". This module provides support for three types of critical sections, each with different interrupt blocking capabilities.
CRITICAL section: Inside a critical section, all interrupts are disabled (except for fault handlers). The PRIMASK register is always used for interrupt disable/enable.
ATOMIC section: This type of section is configurable and the default method is to use PRIMASK. With BASEPRI configuration, interrupts with priority equal to or lower than a given configurable level are disabled. The interrupt disable priority level is defined at compile time. The BASEPRI register is not available for all architectures.
NVIC mask section: Disable NVIC (external interrupts) on an individual manner.
em_core also has an API for manipulating RAM-based interrupt vector tables.
Compile-time Configuration#
The following #defines are used to configure em_core:
// The interrupt priority level used inside ATOMIC sections.
#define CORE_ATOMIC_BASE_PRIORITY_LEVEL 3
// A method used for interrupt disable/enable within ATOMIC sections.
#define CORE_ATOMIC_METHOD CORE_ATOMIC_METHOD_PRIMASK
If the default values do not support your needs, they can be overridden by supplying -D compiler flags on the compiler command line or by collecting all macro redefinitions in a file named emlib_config.h and then supplying -DEMLIB_USER_CONFIG on a compiler command line.
Note
The default emlib configuration for ATOMIC section interrupt disable method is using PRIMASK, i.e., ATOMIC sections are implemented as CRITICAL sections.
Due to architectural limitations Cortex-M0+ devices do not support ATOMIC type critical sections using the BASEPRI register. On M0+ devices ATOMIC section helper macros are available but they are implemented as CRITICAL sections using PRIMASK register.
Macro API#
The primary em_core API is the macro API. Macro API will map to correct CORE functions according to the selected CORE_ATOMIC_METHOD and similar configurations (the full CORE API is of course also available). The most useful macros are as follows:
CORE_DECLARE_IRQ_STATECORE_ENTER_ATOMIC()@n Used together to implement an ATOMIC section.
{
CORE_DECLARE_IRQ_STATE; // Storage for saving IRQ state prior to
// atomic section entry.
CORE_ENTER_ATOMIC(); // Enter atomic section.
...
... your code goes here ...
...
CORE_EXIT_ATOMIC(); // Exit atomic section, IRQ state is restored.
}
@n A concatenation of all three macros above.
{
CORE_ATOMIC_SECTION(
...
... your code goes here ...
...
)
}
CORE_DECLARE_IRQ_STATECORE_ENTER_CRITICAL()CORE_EXIT_CRITICAL()@n These macros implement CRITICAL sections in a similar fashion as described above for ATOMIC sections.
CORE_DECLARE_NVIC_STATECORE_ENTER_NVIC()CORE_EXIT_NVIC()@n These macros implement NVIC mask sections in a similar fashion as described above for ATOMIC sections. See Examples for an example.
Refer to Macros or Macro Definition Documentation below for a full list of macros.
API reimplementation#
Most of the functions in the API are implemented as weak functions. This means that it is easy to reimplement when special needs arise. Shown below is a reimplementation of CRITICAL sections suitable if FreeRTOS OS is used:
CORE_irqState_t CORE_EnterCritical(void)
{
vPortEnterCritical();
return 0;
}
void CORE_ExitCritical(CORE_irqState_t irqState)
{
(void)irqState;
vPortExitCritical();
}
Also note that CORE_Enter/ExitCritical() are not implemented as inline functions. As a result, reimplementations will be possible even when original implementations are inside a linked library.
Some RTOSes must be notified on interrupt handler entry and exit. Macros CORE_INTERRUPT_ENTRY() and CORE_INTERRUPT_EXIT() are suitable placeholders for inserting such code. Insert these macros in all your interrupt handlers and then override the default macro implementations. This is an example if uC/OS is used:
// In emlib_config.h:
#define CORE_INTERRUPT_ENTRY() OSIntEnter()
#define CORE_INTERRUPT_EXIT() OSIntExit()
Interrupt vector tables#
When using RAM based interrupt vector tables it is the user's responsibility to allocate the table space correctly. The tables must be aligned as specified in the CPU reference manual.
@n Initialize a RAM based vector table by copying table entries from a source vector table to a target table. VTOR is set to the address of the target vector table.
CORE_GetNvicRamTableHandler()@n Use these functions to get or set the interrupt handler for a specific IRQn. They both use the interrupt vector table defined by the current VTOR register value.
Maximum Interrupt Disabled Time#
The maximum time spent (in cycles) in critical and atomic sections can be measured for performance and interrupt latency analysis. To activate this feature, the Cycle Counter driver must be included in the project. To enable the timings, use the SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING configuration option. When enabled, the functions CORE_get_max_time_critical_section()CORE_get_max_time_atomic_section() can be used to get the max timings since startup.
Examples#
Implement an NVIC critical section:
{
CORE_DECLARE_NVIC_ZEROMASK(mask); // A zero initialized NVIC disable mask
// Set mask bits for IRQs to block in the NVIC critical section.
// In many cases, you can create the disable mask once upon application
// startup and use the mask globally throughout the application lifetime.
CORE_NvicMaskSetIRQ(LEUART0_IRQn, &mask);
CORE_NvicMaskSetIRQ(VCMP_IRQn, &mask);
// Enter NVIC critical section with the disable mask
CORE_NVIC_SECTION(&mask,
...
... your code goes here ...
...
)
}
Porting from em_int#
Existing code using INT_Enable() and INT_Disable() must be ported to the em_core API. While em_int used, a global counter to store the interrupt state, em_core uses a local variable. Any usage of INT_Disable(), therefore, needs to be replaced with a declaration of the interrupt state variable before entering the critical section.
Since the state variable is in local scope, the critical section exit needs to occur within the scope of the variable. If multiple nested critical sections are used, each needs to have its own state variable in its own scope.
In many cases, completely disabling all interrupts using CRITICAL sections might be more heavy-handed than needed. When porting, consider whether other types of sections, such as ATOMIC or NVIC mask, can be used to only disable a subset of the interrupts.
Replacing em_int calls with em_core function calls:
void func(void)
{
// INT_Disable();
CORE_DECLARE_IRQ_STATE;
CORE_ENTER_ATOMIC();
.
.
.
// INT_Enable();
CORE_EXIT_ATOMIC();
}
Modules#
Typedefs#
Storage for PRIMASK or BASEPRI value.
Storage for PRIMASK or BASEPRI value.
Functions#
Check if a specific interrupt is disabled or blocked.
Get the current NVIC enable mask state.
Get NVIC disable state for a given mask.
Enter a NVIC mask section.
Disable NVIC interrupts.
Set current NVIC interrupt enable mask.
Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts.
Utility function to set an IRQn bit in a NVIC enable/disable mask.
Utility function to clear an IRQn bit in a NVIC enable/disable mask.
Check if an NVIC interrupt is disabled.
Utility function to get the handler for a specific interrupt.
Utility function to set the handler for a specific interrupt.
Initialize an interrupt vector table by copying table entries from a source to a target table.
Disable interrupts.
Enable interrupts.
Exit a CRITICAL section.
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
Enter a CRITICAL section.
Disable interrupts.
Enable interrupts.
Exit an ATOMIC section.
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
Enter an ATOMIC section.
Check whether the current CPU operation mode is handler mode.
Check if interrupts are disabled.
Returns the max time spent in critical section.
Returns the max time spent in atomic section.
Clears the max time spent in atomic section.
Clears the max time spent in atomic section.
Macros#
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
CRITICAL style interrupt disable.
CRITICAL style interrupt enable.
Convenience macro for implementing a CRITICAL section.
Enter CRITICAL section.
Exit CRITICAL section.
CRITICAL style yield.
ATOMIC style interrupt disable.
ATOMIC style interrupt enable.
Convenience macro for implementing an ATOMIC section.
Enter ATOMIC section.
Exit ATOMIC section.
ATOMIC style yield.
Number of words in a NVIC mask set.
Number of entries in a default interrupt vector table.
Highest priority for core interrupt.
Default priority for core interrupt.
Lowest priority for core interrupt.
Default method to disable interrupts in ATOMIC sections.
Specify which method to use when implementing ATOMIC sections.
Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros.
Allocate storage for NVIC interrupt masks.
Allocate storage for and zero initialize NVIC interrupt mask.
NVIC mask style interrupt disable.
NVIC mask style interrupt enable.
Convenience macro for implementing a NVIC mask section.
Enter NVIC mask section.
Exit NVIC mask section.
NVIC maks style yield.
Start counter.
Stop counter.
Use PRIMASK register to disable interrupts in ATOMIC sections.
Use BASEPRI register to disable interrupts in ATOMIC sections.
The interrupt priority level disabled within ATOMIC regions.
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
CRITICAL style interrupt disable.
CRITICAL style interrupt enable.
Convenience macro for implementing a CRITICAL section.
Enter CRITICAL section.
Exit CRITICAL section.
CRITICAL style yield.
ATOMIC style interrupt disable.
ATOMIC style interrupt enable.
Convenience macro for implementing an ATOMIC section.
Enter ATOMIC section.
Exit ATOMIC section.
ATOMIC style yield.
Check if IRQ is disabled.
Check if inside an IRQ handler.
Placeholder for optional interrupt handler entry code.
Placeholder for optional interrupt handler exit code.
Typedef Documentation#
CORE_irqState_t#
typedef uint32_t CORE_irqState_t
Storage for PRIMASK or BASEPRI value.
119
of file platform/emlib/host/inc/em_core_generic.h
CORE_irqState_t#
typedef uint32_t CORE_irqState_t
Storage for PRIMASK or BASEPRI value.
146
of file platform/emlib/inc/em_core_generic.h
Function Documentation#
CORE_IrqIsBlocked#
bool CORE_IrqIsBlocked (IRQn_Type irqN)
Check if a specific interrupt is disabled or blocked.
[in] | irqN | The IRQn_Type enumerator for the interrupt to check. |
Returns
True if the interrupt is disabled or blocked.
669
of file platform/emlib/src/em_core.c
CORE_GetNvicEnabledMask#
void CORE_GetNvicEnabledMask (CORE_nvicMask_t * mask)
Get the current NVIC enable mask state.
[out] | mask | The current NVIC enable mask. |
737
of file platform/emlib/src/em_core.c
CORE_GetNvicMaskDisableState#
bool CORE_GetNvicMaskDisableState (const CORE_nvicMask_t * mask)
Get NVIC disable state for a given mask.
[in] | mask | An NVIC mask to check. |
Returns
True if all NVIC interrupt mask bits are clear.
754
of file platform/emlib/src/em_core.c
CORE_EnterNvicMask#
void CORE_EnterNvicMask (CORE_nvicMask_t * nvicState, const CORE_nvicMask_t * disable)
Enter a NVIC mask section.
[out] | nvicState | Return NVIC interrupts enable mask prior to section entry. |
[in] | disable | A mask specifying which NVIC interrupts to disable within the section. |
When a NVIC mask section is entered, specified NVIC interrupts are disabled.
524
of file platform/emlib/src/em_core.c
CORE_NvicDisableMask#
void CORE_NvicDisableMask (const CORE_nvicMask_t * disable)
Disable NVIC interrupts.
[in] | disable | A mask specifying which NVIC interrupts to disable. |
540
of file platform/emlib/src/em_core.c
CORE_NvicEnableMask#
void CORE_NvicEnableMask (const CORE_nvicMask_t * enable)
Set current NVIC interrupt enable mask.
[out] | enable | A mask specifying which NVIC interrupts are currently enabled. |
554
of file platform/emlib/src/em_core.c
CORE_YieldNvicMask#
void CORE_YieldNvicMask (const CORE_nvicMask_t * enable)
Brief NVIC interrupt enable/disable sequence to allow handling of pending interrupts.
[in] | enable | A mask specifying which NVIC interrupts to briefly enable. |
Note
Usually used within an NVIC mask section.
572
of file platform/emlib/src/em_core.c
CORE_NvicMaskSetIRQ#
void CORE_NvicMaskSetIRQ (IRQn_Type irqN, CORE_nvicMask_t * mask)
Utility function to set an IRQn bit in a NVIC enable/disable mask.
[in] | irqN | The IRQn_Type enumerator for the interrupt. |
[inout] | mask | The mask to set the interrupt bit in. |
624
of file platform/emlib/src/em_core.c
CORE_NvicMaskClearIRQ#
void CORE_NvicMaskClearIRQ (IRQn_Type irqN, CORE_nvicMask_t * mask)
Utility function to clear an IRQn bit in a NVIC enable/disable mask.
[in] | irqN | The IRQn_Type enumerator for the interrupt. |
[inout] | mask | The mask to clear the interrupt bit in. |
640
of file platform/emlib/src/em_core.c
CORE_NvicIRQDisabled#
bool CORE_NvicIRQDisabled (IRQn_Type irqN)
Check if an NVIC interrupt is disabled.
[in] | irqN | The IRQn_Type enumerator for the interrupt to check. |
Returns
True if the interrupt is disabled.
786
of file platform/emlib/src/em_core.c
CORE_GetNvicRamTableHandler#
void * CORE_GetNvicRamTableHandler (IRQn_Type irqN)
Utility function to get the handler for a specific interrupt.
[in] | irqN | The IRQn_Type enumerator for the interrupt. |
Returns
The handler address.
Note
Uses the interrupt vector table defined by the current VTOR register value.
809
of file platform/emlib/src/em_core.c
CORE_SetNvicRamTableHandler#
void CORE_SetNvicRamTableHandler (IRQn_Type irqN, void * handler)
Utility function to set the handler for a specific interrupt.
[in] | irqN | The IRQn_Type enumerator for the interrupt. |
[in] | handler | The handler address. |
Note
Uses the interrupt vector table defined by the current VTOR register value.
828
of file platform/emlib/src/em_core.c
CORE_InitNvicVectorTable#
void CORE_InitNvicVectorTable (uint32_t * sourceTable, uint32_t sourceSize, uint32_t * targetTable, uint32_t targetSize, void * defaultHandler, bool overwriteActive)
Initialize an interrupt vector table by copying table entries from a source to a target table.
[in] | sourceTable | The address of the source vector table. |
[in] | sourceSize | A number of entries in the source vector table. |
[in] | targetTable | The address of the target (new) vector table. |
[in] | targetSize | A number of entries in the target vector table. |
[in] | defaultHandler | An address of the interrupt handler used for target entries for which where there is no corresponding source entry (i.e., the target table is larger than the source table). |
[in] | overwriteActive | When true, a target table entry is always overwritten with the corresponding source entry. If false, a target table entry is only overwritten if it is zero. This makes it possible for an application to partly initialize a target table before passing it to this function. |
Note
This function will set a new VTOR register value.
865
of file platform/emlib/src/em_core.c
CORE_CriticalDisableIrq#
void CORE_CriticalDisableIrq (void )
Disable interrupts.
N/A |
Disable all interrupts by setting PRIMASK. (Fault exception handlers will still be enabled).
303
of file platform/emlib/src/em_core.c
CORE_CriticalEnableIrq#
void CORE_CriticalEnableIrq (void )
Enable interrupts.
N/A |
Enable interrupts by clearing PRIMASK.
314
of file platform/emlib/src/em_core.c
CORE_ExitCritical#
void CORE_ExitCritical (CORE_irqState_t irqState)
Exit a CRITICAL section.
[in] | irqState | The interrupt priority blocking level to restore to PRIMASK when exiting the CRITICAL section. This value is usually the one returned by a prior call to CORE_EnterCritical(). |
348
of file platform/emlib/src/em_core.c
CORE_YieldCritical#
void CORE_YieldCritical (void )
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
N/A |
Note
Usually used within a CRITICAL section.
364
of file platform/emlib/src/em_core.c
CORE_EnterCritical#
CORE_irqState_t CORE_EnterCritical (void )
Enter a CRITICAL section.
N/A |
When a CRITICAL section is entered, all interrupts (except fault handlers) are disabled.
Returns
The value of PRIMASK register prior to the CRITICAL section entry.
329
of file platform/emlib/src/em_core.c
CORE_AtomicDisableIrq#
void CORE_AtomicDisableIrq (void )
Disable interrupts.
N/A |
Disable interrupts with a priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL. Sets core BASEPRI register to CORE_ATOMIC_BASE_PRIORITY_LEVEL.
Note
If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK, this function is identical to CORE_CriticalDisableIrq().
385
of file platform/emlib/src/em_core.c
CORE_AtomicEnableIrq#
void CORE_AtomicEnableIrq (void )
Enable interrupts.
N/A |
Enable interrupts by setting core BASEPRI register to 0.
Note
If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_BASEPRI and PRIMASK is set (CPU is inside a CRITICAL section), interrupts will still be disabled after calling this function.
If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK, this function is identical to CORE_CriticalEnableIrq().
409
of file platform/emlib/src/em_core.c
CORE_ExitAtomic#
void CORE_ExitAtomic (CORE_irqState_t irqState)
Exit an ATOMIC section.
[in] | irqState | The interrupt priority blocking level to restore to BASEPRI when exiting the ATOMIC section. This value is usually the one returned by a prior call to CORE_EnterAtomic(). |
Note
If CORE_ATOMIC_METHOD is set to CORE_ATOMIC_METHOD_PRIMASK, this function is identical to CORE_ExitCritical().
465
of file platform/emlib/src/em_core.c
CORE_YieldAtomic#
void CORE_YieldAtomic (void )
Brief interrupt enable/disable sequence to allow handling of pending interrupts.
N/A |
Note
Usully used within an ATOMIC section.
If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK, this function is identical to CORE_YieldCritical().
493
of file platform/emlib/src/em_core.c
CORE_EnterAtomic#
CORE_irqState_t CORE_EnterAtomic (void )
Enter an ATOMIC section.
N/A |
When an ATOMIC section is entered, interrupts with priority lower or equal to CORE_ATOMIC_BASE_PRIORITY_LEVEL are disabled.
Note
If CORE_ATOMIC_METHOD is CORE_ATOMIC_METHOD_PRIMASK, this function is identical to CORE_EnterCritical().
Returns
The value of BASEPRI register prior to ATOMIC section entry.
432
of file platform/emlib/src/em_core.c
CORE_InIrqContext#
bool CORE_InIrqContext (void )
Check whether the current CPU operation mode is handler mode.
N/A |
Returns
True if the CPU is in handler mode (currently executing an interrupt handler). False if the CPU is in thread mode.
654
of file platform/emlib/src/em_core.c
CORE_IrqIsDisabled#
bool CORE_IrqIsDisabled (void )
Check if interrupts are disabled.
N/A |
Returns
True if interrupts are disabled.
718
of file platform/emlib/src/em_core.c
CORE_get_max_time_critical_section#
uint32_t CORE_get_max_time_critical_section (void )
Returns the max time spent in critical section.
N/A |
Returns
The max time spent in critical section.
Note
SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
924
of file platform/emlib/src/em_core.c
CORE_get_max_time_atomic_section#
uint32_t CORE_get_max_time_atomic_section (void )
Returns the max time spent in atomic section.
N/A |
Returns
The max time spent in atomic section.
Note
SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
938
of file platform/emlib/src/em_core.c
CORE_clear_max_time_critical_section#
void CORE_clear_max_time_critical_section (void )
Clears the max time spent in atomic section.
N/A |
Note
SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
949
of file platform/emlib/src/em_core.c
CORE_clear_max_time_atomic_section#
void CORE_clear_max_time_atomic_section (void )
Clears the max time spent in atomic section.
N/A |
Note
SL_EMLIB_CORE_ENABLE_INTERRUPT_DISABLED_TIMING must be enabled.
960
of file platform/emlib/src/em_core.c
Macro Definition Documentation#
CORE_DECLARE_IRQ_STATE#
#define CORE_DECLARE_IRQ_STATE
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
52
of file platform/emlib/host/inc/em_core_generic.h
CORE_CRITICAL_IRQ_DISABLE#
#define CORE_CRITICAL_IRQ_DISABLE
CRITICAL style interrupt disable.
55
of file platform/emlib/host/inc/em_core_generic.h
CORE_CRITICAL_IRQ_ENABLE#
#define CORE_CRITICAL_IRQ_ENABLE
CRITICAL style interrupt enable.
58
of file platform/emlib/host/inc/em_core_generic.h
CORE_CRITICAL_SECTION#
#define CORE_CRITICAL_SECTIONValue:
Convenience macro for implementing a CRITICAL section.
61
of file platform/emlib/host/inc/em_core_generic.h
CORE_ENTER_CRITICAL#
#define CORE_ENTER_CRITICAL
Enter CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
73
of file platform/emlib/host/inc/em_core_generic.h
CORE_EXIT_CRITICAL#
#define CORE_EXIT_CRITICAL
Exit CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
77
of file platform/emlib/host/inc/em_core_generic.h
CORE_YIELD_CRITICAL#
#define CORE_YIELD_CRITICAL
CRITICAL style yield.
80
of file platform/emlib/host/inc/em_core_generic.h
CORE_ATOMIC_IRQ_DISABLE#
#define CORE_ATOMIC_IRQ_DISABLE
ATOMIC style interrupt disable.
87
of file platform/emlib/host/inc/em_core_generic.h
CORE_ATOMIC_IRQ_ENABLE#
#define CORE_ATOMIC_IRQ_ENABLE
ATOMIC style interrupt enable.
90
of file platform/emlib/host/inc/em_core_generic.h
CORE_ATOMIC_SECTION#
#define CORE_ATOMIC_SECTIONValue:
Convenience macro for implementing an ATOMIC section.
93
of file platform/emlib/host/inc/em_core_generic.h
CORE_ENTER_ATOMIC#
#define CORE_ENTER_ATOMIC
Enter ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
105
of file platform/emlib/host/inc/em_core_generic.h
CORE_EXIT_ATOMIC#
#define CORE_EXIT_ATOMIC
Exit ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
109
of file platform/emlib/host/inc/em_core_generic.h
CORE_YIELD_ATOMIC#
#define CORE_YIELD_ATOMIC
ATOMIC style yield.
112
of file platform/emlib/host/inc/em_core_generic.h
CORE_NVIC_REG_WORDS#
#define CORE_NVIC_REG_WORDSValue:
((EXT_IRQ_COUNT + 31) / 32)
Number of words in a NVIC mask set.
67
of file platform/emlib/inc/em_core.h
CORE_DEFAULT_VECTOR_TABLE_ENTRIES#
#define CORE_DEFAULT_VECTOR_TABLE_ENTRIESValue:
(EXT_IRQ_COUNT + 16)
Number of entries in a default interrupt vector table.
70
of file platform/emlib/inc/em_core.h
CORE_INTERRUPT_HIGHEST_PRIORITY#
#define CORE_INTERRUPT_HIGHEST_PRIORITYValue:
0
Highest priority for core interrupt.
90
of file platform/emlib/inc/em_core.h
CORE_INTERRUPT_DEFAULT_PRIORITY#
#define CORE_INTERRUPT_DEFAULT_PRIORITYValue:
1
Default priority for core interrupt.
93
of file platform/emlib/inc/em_core.h
CORE_INTERRUPT_LOWEST_PRIORITY#
#define CORE_INTERRUPT_LOWEST_PRIORITYValue:
3
Lowest priority for core interrupt.
96
of file platform/emlib/inc/em_core.h
CORE_ATOMIC_METHOD_DEFAULT#
#define CORE_ATOMIC_METHOD_DEFAULTValue:
CORE_ATOMIC_METHOD_PRIMASK
Default method to disable interrupts in ATOMIC sections.
99
of file platform/emlib/inc/em_core.h
CORE_ATOMIC_METHOD#
#define CORE_ATOMIC_METHODValue:
CORE_ATOMIC_METHOD_PRIMASK
Specify which method to use when implementing ATOMIC sections.
You can select between BASEPRI or PRIMASK method. Note
On Cortex-M0+ devices only PRIMASK can be used.
107
of file platform/emlib/inc/em_core.h
CORE_DECLARE_NVIC_STATE#
#define CORE_DECLARE_NVIC_STATEValue:
CORE_nvicMask_t nvicState
Allocate storage for NVIC interrupt masks for use by CORE_ENTER/EXIT_NVIC() macros.
132
of file platform/emlib/inc/em_core.h
CORE_DECLARE_NVIC_MASK#
#define CORE_DECLARE_NVIC_MASKValue:
(x)
Allocate storage for NVIC interrupt masks.
137
of file platform/emlib/inc/em_core.h
CORE_DECLARE_NVIC_ZEROMASK#
#define CORE_DECLARE_NVIC_ZEROMASKValue:
(x)
Allocate storage for and zero initialize NVIC interrupt mask.
142
of file platform/emlib/inc/em_core.h
CORE_NVIC_DISABLE#
#define CORE_NVIC_DISABLEValue:
(mask)
NVIC mask style interrupt disable.
147
of file platform/emlib/inc/em_core.h
CORE_NVIC_ENABLE#
#define CORE_NVIC_ENABLEValue:
(mask)
NVIC mask style interrupt enable.
152
of file platform/emlib/inc/em_core.h
CORE_NVIC_SECTION#
#define CORE_NVIC_SECTIONValue:
Convenience macro for implementing a NVIC mask section.
159
of file platform/emlib/inc/em_core.h
CORE_ENTER_NVIC#
#define CORE_ENTER_NVICValue:
(disable)
Enter NVIC mask section.
Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.
173
of file platform/emlib/inc/em_core.h
CORE_EXIT_NVIC#
#define CORE_EXIT_NVICValue:
()
Exit NVIC mask section.
Assumes that a CORE_DECLARE_NVIC_STATE exist in scope.
177
of file platform/emlib/inc/em_core.h
CORE_YIELD_NVIC#
#define CORE_YIELD_NVICValue:
(enable)
NVIC maks style yield.
182
of file platform/emlib/inc/em_core.h
START_COUNTER#
#define START_COUNTER
Start counter.
196
of file platform/emlib/inc/em_core.h
STOP_COUNTER#
#define STOP_COUNTER
Stop counter.
198
of file platform/emlib/inc/em_core.h
CORE_ATOMIC_METHOD_PRIMASK#
#define CORE_ATOMIC_METHOD_PRIMASKValue:
0
Use PRIMASK register to disable interrupts in ATOMIC sections.
47
of file platform/emlib/inc/em_core_generic.h
CORE_ATOMIC_METHOD_BASEPRI#
#define CORE_ATOMIC_METHOD_BASEPRIValue:
1
Use BASEPRI register to disable interrupts in ATOMIC sections.
50
of file platform/emlib/inc/em_core_generic.h
CORE_ATOMIC_BASE_PRIORITY_LEVEL#
#define CORE_ATOMIC_BASE_PRIORITY_LEVELValue:
3
The interrupt priority level disabled within ATOMIC regions.
Interrupts with priority level equal to or lower than this definition will be disabled within ATOMIC regions.
56
of file platform/emlib/inc/em_core_generic.h
CORE_DECLARE_IRQ_STATE#
#define CORE_DECLARE_IRQ_STATEValue:
CORE_irqState_t irqState
Allocate storage for PRIMASK or BASEPRI value for use by CORE_ENTER/EXIT_ATOMIC() and CORE_ENTER/EXIT_CRITICAL() macros.
73
of file platform/emlib/inc/em_core_generic.h
CORE_CRITICAL_IRQ_DISABLE#
#define CORE_CRITICAL_IRQ_DISABLEValue:
()
CRITICAL style interrupt disable.
76
of file platform/emlib/inc/em_core_generic.h
CORE_CRITICAL_IRQ_ENABLE#
#define CORE_CRITICAL_IRQ_ENABLEValue:
()
CRITICAL style interrupt enable.
79
of file platform/emlib/inc/em_core_generic.h
CORE_CRITICAL_SECTION#
#define CORE_CRITICAL_SECTIONValue:
Convenience macro for implementing a CRITICAL section.
82
of file platform/emlib/inc/em_core_generic.h
CORE_ENTER_CRITICAL#
#define CORE_ENTER_CRITICALValue:
()
Enter CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
94
of file platform/emlib/inc/em_core_generic.h
CORE_EXIT_CRITICAL#
#define CORE_EXIT_CRITICALValue:
()
Exit CRITICAL section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
98
of file platform/emlib/inc/em_core_generic.h
CORE_YIELD_CRITICAL#
#define CORE_YIELD_CRITICALValue:
()
CRITICAL style yield.
101
of file platform/emlib/inc/em_core_generic.h
CORE_ATOMIC_IRQ_DISABLE#
#define CORE_ATOMIC_IRQ_DISABLEValue:
()
ATOMIC style interrupt disable.
108
of file platform/emlib/inc/em_core_generic.h
CORE_ATOMIC_IRQ_ENABLE#
#define CORE_ATOMIC_IRQ_ENABLEValue:
()
ATOMIC style interrupt enable.
111
of file platform/emlib/inc/em_core_generic.h
CORE_ATOMIC_SECTION#
#define CORE_ATOMIC_SECTIONValue:
Convenience macro for implementing an ATOMIC section.
114
of file platform/emlib/inc/em_core_generic.h
CORE_ENTER_ATOMIC#
#define CORE_ENTER_ATOMICValue:
()
Enter ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
126
of file platform/emlib/inc/em_core_generic.h
CORE_EXIT_ATOMIC#
#define CORE_EXIT_ATOMICValue:
()
Exit ATOMIC section.
Assumes that a CORE_DECLARE_IRQ_STATE exist in scope.
130
of file platform/emlib/inc/em_core_generic.h
CORE_YIELD_ATOMIC#
#define CORE_YIELD_ATOMICValue:
()
ATOMIC style yield.
133
of file platform/emlib/inc/em_core_generic.h
CORE_IRQ_DISABLED#
#define CORE_IRQ_DISABLEDValue:
()
Check if IRQ is disabled.
136
of file platform/emlib/inc/em_core_generic.h
CORE_IN_IRQ_CONTEXT#
#define CORE_IN_IRQ_CONTEXTValue:
()
Check if inside an IRQ handler.
139
of file platform/emlib/inc/em_core_generic.h
CORE_INTERRUPT_ENTRY#
#define CORE_INTERRUPT_ENTRY
Placeholder for optional interrupt handler entry code.
This might be needed when working with an RTOS.
262
of file platform/emlib/src/em_core.c
CORE_INTERRUPT_EXIT#
#define CORE_INTERRUPT_EXIT
Placeholder for optional interrupt handler exit code.
This might be needed when working with an RTOS.
268
of file platform/emlib/src/em_core.c