VB Configuration structure.
This structure is used to configure the VB voltage input source and its dividers.
Public Attributes#
VB Voltage input source.
uint32_t
A divider for VB voltage input source when ACMP output is 0.
uint32_t
A divider for VB voltage input source when ACMP output is 1.
Public Attribute Documentation#
input#
ACMP_VBInput_TypeDef ACMP_VBConfig_TypeDef::input
VB Voltage input source.
Definition at line
915
of file platform/emlib/inc/em_acmp.h
div0#
uint32_t ACMP_VBConfig_TypeDef::div0
A divider for VB voltage input source when ACMP output is 0.
This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div0 + 1) / 64
Definition at line
924
of file platform/emlib/inc/em_acmp.h
div1#
uint32_t ACMP_VBConfig_TypeDef::div1
A divider for VB voltage input source when ACMP output is 1.
This value is used to divide the VB voltage input source by a specific value. The valid range is between 0 and 63.
VB divided = VB input * (div1 + 1) / 64
Definition at line
933
of file platform/emlib/inc/em_acmp.h