Alternate excitation descriptor structure.
Public Attributes#
Configure alternate excitation pins.
Configure idle phase setup of alternate excitation pins.
Configure how to control external alternate excitation pins.
Public Attribute Documentation#
enablePin#
bool LESENSE_AltExDesc_TypeDef::enablePin
Configure alternate excitation pins.
If set, the corresponding alternate excitation pin/signal is enabled.
1175
of file platform/emlib/inc/em_lesense.h
idleConf#
LESENSE_AltExPinIdle_TypeDef LESENSE_AltExDesc_TypeDef::idleConf
Configure idle phase setup of alternate excitation pins.
The idleConf parameter is not valid when altExMap==lesenseAltExMapACMP.
1180
of file platform/emlib/inc/em_lesense.h
alwaysEx#
bool LESENSE_AltExDesc_TypeDef::alwaysEx
Configure how to control external alternate excitation pins.
Only applies if altExMap has been set to lesenseAltExMapALTEX. If true, excitation happens on the corresponding alternate excitation pin during excitation periods of all the enabled channels. If false, excitation happens on the corresponding alternate excitation pin ONLY during excitation period of the corresponding channel. The alwaysEx parameter is not valid when altExMap==lesenseAltExMapACMP.
1189
of file platform/emlib/inc/em_lesense.h