VA Configuration structure.
This structure is used to configure the VA voltage input source and its dividers.
Public Attributes#
VA voltage input source.
uint32_t
A divider for VA voltage input source when ACMP output is 0.
uint32_t
A divider for VA voltage input source when ACMP output is 1.
Public Attribute Documentation#
input#
ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input
VA voltage input source.
Definition at line
887
of file platform/emlib/inc/em_acmp.h
div0#
uint32_t ACMP_VAConfig_TypeDef::div0
A divider for VA voltage input source when ACMP output is 0.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div0 + 1) / 64
Definition at line
896
of file platform/emlib/inc/em_acmp.h
div1#
uint32_t ACMP_VAConfig_TypeDef::div1
A divider for VA voltage input source when ACMP output is 1.
This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div1 + 1) / 64
Definition at line
905
of file platform/emlib/inc/em_acmp.h