CMU - Clock Management Unit#
Clock management unit (CMU) Peripheral API.
This module contains functions for the CMU peripheral of Silicon Labs 32-bit MCUs and SoCs. The CMU module controls oscillators, clocks gates, clock multiplexers, pre-scalers, calibration modules and wait-states.
Modules#
Enumerations#
High-frequency system RCO bands.
AUX high-frequency RCO bands.
Clock points in CMU.
Oscillator types.
Selectable clock sources.
HFXO tuning modes.
DPLL reference clock selector.
DPLL reference clock edge detect selector.
DPLL lock mode selector.
Functions#
Get the AUX clock frequency.
Get the HFSRCCLK frequency.
Get the Debug Trace clock frequency.
Get the ADC n asynchronous clock frequency.
Configure flash access wait states to support the given core clock frequency.
Configure flash access wait states to the most conservative setting for this target.
Configure various wait states to switch to a certain frequency and a certain voltage scale.
Return the upper value for CMU_HFXOSTEADYSTATECTRL_REGISH.
Get the HFXO tuning mode.
Set the HFXO tuning mode.
Get the LFnCLK frequency based on the current configuration.
Wait for an ongoing sync of register(s) to low-frequency domain to complete.
Set HFPER clock tree prescalers to safe values.
Set HFPER clock tree prescalers to give highest possible clock node frequency while still beeing within spec.
Get the AUXHFRCO frequency calibration word in DEVINFO.
Get the current AUXHFRCO frequency.
Set AUXHFRCO calibration for the selected target frequency.
Calibrate the clock.
Configure the clock calibration.
Get the calibration count register.
Get the clock divisor/prescaler.
Set the clock divisor/prescaler.
Enable/disable a clock.
Get the clock frequency for a clock point.
Get the clock prescaler.
Set the clock prescaler.
Get the currently selected reference clock used for a clock branch.
Select the reference clock/oscillator used for a clock branch.
Gets the precision (in PPM) of the specified low frequency clock branch.
Gets the precision (in PPM) of the specified high frequency clock branch.
Lock the DPLL to a given frequency.
CMU low frequency register synchronization freeze control.
Get the HFRCO frequency calibration word in DEVINFO.
Get the current HFRCO frequency.
Set the HFRCO calibration for the selected target frequency.
Enable or disable HFXO autostart.
Set HFXO control registers.
Get the LCD framerate divisor (FDIV) setting.
Set the LCD framerate divisor (FDIV) setting.
Set LFXO control registers.
Sets LFXO's crystal precision, in PPM.
Gets LFXO's crystal precision, in PPM.
Sets HFXO's crystal precision, in PPM.
Gets HFXO's crystal precision, in PPM.
Enable/disable oscillator.
Get the oscillator frequency tuning setting.
Set the oscillator frequency tuning control.
Wait for the oscillator tuning optimization.
Start and optionally wait for the oscillator tuning optimization.
Determine if the currently selected PCNTn clock used is external or LFBCLK.
Select the PCNTn clock.
Configure continuous calibration mode.
Start calibration.
Stop the calibration counters.
Convert divider to logarithmic value.
Unlock DPLL.
Clear one or more pending CMU interrupts.
Disable one or more CMU interrupts.
Enable one or more CMU interrupts.
Get pending CMU interrupts.
Get enabled and pending CMU interrupt flags.
Set one or more pending CMU interrupts.
Lock the CMU to protect some of its registers against unintended modification.
Unlock the CMU so that writing to locked registers again is possible.
Convert prescaler divider to a logarithmic value.
Macros#
Macro to set clock sources in the clock tree.
Clock divisors.
Divide clock by 2.
Divide clock by 4.
Divide clock by 8.
Divide clock by 16.
Divide clock by 32.
Divide clock by 64.
Divide clock by 128.
Divide clock by 256.
Divide clock by 512.
Divide clock by 1024.
Divide clock by 2048.
Divide clock by 4096.
Divide clock by 8192.
Divide clock by 16384.
Divide clock by 32768.
HFRCO minimum frequency.
HFRCO maximum frequency.
AUXHFRCO minimum frequency.
AUXHFRCO maximum frequency.
Default LFXO initialization values.
Default LFXO initialization for external clock.
Default HFXO initialization values for Platform 2 devices, which contain a separate HFXOCTRL register.
Init of HFXO with external clock.
DPLL initialization values for 39,998,805 Hz using LFXO as reference clock, M=2 and N=3661.
Enumeration Documentation#
CMU_HFRCOFreq_TypeDef#
CMU_HFRCOFreq_TypeDef
High-frequency system RCO bands.
Enumerator | |
---|---|
cmuHFRCOFreq_1M0Hz | 1 MHz RC band |
cmuHFRCOFreq_2M0Hz | 2 MHz RC band |
cmuHFRCOFreq_4M0Hz | 4 MHz RC band |
cmuHFRCOFreq_7M0Hz | 7 MHz RC band |
cmuHFRCOFreq_13M0Hz | 13 MHz RC band |
cmuHFRCOFreq_16M0Hz | 16 MHz RC band |
cmuHFRCOFreq_19M0Hz | 19 MHz RC band |
cmuHFRCOFreq_26M0Hz | 26 MHz RC band |
cmuHFRCOFreq_32M0Hz | 32 MHz RC band |
cmuHFRCOFreq_38M0Hz | 38 MHz RC band |
cmuHFRCOFreq_UserDefined |
1900
of file platform/emlib/inc/em_cmu.h
CMU_AUXHFRCOFreq_TypeDef#
CMU_AUXHFRCOFreq_TypeDef
AUX high-frequency RCO bands.
Enumerator | |
---|---|
cmuAUXHFRCOFreq_1M0Hz | 1 MHz RC band |
cmuAUXHFRCOFreq_2M0Hz | 2 MHz RC band |
cmuAUXHFRCOFreq_4M0Hz | 4 MHz RC band |
cmuAUXHFRCOFreq_7M0Hz | 7 MHz RC band |
cmuAUXHFRCOFreq_13M0Hz | 13 MHz RC band |
cmuAUXHFRCOFreq_16M0Hz | 16 MHz RC band |
cmuAUXHFRCOFreq_19M0Hz | 19 MHz RC band |
cmuAUXHFRCOFreq_26M0Hz | 26 MHz RC band |
cmuAUXHFRCOFreq_32M0Hz | 32 MHz RC band |
cmuAUXHFRCOFreq_38M0Hz | 38 MHz RC band |
cmuAUXHFRCOFreq_UserDefined |
1948
of file platform/emlib/inc/em_cmu.h
CMU_Clock_TypeDef#
CMU_Clock_TypeDef
Clock points in CMU.
See CMU overview in the reference manual.
Enumerator | |
---|---|
cmuClock_HF | High-frequency clock. |
cmuClock_DBG | Debug clock. |
cmuClock_AUX | AUX clock. |
cmuClock_EXPORT | Export clock. |
cmuClock_BUS | High-frequency bus clock. |
cmuClock_CRYPTO | Cryptography accelerator clock. |
cmuClock_CRYPTO0 | Cryptography accelerator 0 clock. |
cmuClock_CRYPTO1 | Cryptography accelerator 1 clock. |
cmuClock_LDMA | Direct-memory access controller clock. |
cmuClock_GPCRC | General-purpose cyclic redundancy checksum clock. |
cmuClock_GPIO | General-purpose input/output clock. |
cmuClock_HFLE | Low-energy clock divided down from HFCLK. |
cmuClock_PRS | Peripheral reflex system clock. |
cmuClock_HFPER | High-frequency peripheral clock. |
cmuClock_USART0 | Universal sync/async receiver/transmitter 0 clock. |
cmuClock_USART1 | Universal sync/async receiver/transmitter 1 clock. |
cmuClock_USART2 | Universal sync/async receiver/transmitter 2 clock. |
cmuClock_USART3 | Universal sync/async receiver/transmitter 3 clock. |
cmuClock_TIMER0 | Timer 0 clock. |
cmuClock_TIMER1 | Timer 1 clock. |
cmuClock_WTIMER0 | Wide-timer 0 clock. |
cmuClock_WTIMER1 | Wide-timer 1 clock. |
cmuClock_CRYOTIMER | CRYOtimer clock. |
cmuClock_ACMP0 | Analog comparator 0 clock. |
cmuClock_ACMP1 | Analog comparator 1 clock. |
cmuClock_VDAC0 | Voltage digital-to-analog converter 0 clock. |
cmuClock_IDAC0 | Current digital-to-analog converter 0 clock. |
cmuClock_ADC0 | Analog-to-digital converter 0 clock. |
cmuClock_I2C0 | I2C 0 clock. |
cmuClock_I2C1 | I2C 1 clock. |
cmuClock_CSEN_HF | Capacitive Sense HF clock. |
cmuClock_TRNG0 | True random number generator clock. |
cmuClock_CORE | Core clock. |
cmuClock_LFA | Low-frequency A clock. |
cmuClock_LETIMER0 | Low-energy timer 0 clock. |
cmuClock_PCNT0 | Pulse counter 0 clock. |
cmuClock_PCNT1 | Pulse counter 1 clock. |
cmuClock_PCNT2 | Pulse counter 2 clock. |
cmuClock_LESENSE | LESENSE clock. |
cmuClock_LFB | Low-frequency B clock. |
cmuClock_LEUART0 | Low-energy universal asynchronous receiver/transmitter 0 clock. |
cmuClock_CSEN_LF | Capacitive Sense LF clock. |
cmuClock_SYSTICK | Cortex SYSTICK LF clock. |
cmuClock_LFE | Low-frequency E clock. |
cmuClock_RTCC | Real-time counter and calendar clock. |
cmuClock_ADC0ASYNC | ADC0 asynchronous clock. |
1982
of file platform/emlib/inc/em_cmu.h
CMU_Osc_TypeDef#
CMU_Osc_TypeDef
Oscillator types.
Enumerator | |
---|---|
cmuOsc_LFXO | Low-frequency crystal oscillator. |
cmuOsc_LFRCO | Low-frequency RC oscillator. |
cmuOsc_HFXO | High-frequency crystal oscillator. |
cmuOsc_HFRCO | High-frequency RC oscillator. |
cmuOsc_AUXHFRCO | Auxiliary high-frequency RC oscillator. |
cmuOsc_ULFRCO | Ultra low-frequency RC oscillator. |
cmuOsc_CLKIN0 | External oscillator. |
2976
of file platform/emlib/inc/em_cmu.h
CMU_OscMode_TypeDef#
CMU_OscMode_TypeDef
Oscillator modes.
Enumerator | |
---|---|
cmuOscMode_Crystal | Crystal oscillator. |
cmuOscMode_AcCoupled | AC-coupled buffer. |
cmuOscMode_External | External digital clock. |
2997
of file platform/emlib/inc/em_cmu.h
CMU_Select_TypeDef#
CMU_Select_TypeDef
Selectable clock sources.
Enumerator | |
---|---|
cmuSelect_Error | Usage error. |
cmuSelect_Disabled | Clock selector disabled. |
cmuSelect_LFXO | Low-frequency crystal oscillator. |
cmuSelect_LFRCO | Low-frequency RC oscillator. |
cmuSelect_HFXO | High-frequency crystal oscillator. |
cmuSelect_HFRCO | High-frequency RC oscillator. |
cmuSelect_HFCLKLE | High-frequency LE clock divided by 2 or 4. |
cmuSelect_AUXHFRCO | Auxiliary clock source can be used for debug clock. |
cmuSelect_HFSRCCLK | High-frequency source clock. |
cmuSelect_HFCLK | Divided HFCLK on Giant for debug clock, undivided on Tiny Gecko and for USBC (not used on Gecko). |
cmuSelect_ULFRCO | Ultra low-frequency RC oscillator. |
cmuSelect_HFRCODIV2 | High-frequency RC oscillator divided by 2. |
cmuSelect_CLKIN0 | External clock input. |
3004
of file platform/emlib/inc/em_cmu.h
CMU_HFXOTuningMode_TypeDef#
CMU_HFXOTuningMode_TypeDef
HFXO tuning modes.
Enumerator | |
---|---|
cmuHFXOTuningMode_Auto | |
cmuHFXOTuningMode_PeakDetectCommand | Run peak detect optimization only. |
cmuHFXOTuningMode_ShuntCommand | Run shunt current optimization only. |
cmuHFXOTuningMode_PeakShuntCommand | Run peak and shunt current optimization. |
3048
of file platform/emlib/inc/em_cmu.h
CMU_DPLLClkSel_TypeDef#
CMU_DPLLClkSel_TypeDef
DPLL reference clock selector.
Enumerator | |
---|---|
cmuDPLLClkSel_Hfxo | HFXO is DPLL reference clock. |
cmuDPLLClkSel_Lfxo | LFXO is DPLL reference clock. |
cmuDPLLClkSel_Clkin0 | CLKIN0 is DPLL reference clock. |
3073
of file platform/emlib/inc/em_cmu.h
CMU_DPLLEdgeSel_TypeDef#
CMU_DPLLEdgeSel_TypeDef
DPLL reference clock edge detect selector.
Enumerator | |
---|---|
cmuDPLLEdgeSel_Fall | Detect falling edge of reference clock. |
cmuDPLLEdgeSel_Rise | Detect rising edge of reference clock. |
3080
of file platform/emlib/inc/em_cmu.h
CMU_DPLLLockMode_TypeDef#
CMU_DPLLLockMode_TypeDef
DPLL lock mode selector.
Enumerator | |
---|---|
cmuDPLLLockMode_Freq | Frequency lock mode. |
cmuDPLLLockMode_Phase | Phase lock mode. |
3086
of file platform/emlib/inc/em_cmu.h
Typedef Documentation#
CMU_ClkDiv_TypeDef#
typedef uint32_t CMU_ClkDiv_TypeDef
Clock divider configuration.
1838
of file platform/emlib/inc/em_cmu.h
CMU_ClkPresc_TypeDef#
typedef uint32_t CMU_ClkPresc_TypeDef
Clockprescaler configuration.
1842
of file platform/emlib/inc/em_cmu.h
Function Documentation#
auxClkGet#
static uint32_t auxClkGet (void )
Get the AUX clock frequency.
N/A |
Used by MSC flash programming and LESENSE, by default also as a debug clock.
Returns
AUX Frequency in Hz.
5742
of file platform/emlib/src/em_cmu.c
hfSrcClkGet#
static uint32_t hfSrcClkGet (void )
Get the HFSRCCLK frequency.
N/A |
Returns
HFSRCCLK Frequency in Hz.
5810
of file platform/emlib/src/em_cmu.c
dbgClkGet#
static uint32_t dbgClkGet (void )
Get the Debug Trace clock frequency.
N/A |
Returns
Debug Trace frequency in Hz.
5827
of file platform/emlib/src/em_cmu.c
adcAsyncClkGet#
static uint32_t adcAsyncClkGet (uint32_t adc)
Get the ADC n asynchronous clock frequency.
N/A | adc |
Returns
ADC n asynchronous frequency in Hz.
5860
of file platform/emlib/src/em_cmu.c
flashWaitStateControl#
static void flashWaitStateControl (uint32_t coreFreq, int vscale)
Configure flash access wait states to support the given core clock frequency.
[in] | coreFreq | The core clock frequency to configure flash wait-states. |
[in] | vscale | Voltage Scale level. Supported levels are 0 and 2 where 0 is the default. |
6098
of file platform/emlib/src/em_cmu.c
flashWaitStateMax#
static void flashWaitStateMax (void )
Configure flash access wait states to the most conservative setting for this target.
N/A |
Retain SCBTP (Suppressed Conditional Branch Target Prefetch) setting.
6207
of file platform/emlib/src/em_cmu.c
CMU_UpdateWaitStates#
void CMU_UpdateWaitStates (uint32_t freq, int vscale)
Configure various wait states to switch to a certain frequency and a certain voltage scale.
[in] | freq | The core clock frequency to configure wait-states. |
[in] | vscale | The voltage scale to configure wait-states. Expected values are 0 or 2, higher number is lower voltage. |
This function will set up the necessary flash, bus, and RAM wait states. Updating the wait state configuration must be done before increasing the clock frequency and it must be done after decreasing the clock frequency. Updating the wait state configuration must be done before core voltage is decreased and it must be done after a core voltage is increased.
0 = 1.2 V (VSCALE2)
2 = 1.0 V (VSCALE0)
6316
of file platform/emlib/src/em_cmu.c
getRegIshUpperVal#
static uint32_t getRegIshUpperVal (uint32_t steadyStateRegIsh)
Return the upper value for CMU_HFXOSTEADYSTATECTRL_REGISH.
N/A | steadyStateRegIsh |
6340
of file platform/emlib/src/em_cmu.c
getHfxoTuningMode#
uint32_t getHfxoTuningMode (void )
Get the HFXO tuning mode.
N/A |
Returns
The current HFXO tuning mode from the HFXOCTRL register.
6360
of file platform/emlib/src/em_cmu.c
setHfxoTuningMode#
void setHfxoTuningMode (uint32_t mode)
Set the HFXO tuning mode.
[in] | mode | The new HFXO tuning mode. This can be HFXO_TUNING_MODE_AUTO or HFXO_TUNING_MODE_CMD. |
6379
of file platform/emlib/src/em_cmu.c
lfClkGet#
static uint32_t lfClkGet (CMU_Clock_TypeDef lfClkBranch)
Get the LFnCLK frequency based on the current configuration.
[in] | lfClkBranch | Selected LF branch. |
Returns
The LFnCLK frequency in Hz. If no LFnCLK is selected (disabled), 0 is returned.
6402
of file platform/emlib/src/em_cmu.c
syncReg#
void syncReg (uint32_t mask)
Wait for an ongoing sync of register(s) to low-frequency domain to complete.
[in] | mask | A bitmask corresponding to SYNCBUSY register defined bits, indicating registers that must complete any ongoing synchronization. |
6564
of file platform/emlib/src/em_cmu.c
hfperClkSafePrescaler#
static void hfperClkSafePrescaler (void )
Set HFPER clock tree prescalers to safe values.
N/A |
Note
This function applies to EFM32GG11B. There are 3 HFPER clock trees with these frequency limits: HFPERCLK (A-tree): 20MHz in VSCALE0 mode, 50MHz in VSCALE2 mode. HFPERBCLK (B-tree): 20MHz in VSCALE0 mode, 72MHz in VSCALE2 mode. HFPERCCLK (C-tree): 20MHz in VSCALE0 mode, 50MHz in VSCALE2 mode.
6629
of file platform/emlib/src/em_cmu.c
hfperClkOptimizedPrescaler#
static void hfperClkOptimizedPrescaler (void )
Set HFPER clock tree prescalers to give highest possible clock node frequency while still beeing within spec.
N/A |
Note
This function applies to EFM32GG11B. There are 3 HFPER clock trees with these frequency limits: HFPERCLK (A-tree): 20MHz in VSCALE0 mode, 50MHz in VSCALE2 mode. HFPERBCLK (B-tree): 20MHz in VSCALE0 mode, 72MHz in VSCALE2 mode. HFPERCCLK (C-tree): 20MHz in VSCALE0 mode, 50MHz in VSCALE2 mode.
6652
of file platform/emlib/src/em_cmu.c
CMU_AUXHFRCODevinfoGet#
static uint32_t CMU_AUXHFRCODevinfoGet (CMU_AUXHFRCOFreq_TypeDef freq)
Get the AUXHFRCO frequency calibration word in DEVINFO.
[in] | freq | Frequency in Hz. |
Returns
AUXHFRCO calibration word for a given frequency.
6777
of file platform/emlib/src/em_cmu.c
CMU_AUXHFRCOBandGet#
CMU_AUXHFRCOFreq_TypeDef CMU_AUXHFRCOBandGet (void )
Get the current AUXHFRCO frequency.
N/A |
Returns
AUXHFRCO frequency.
6830
of file platform/emlib/src/em_cmu.c
CMU_AUXHFRCOBandSet#
void CMU_AUXHFRCOBandSet (CMU_AUXHFRCOFreq_TypeDef setFreq)
Set AUXHFRCO calibration for the selected target frequency.
[in] | setFreq | AUXHFRCO frequency to set |
6844
of file platform/emlib/src/em_cmu.c
CMU_Calibrate#
uint32_t CMU_Calibrate (uint32_t HFCycles, CMU_Osc_TypeDef reference)
Calibrate the clock.
[in] | HFCycles | The number of HFCLK cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. |
[in] | reference | The reference clock used to compare HFCLK. |
Run a calibration for HFCLK against a selectable reference clock. See the reference manual, CMU chapter, for more details.
Note
This function will not return until the calibration measurement is completed.
Returns
The number of ticks the reference clock after HFCycles ticks on the HF clock.
6905
of file platform/emlib/src/em_cmu.c
CMU_CalibrateConfig#
void CMU_CalibrateConfig (uint32_t downCycles, CMU_Osc_TypeDef downSel, CMU_Osc_TypeDef upSel)
Configure the clock calibration.
[in] | downCycles | The number of downSel clock cycles to run the calibration. Increasing this number increases precision but the calibration will take more time. |
[in] | downSel | The clock, which will be counted down downCycles. |
[in] | upSel | The reference clock; the number of cycles generated by this clock will be counted and added up and the result can be given with the CMU_CalibrateCountGet() function call. |
Configure a calibration for a selectable clock source against another selectable reference clock. See the reference manual, CMU chapter, for more details.
Note
After configuration, a call to CMU_CalibrateStart() is required and the resulting calibration value can be read out with the CMU_CalibrateCountGet() function call.
6994
of file platform/emlib/src/em_cmu.c
CMU_CalibrateCountGet#
uint32_t CMU_CalibrateCountGet (void )
Get the calibration count register.
N/A |
Note
If continuous calibration mode is active, calibration busy will almost always be off and only the value needs to be read. In a normal case, this function call is triggered by the CALRDY interrupt flag.
Returns
The calibration count, the number of UPSEL clocks in the period of DOWNSEL oscillator clock cycles configured by a previous write operation to CMU->CALCNT.
7102
of file platform/emlib/src/em_cmu.c
CMU_ClockDivGet#
CMU_ClkDiv_TypeDef CMU_ClockDivGet (CMU_Clock_TypeDef clock)
Get the clock divisor/prescaler.
[in] | clock | A clock point to get the divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual. |
Returns
The current clock point divisor/prescaler. 1 is returned if
clock
specifies a clock point without a divisor/prescaler.
7137
of file platform/emlib/src/em_cmu.c
CMU_ClockDivSet#
void CMU_ClockDivSet (CMU_Clock_TypeDef clock, CMU_ClkDiv_TypeDef div)
Set the clock divisor/prescaler.
[in] | clock | Clock point to set divisor/prescaler for. Notice that not all clock points have a divisor/prescaler. See the CMU overview in the reference manual. |
[in] | div | The clock divisor to use (<= cmuClkDiv_512). |
Note
If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
7277
of file platform/emlib/src/em_cmu.c
CMU_ClockEnable#
void CMU_ClockEnable (CMU_Clock_TypeDef clock, bool enable)
Enable/disable a clock.
[in] | clock | The clock to enable/disable. Notice that not all defined clock points have separate enable/disable control. See the CMU overview in the reference manual. |
[in] | enable |
|
In general, module clocking is disabled after a reset. If a module clock is disabled, the registers of that module are not accessible and reading from such registers may return undefined values. Writing to registers of clock-disabled modules has no effect. Avoid accessing module registers of a module with a disabled clock.
Note
If enabling/disabling an LF clock, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
7502
of file platform/emlib/src/em_cmu.c
CMU_ClockFreqGet#
uint32_t CMU_ClockFreqGet (CMU_Clock_TypeDef clock)
Get the clock frequency for a clock point.
[in] | clock | A clock point to fetch the frequency for. |
Returns
The current frequency in Hz.
7626
of file platform/emlib/src/em_cmu.c
CMU_ClockPrescGet#
uint32_t CMU_ClockPrescGet (CMU_Clock_TypeDef clock)
Get the clock prescaler.
[in] | clock | A clock point to get the prescaler for. Notice that not all clock points have a prescaler. See the CMU overview in the reference manual. |
Returns
The prescaler value of the current clock point. 0 is returned if
clock
specifies a clock point without a prescaler.
7924
of file platform/emlib/src/em_cmu.c
CMU_ClockPrescSet#
void CMU_ClockPrescSet (CMU_Clock_TypeDef clock, CMU_ClkPresc_TypeDef presc)
Set the clock prescaler.
[in] | clock | A clock point to set the prescaler for. Notice that not all clock points have a prescaler. See the CMU overview in the reference manual. |
[in] | presc | The clock prescaler. The prescaler value is linked to the clock divider by: divider = 'presc' + 1. |
Note
If setting an LF clock prescaler, synchronization into the low-frequency domain is required. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. See CMU_FreezeEnable() for a suggestion on how to reduce the stalling time in some use cases.
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
8139
of file platform/emlib/src/em_cmu.c
CMU_ClockSelectGet#
CMU_Select_TypeDef CMU_ClockSelectGet (CMU_Clock_TypeDef clock)
Get the currently selected reference clock used for a clock branch.
[in] | clock | Clock branch to fetch selected ref. clock for. One of: |
Returns
The reference clock used for clocking the selected branch, cmuSelect_Error if invalid
clock
provided.
8477
of file platform/emlib/src/em_cmu.c
CMU_ClockSelectSet#
void CMU_ClockSelectSet (CMU_Clock_TypeDef clock, CMU_Select_TypeDef ref)
Select the reference clock/oscillator used for a clock branch.
[in] | clock | A clock branch to select reference clock for. One of: |
[in] | ref | A reference selected for clocking. See the reference manual for details about references available for a specific clock branch. |
Notice that if a selected reference is not enabled prior to selecting its use, it will be enabled and this function will wait for the selected oscillator to be stable. It will however NOT be disabled if another reference clock is selected later.
This feature is particularly important if selecting a new reference clock for the clock branch clocking the core. Otherwise, the system may halt.
Note
HFCLKLE prescaler is automatically modified when peripherals with clock domain HFBUSCLK is chosen based on the maximum HFLE frequency allowed.
9393
of file platform/emlib/src/em_cmu.c
CMU_LF_ClockPrecisionGet#
uint16_t CMU_LF_ClockPrecisionGet (CMU_Clock_TypeDef clock)
Gets the precision (in PPM) of the specified low frequency clock branch.
[in] | clock | Clock branch. |
Returns
Precision, in PPM, of the specified clock branch.
Note
This function is only for internal usage.
The current implementation of this function is used to determine if the clock has a precision <= 500 ppm or not (which is the minimum required for BLE). Future version of this function should provide more accurate precision numbers to allow for further optimizations from the stacks.
10117
of file platform/emlib/src/em_cmu.c
CMU_HF_ClockPrecisionGet#
uint16_t CMU_HF_ClockPrecisionGet (CMU_Clock_TypeDef clock)
Gets the precision (in PPM) of the specified high frequency clock branch.
[in] | clock | Clock branch. |
Returns
Precision, in PPM, of the specified clock branch.
Note
This function is only for internal usage.
The current implementation of this function is used to determine if the clock has a precision <= 500 ppm or not (which is the minimum required for BLE). Future version of this function should provide more accurate precision numbers to allow for further optimizations from the stacks.
10160
of file platform/emlib/src/em_cmu.c
CMU_DPLLLock#
bool CMU_DPLLLock (const CMU_DPLLInit_TypeDef * init)
Lock the DPLL to a given frequency.
[in] | init | DPLL setup parameters. |
The frequency is given by: Fout = Fref * (N+1) / (M+1).
Note
This function does not check if the given N & M values will actually produce the desired target frequency.
N & M limitations:
300 < N <= 4095
0 <= M <= 4095
Any peripheral running off HFRCO should be switched to HFRCODIV2 prior to calling this function to avoid over-clocking.
HFCLKLE prescaler is automatically modified before updating HFRCO based on the maximum HFLE frequency allowed.
Returns
Returns false on invalid target frequency or DPLL locking error.
10207
of file platform/emlib/src/em_cmu.c
CMU_FreezeEnable#
void CMU_FreezeEnable (bool enable)
CMU low frequency register synchronization freeze control.
[in] | enable |
|
Some CMU registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several such registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).
Another use case for this feature is using an API (such as the CMU API) for modifying several bit fields consecutively in the same register. If freeze mode is enabled during this sequence, stalling can be avoided.
Note
When enabling freeze mode, this function will wait for all current ongoing CMU synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling.
10363
of file platform/emlib/src/em_cmu.c
CMU_HFRCODevinfoGet#
static uint32_t CMU_HFRCODevinfoGet (CMU_HFRCOFreq_TypeDef freq)
Get the HFRCO frequency calibration word in DEVINFO.
[in] | freq | Frequency in Hz. |
Returns
HFRCO calibration word for a given frequency.
10493
of file platform/emlib/src/em_cmu.c
CMU_HFRCOBandGet#
CMU_HFRCOFreq_TypeDef CMU_HFRCOBandGet (void )
Get the current HFRCO frequency.
N/A |
Returns
HFRCO frequency.
10555
of file platform/emlib/src/em_cmu.c
CMU_HFRCOBandSet#
void CMU_HFRCOBandSet (CMU_HFRCOFreq_TypeDef setFreq)
Set the HFRCO calibration for the selected target frequency.
[in] | setFreq | HFRCO frequency to set. |
Note
HFCLKLE prescaler is automatically modified based on the maximum HFLE frequency allowed.
10571
of file platform/emlib/src/em_cmu.c
CMU_HFXOAutostartEnable#
void CMU_HFXOAutostartEnable (uint32_t userSel, bool enEM0EM1Start, bool enEM0EM1StartSel)
Enable or disable HFXO autostart.
[in] | userSel | Additional user specified enable bit. |
[in] | enEM0EM1Start | If true, HFXO is automatically started upon entering EM0/EM1 entry from EM2/EM3. HFXO selection has to be handled by the user. If false, HFXO is not started automatically when entering EM0/EM1. |
[in] | enEM0EM1StartSel | If true, HFXO is automatically started and immediately selected upon entering EM0/EM1 entry from EM2/EM3. Note that this option stalls the use of HFSRCCLK until HFXO becomes ready. HFCLKLE prescaler is also automatically modified if userSel is specified. If false, HFXO is not started or selected automatically when entering EM0/EM1. |
10799
of file platform/emlib/src/em_cmu.c
CMU_HFXOInit#
void CMU_HFXOInit (const CMU_HFXOInit_TypeDef * hfxoInit)
Set HFXO control registers.
[in] | hfxoInit | HFXO setup parameters. |
Note
HFXO configuration should be obtained from a configuration tool, app note, or crystal data sheet. This function disables the HFXO to ensure a valid state before update.
10864
of file platform/emlib/src/em_cmu.c
CMU_LCDClkFDIVGet#
uint32_t CMU_LCDClkFDIVGet (void )
Get the LCD framerate divisor (FDIV) setting.
N/A |
Returns
The LCD framerate divisor.
10996
of file platform/emlib/src/em_cmu.c
CMU_LCDClkFDIVSet#
void CMU_LCDClkFDIVSet (uint32_t div)
Set the LCD framerate divisor (FDIV) setting.
[in] | div | The FDIV setting to use. |
Note
The FDIV field (CMU LCDCTRL register) should only be modified while the LCD module is clock disabled (CMU LFACLKEN0.LCD bit is 0). This function will NOT modify FDIV if the LCD module clock is enabled. See CMU_ClockEnable() for disabling/enabling LCD clock.
11018
of file platform/emlib/src/em_cmu.c
CMU_LFXOInit#
void CMU_LFXOInit (const CMU_LFXOInit_TypeDef * lfxoInit)
Set LFXO control registers.
[in] | lfxoInit | LFXO setup parameters. |
Note
LFXO configuration should be obtained from a configuration tool, app note, or crystal data sheet. This function disables the LFXO when necessary to ensure a valid state before update.
11048
of file platform/emlib/src/em_cmu.c
CMU_LFXOPrecisionSet#
void CMU_LFXOPrecisionSet (uint16_t precision)
Sets LFXO's crystal precision, in PPM.
[in] | precision | LFXO's crystal precision, in PPM. |
Note
LFXO precision should be obtained from a crystal datasheet.
11101
of file platform/emlib/src/em_cmu.c
CMU_LFXOPrecisionGet#
uint16_t CMU_LFXOPrecisionGet (void )
Gets LFXO's crystal precision, in PPM.
[in] | LFXO's crystal precision, in PPM. |
11113
of file platform/emlib/src/em_cmu.c
CMU_HFXOPrecisionSet#
void CMU_HFXOPrecisionSet (uint16_t precision)
Sets HFXO's crystal precision, in PPM.
[in] | precision | HFXO's crystal precision, in PPM. |
Note
HFXO precision should be obtained from a crystal datasheet.
11128
of file platform/emlib/src/em_cmu.c
CMU_HFXOPrecisionGet#
uint16_t CMU_HFXOPrecisionGet (void )
Gets HFXO's crystal precision, in PPM.
[in] | HFXO's crystal precision, in PPM. |
11140
of file platform/emlib/src/em_cmu.c
CMU_OscillatorEnable#
void CMU_OscillatorEnable (CMU_Osc_TypeDef osc, bool enable, bool wait)
Enable/disable oscillator.
[in] | osc | The oscillator to enable/disable. |
[in] | enable |
|
[in] | wait | Only used if
|
Note
WARNING: When this function is called to disable either cmuOsc_LFXO or cmuOsc_HFXO, the LFXOMODE or HFXOMODE fields of the CMU_CTRL register are reset to the reset value. In other words, if external clock sources are selected in either LFXOMODE or HFXOMODE fields, the configuration will be cleared and needs to be reconfigured if needed later.
11169
of file platform/emlib/src/em_cmu.c
CMU_OscillatorTuningGet#
uint32_t CMU_OscillatorTuningGet (CMU_Osc_TypeDef osc)
Get the oscillator frequency tuning setting.
[in] | osc | An oscillator to get tuning value for, one of the following:
|
Returns
The oscillator frequency tuning setting in use.
11358
of file platform/emlib/src/em_cmu.c
CMU_OscillatorTuningSet#
void CMU_OscillatorTuningSet (CMU_Osc_TypeDef osc, uint32_t val)
Set the oscillator frequency tuning control.
[in] | osc | An oscillator to set tuning value for, one of the following:
|
[in] | val | The oscillator frequency tuning setting to use. |
Note
Oscillator tuning is done during production and the tuning value is automatically loaded after reset. Changing the tuning value from the calibrated value is for more advanced use. Certain oscillators also have build-in tuning optimization.
11432
of file platform/emlib/src/em_cmu.c
CMU_OscillatorTuningWait#
bool CMU_OscillatorTuningWait (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode)
Wait for the oscillator tuning optimization.
[in] | osc | An oscillator to set tuning value for, one of the following: |
[in] | mode | Tuning optimization mode. |
Returns
Returns false on invalid parameters or oscillator error status.
11561
of file platform/emlib/src/em_cmu.c
CMU_OscillatorTuningOptimize#
bool CMU_OscillatorTuningOptimize (CMU_Osc_TypeDef osc, CMU_HFXOTuningMode_TypeDef mode, bool wait)
Start and optionally wait for the oscillator tuning optimization.
[in] | osc | An oscillator to set tuning value for, one of the following: |
[in] | mode | Tuning optimization mode. |
[in] | wait | Wait for tuning optimization to complete. true - wait for tuning optimization to complete. false - return without waiting. |
Returns
Returns false on invalid parameters or oscillator error status.
11627
of file platform/emlib/src/em_cmu.c
CMU_PCNTClockExternalGet#
bool CMU_PCNTClockExternalGet (unsigned int instance)
Determine if the currently selected PCNTn clock used is external or LFBCLK.
[in] | instance | PCNT instance number to get currently selected clock source for. |
Returns
true - selected clock is external clock.
false - selected clock is LFBCLK.
11664
of file platform/emlib/src/em_cmu.c
CMU_PCNTClockExternalSet#
void CMU_PCNTClockExternalSet (unsigned int instance, bool external)
Select the PCNTn clock.
[in] | instance | PCNT instance number to set selected clock source for. |
[in] | external | Set to true to select the external clock, false to select LFBCLK. |
11704
of file platform/emlib/src/em_cmu.c
CMU_CalibrateCont#
void CMU_CalibrateCont (bool enable)
Configure continuous calibration mode.
[in] | enable | If true, enables continuous calibration, if false disables continuous calibration. |
3429
of file platform/emlib/inc/em_cmu.h
CMU_CalibrateStart#
void CMU_CalibrateStart (void )
Start calibration.
N/A |
Note
This call is usually invoked after CMU_CalibrateConfig() and possibly CMU_CalibrateCont().
3442
of file platform/emlib/inc/em_cmu.h
CMU_CalibrateStop#
void CMU_CalibrateStop (void )
Stop the calibration counters.
N/A |
3452
of file platform/emlib/inc/em_cmu.h
CMU_DivToLog2#
uint32_t CMU_DivToLog2 (CMU_ClkDiv_TypeDef div)
Convert divider to logarithmic value.
[in] | div | An unscaled divider. |
It only works for even numbers equal to 2^n.
Returns
Logarithm base 2 (binary) value, i.e. exponent as used by fixed 2^n prescalers.
3470
of file platform/emlib/inc/em_cmu.h
CMU_DPLLUnlock#
void CMU_DPLLUnlock (void )
Unlock DPLL.
N/A |
Note
HFRCO is not turned off.
3490
of file platform/emlib/inc/em_cmu.h
CMU_IntClear#
void CMU_IntClear (uint32_t flags)
Clear one or more pending CMU interrupts.
[in] | flags | CMU interrupt sources to clear. |
3503
of file platform/emlib/inc/em_cmu.h
CMU_IntDisable#
void CMU_IntDisable (uint32_t flags)
Disable one or more CMU interrupts.
[in] | flags | CMU interrupt sources to disable. |
3515
of file platform/emlib/inc/em_cmu.h
CMU_IntEnable#
void CMU_IntEnable (uint32_t flags)
Enable one or more CMU interrupts.
[in] | flags | CMU interrupt sources to enable. |
Note
Depending on use case, a pending interrupt may already be set prior to enabling the interrupt. Consider using CMU_IntClear() prior to enabling if the pending interrupt should be ignored.
3532
of file platform/emlib/inc/em_cmu.h
CMU_IntGet#
uint32_t CMU_IntGet (void )
Get pending CMU interrupts.
N/A |
Returns
CMU interrupt sources pending.
3544
of file platform/emlib/inc/em_cmu.h
CMU_IntGetEnabled#
uint32_t CMU_IntGetEnabled (void )
Get enabled and pending CMU interrupt flags.
N/A |
Useful for handling more interrupt sources in the same interrupt handler.
Note
This function does not clear event bits.
Returns
Pending and enabled CMU interrupt sources. The return value is the bitwise AND of
the enabled interrupt sources in CMU_IEN and
the pending interrupt flags CMU_IF
3565
of file platform/emlib/inc/em_cmu.h
CMU_IntSet#
void CMU_IntSet (uint32_t flags)
Set one or more pending CMU interrupts.
[in] | flags | CMU interrupt sources to set to pending. |
3580
of file platform/emlib/inc/em_cmu.h
CMU_Lock#
void CMU_Lock (void )
Lock the CMU to protect some of its registers against unintended modification.
N/A |
See the reference manual for CMU registers that will be locked.
Note
If locking the CMU registers, they must be unlocked prior to using any CMU API functions modifying CMU registers protected by the lock.
3598
of file platform/emlib/inc/em_cmu.h
CMU_Unlock#
void CMU_Unlock (void )
Unlock the CMU so that writing to locked registers again is possible.
N/A |
3607
of file platform/emlib/inc/em_cmu.h
CMU_PrescToLog2#
uint32_t CMU_PrescToLog2 (uint32_t presc)
Convert prescaler divider to a logarithmic value.
[in] | presc | Prescaler value used to set the frequency divider. The divider is equal to ('presc' + 1). If a divider value is passed for 'presc', 'presc' will be equal to (divider - 1). |
It only works for even numbers equal to 2^n.
Returns
Logarithm base 2 (binary) value, i.e. exponent as used by fixed 2^n prescalers.
3629
of file platform/emlib/inc/em_cmu.h
Macro Definition Documentation#
CMU_CLOCK_SELECT_SET#
#define CMU_CLOCK_SELECT_SETValue:
(clock, sel)
Macro to set clock sources in the clock tree.
55
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_1#
#define cmuClkDiv_1Value:
1
Clock divisors.
These values are valid for prescalers. Divide clock by 1.
1820
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_2#
#define cmuClkDiv_2Value:
2
Divide clock by 2.
1821
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_4#
#define cmuClkDiv_4Value:
4
Divide clock by 4.
1822
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_8#
#define cmuClkDiv_8Value:
8
Divide clock by 8.
1823
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_16#
#define cmuClkDiv_16Value:
16
Divide clock by 16.
1824
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_32#
#define cmuClkDiv_32Value:
32
Divide clock by 32.
1825
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_64#
#define cmuClkDiv_64Value:
64
Divide clock by 64.
1826
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_128#
#define cmuClkDiv_128Value:
128
Divide clock by 128.
1827
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_256#
#define cmuClkDiv_256Value:
256
Divide clock by 256.
1828
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_512#
#define cmuClkDiv_512Value:
512
Divide clock by 512.
1829
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_1024#
#define cmuClkDiv_1024Value:
1024
Divide clock by 1024.
1830
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_2048#
#define cmuClkDiv_2048Value:
2048
Divide clock by 2048.
1831
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_4096#
#define cmuClkDiv_4096Value:
4096
Divide clock by 4096.
1832
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_8192#
#define cmuClkDiv_8192Value:
8192
Divide clock by 8192.
1833
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_16384#
#define cmuClkDiv_16384Value:
16384
Divide clock by 16384.
1834
of file platform/emlib/inc/em_cmu.h
cmuClkDiv_32768#
#define cmuClkDiv_32768Value:
32768
Divide clock by 32768.
1835
of file platform/emlib/inc/em_cmu.h
CMU_HFRCO_MIN#
#define CMU_HFRCO_MINValue:
cmuHFRCOFreq_1M0Hz
HFRCO minimum frequency.
1927
of file platform/emlib/inc/em_cmu.h
CMU_HFRCO_MAX#
#define CMU_HFRCO_MAXValue:
cmuHFRCOFreq_38M0Hz
HFRCO maximum frequency.
1942
of file platform/emlib/inc/em_cmu.h
CMU_AUXHFRCO_MIN#
#define CMU_AUXHFRCO_MINValue:
cmuAUXHFRCOFreq_1M0Hz
AUXHFRCO minimum frequency.
1968
of file platform/emlib/inc/em_cmu.h
CMU_AUXHFRCO_MAX#
#define CMU_AUXHFRCO_MAXValue:
cmuAUXHFRCOFreq_38M0Hz
AUXHFRCO maximum frequency.
1977
of file platform/emlib/inc/em_cmu.h
CMU_LFXOINIT_DEFAULT#
#define CMU_LFXOINIT_DEFAULTValue:
Default LFXO initialization values.
3112
of file platform/emlib/inc/em_cmu.h
CMU_LFXOINIT_EXTERNAL_CLOCK#
#define CMU_LFXOINIT_EXTERNAL_CLOCKValue:
Default LFXO initialization for external clock.
3120
of file platform/emlib/inc/em_cmu.h
CMU_HFXOINIT_DEFAULT#
#define CMU_HFXOINIT_DEFAULTValue:
Default HFXO initialization values for Platform 2 devices, which contain a separate HFXOCTRL register.
3229
of file platform/emlib/inc/em_cmu.h
CMU_HFXOINIT_EXTERNAL_CLOCK#
#define CMU_HFXOINIT_EXTERNAL_CLOCKValue:
Init of HFXO with external clock.
3249
of file platform/emlib/inc/em_cmu.h
CMU_DPLL_LFXO_TO_40MHZ#
#define CMU_DPLL_LFXO_TO_40MHZValue:
DPLL initialization values for 39,998,805 Hz using LFXO as reference clock, M=2 and N=3661.
3307
of file platform/emlib/inc/em_cmu.h