RTCC - Real Timer Counter/Calendar#
Real Time Counter and Calendar (RTCC) Peripheral API.
This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.
Modules#
Enumerations#
Operational mode of the counter.
Counter prescaler selection.
Prescaler mode of the RTCC counter.
Capture/Compare channel mode.
Compare match output action mode.
Input edge select.
Capture/Compare channel compare mode.
Day compare mode.
Typedefs#
PRS channel number.
Functions#
Get the RTCC compare register value for a selected channel.
Set the RTCC compare register value for a selected channel.
Get the RTCC input capture register value for a selected channel.
Get the RTCC capture/compare register value for a selected channel.
Set RTCC capture/compare register value for a selected channel.
Get the calendar DATE register content for a selected channel.
Set the calendar DATE register for a selected channel.
Get the calendar TIME register content for a selected channel.
Set the calendar TIME register for a selected channel.
Get the combined CNT/PRECNT register content.
Get the RTCC counter value.
Set the RTCC CNT counter.
Get the DATE register value.
Set the RTCC DATE register.
Enable/disable EM4 wakeup capability.
Enable/disable RTCC counting.
Initialize RTCC.
Configure the selected capture/compare channel of the RTCC.
Clear one or more pending RTCC interrupts.
Disable one or more RTCC interrupts.
Enable one or more RTCC interrupts.
Get pending RTCC interrupt flags.
Get enabled and pending RTCC interrupt flags.
Set one or more pending RTCC interrupts from SW.
Lock RTCC registers.
Get the RTCC pre-counter value.
Set the RTCC pre-counter value.
Restore RTCC to its reset state.
Power down retention RAM.
Clear the STATUS register.
Get the STATUS register value.
Get the TIME register value.
Set the RTCC TIME register.
Unlock RTCC registers.
Macros#
Default RTCC initialization structure.
Default RTCC channel output compare initialization structure.
Default RTCC channel input capture initialization structure.
Number of RTCC capture/compare channels.
Validation of valid RTCC channel for assert statements.
Enumeration Documentation#
RTCC_CntMode_TypeDef#
RTCC_CntMode_TypeDef
Operational mode of the counter.
Enumerator | |
---|---|
rtccCntModeNormal | Normal counter mode. |
rtccCntModeCalendar | Calendar mode. |
70
of file platform/emlib/inc/em_rtcc.h
RTCC_CntPresc_TypeDef#
RTCC_CntPresc_TypeDef
Counter prescaler selection.
Enumerator | |
---|---|
rtccCntPresc_1 | Divide clock by 1. |
rtccCntPresc_2 | Divide clock by 2. |
rtccCntPresc_4 | Divide clock by 4. |
rtccCntPresc_8 | Divide clock by 8. |
rtccCntPresc_16 | Divide clock by 16. |
rtccCntPresc_32 | Divide clock by 32. |
rtccCntPresc_64 | Divide clock by 64. |
rtccCntPresc_128 | Divide clock by 128. |
rtccCntPresc_256 | Divide clock by 256. |
rtccCntPresc_512 | Divide clock by 512. |
rtccCntPresc_1024 | Divide clock by 1024. |
rtccCntPresc_2048 | Divide clock by 2048. |
rtccCntPresc_4096 | Divide clock by 4096. |
rtccCntPresc_8192 | Divide clock by 8192. |
rtccCntPresc_16384 | Divide clock by 16384. |
rtccCntPresc_32768 | Divide clock by 32768. |
82
of file platform/emlib/inc/em_rtcc.h
RTCC_PrescMode_TypeDef#
RTCC_PrescMode_TypeDef
Prescaler mode of the RTCC counter.
Enumerator | |
---|---|
rtccCntTickPresc | CNT register ticks according to prescaler value. |
rtccCntTickCCV0Match | CNT register ticks when PRECNT matches the 15 least significant bits of ch. |
124
of file platform/emlib/inc/em_rtcc.h
RTCC_CapComChMode_TypeDef#
RTCC_CapComChMode_TypeDef
Capture/Compare channel mode.
Enumerator | |
---|---|
rtccCapComChModeOff | Capture/Compare channel turned off. |
rtccCapComChModeCapture | Capture mode. |
rtccCapComChModeCompare | Compare mode. |
145
of file platform/emlib/inc/em_rtcc.h
RTCC_CompMatchOutAction_TypeDef#
RTCC_CompMatchOutAction_TypeDef
Compare match output action mode.
Enumerator | |
---|---|
rtccCompMatchOutActionPulse | Generate a pulse. |
rtccCompMatchOutActionToggle | Toggle output. |
rtccCompMatchOutActionClear | Clear output. |
rtccCompMatchOutActionSet | Set output. |
152
of file platform/emlib/inc/em_rtcc.h
RTCC_InEdgeSel_TypeDef#
RTCC_InEdgeSel_TypeDef
Input edge select.
Enumerator | |
---|---|
rtccInEdgeRising | Rising edges detected. |
rtccInEdgeFalling | Falling edges detected. |
rtccInEdgeBoth | Both edges detected. |
rtccInEdgeNone | No edge detection, signal is left as is. |
181
of file platform/emlib/inc/em_rtcc.h
RTCC_CompBase_TypeDef#
RTCC_CompBase_TypeDef
Capture/Compare channel compare mode.
Enumerator | |
---|---|
rtccCompBaseCnt | CCVx is compared with the CNT register. |
rtccCompBasePreCnt | CCVx is compared with a CNT[16:0] and PRECNT[14:0]. |
189
of file platform/emlib/inc/em_rtcc.h
RTCC_DayCompareMode_TypeDef#
RTCC_DayCompareMode_TypeDef
Day compare mode.
Enumerator | |
---|---|
rtccDayCompareModeMonth | Day of month is selected for Capture/Compare. |
rtccDayCompareModeWeek | Day of week is selected for Capture/Compare. |
199
of file platform/emlib/inc/em_rtcc.h
Typedef Documentation#
RTCC_PRSSel_TypeDef#
typedef uint8_t RTCC_PRSSel_TypeDef
PRS channel number.
This type is used when configuring input capture mode on a RTCC channel.
161
of file platform/emlib/inc/em_rtcc.h
Function Documentation#
RTCC_ChannelCompareValueGet#
uint32_t RTCC_ChannelCompareValueGet (int ch)
Get the RTCC compare register value for a selected channel.
[in] | ch | Channel selector. |
Returns
Compare register value.
401
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelCompareValueSet#
void RTCC_ChannelCompareValueSet (int ch, uint32_t value)
Set the RTCC compare register value for a selected channel.
[in] | ch | Channel selector. |
[in] | value | Compare register value |
421
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelCaptureValueGet#
uint32_t RTCC_ChannelCaptureValueGet (int ch)
Get the RTCC input capture register value for a selected channel.
[in] | ch | Channel selector. |
Returns
Capture register value.
441
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelCCVGet#
uint32_t RTCC_ChannelCCVGet (int ch)
Get the RTCC capture/compare register value for a selected channel.
[in] | ch | Channel selector. |
For parts with separate capture compare value registers, this function returns the compare value.
Returns
Capture/compare register value.
463
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelCCVSet#
void RTCC_ChannelCCVSet (int ch, uint32_t value)
Set RTCC capture/compare register value for a selected channel.
[in] | ch | Channel selector. |
[in] | value | Capture/compare register value |
For parts with separate capture compare value registers, this function sets the compare value.
480
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelDateGet#
uint32_t RTCC_ChannelDateGet (int ch)
Get the calendar DATE register content for a selected channel.
[in] | ch | Channel selector. |
Returns
DATE register value.
496
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelDateSet#
void RTCC_ChannelDateSet (int ch, uint32_t date)
Set the calendar DATE register for a selected channel.
[in] | ch | Channel selector. |
[in] | date | DATE value. |
512
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelTimeGet#
uint32_t RTCC_ChannelTimeGet (int ch)
Get the calendar TIME register content for a selected channel.
[in] | ch | Channel selector. |
Returns
TIME register value.
528
of file platform/emlib/inc/em_rtcc.h
RTCC_ChannelTimeSet#
void RTCC_ChannelTimeSet (int ch, uint32_t time)
Set the calendar TIME register for a selected channel.
[in] | ch | Channel selector. |
[in] | time | TIME value. |
544
of file platform/emlib/inc/em_rtcc.h
RTCC_CombinedCounterGet#
uint32_t RTCC_CombinedCounterGet (void )
Get the combined CNT/PRECNT register content.
N/A |
Returns
CNT/PRECNT register value.
558
of file platform/emlib/inc/em_rtcc.h
RTCC_CounterGet#
uint32_t RTCC_CounterGet (void )
Get the RTCC counter value.
N/A |
Returns
Current RTCC counter value.
575
of file platform/emlib/inc/em_rtcc.h
RTCC_CounterSet#
void RTCC_CounterSet (uint32_t value)
Set the RTCC CNT counter.
[in] | value | CNT value. |
592
of file platform/emlib/inc/em_rtcc.h
RTCC_DateGet#
uint32_t RTCC_DateGet (void )
Get the DATE register value.
N/A |
Returns
Current DATE register value.
611
of file platform/emlib/inc/em_rtcc.h
RTCC_DateSet#
void RTCC_DateSet (uint32_t date)
Set the RTCC DATE register.
[in] | date | DATE value. |
623
of file platform/emlib/inc/em_rtcc.h
RTCC_EM4WakeupEnable#
void RTCC_EM4WakeupEnable (bool enable)
Enable/disable EM4 wakeup capability.
[in] | enable | Set to true to enable EM4 wakeup, set to false otherwise. |
637
of file platform/emlib/inc/em_rtcc.h
RTCC_Enable#
void RTCC_Enable (bool enable)
Enable/disable RTCC counting.
[in] | enable | True to enable RTCC counting, false to disable counting. |
112
of file platform/emlib/src/em_rtcc.c
RTCC_Init#
void RTCC_Init (const RTCC_Init_TypeDef * init)
Initialize RTCC.
[in] | init | A pointer to the RTCC initialization structure. |
Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.
152
of file platform/emlib/src/em_rtcc.c
RTCC_ChannelInit#
void RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const * confPtr)
Configure the selected capture/compare channel of the RTCC.
[in] | ch | A channel selector. |
[in] | confPtr | A pointer to the configuration structure. |
Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.
74
of file platform/emlib/src/em_rtcc.c
RTCC_IntClear#
void RTCC_IntClear (uint32_t flags)
Clear one or more pending RTCC interrupts.
[in] | flags | RTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources. |
661
of file platform/emlib/inc/em_rtcc.h
RTCC_IntDisable#
void RTCC_IntDisable (uint32_t flags)
Disable one or more RTCC interrupts.
[in] | flags | RTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt. |
678
of file platform/emlib/inc/em_rtcc.h
RTCC_IntEnable#
void RTCC_IntEnable (uint32_t flags)
Enable one or more RTCC interrupts.
[in] | flags | RTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt. |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.
700
of file platform/emlib/inc/em_rtcc.h
RTCC_IntGet#
uint32_t RTCC_IntGet (void )
Get pending RTCC interrupt flags.
N/A |
Note
Event bits are not cleared by using this function.
Returns
Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
720
of file platform/emlib/inc/em_rtcc.h
RTCC_IntGetEnabled#
uint32_t RTCC_IntGetEnabled (void )
Get enabled and pending RTCC interrupt flags.
N/A |
Useful for handling more interrupt sources in the same interrupt handler.
Returns
Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.
736
of file platform/emlib/inc/em_rtcc.h
RTCC_IntSet#
void RTCC_IntSet (uint32_t flags)
Set one or more pending RTCC interrupts from SW.
[in] | flags | RTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn). |
754
of file platform/emlib/inc/em_rtcc.h
RTCC_Lock#
void RTCC_Lock (void )
Lock RTCC registers.
N/A |
Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
772
of file platform/emlib/inc/em_rtcc.h
RTCC_PreCounterGet#
uint32_t RTCC_PreCounterGet (void )
Get the RTCC pre-counter value.
N/A |
Returns
Current RTCC pre-counter value.
801
of file platform/emlib/inc/em_rtcc.h
RTCC_PreCounterSet#
void RTCC_PreCounterSet (uint32_t preCntVal)
Set the RTCC pre-counter value.
[in] | preCntVal | RTCC pre-counter value to be set. |
818
of file platform/emlib/inc/em_rtcc.h
RTCC_Reset#
void RTCC_Reset (void )
Restore RTCC to its reset state.
N/A |
187
of file platform/emlib/src/em_rtcc.c
RTCC_RetentionRamPowerDown#
void RTCC_RetentionRamPowerDown (void )
Power down retention RAM.
N/A |
Note
Once retention RAM is powered down, it cannot be powered up again.
839
of file platform/emlib/inc/em_rtcc.h
RTCC_StatusClear#
void RTCC_StatusClear (void )
Clear the STATUS register.
N/A |
238
of file platform/emlib/src/em_rtcc.c
RTCC_StatusGet#
uint32_t RTCC_StatusGet (void )
Get the STATUS register value.
N/A |
Returns
Current STATUS register value.
858
of file platform/emlib/inc/em_rtcc.h
RTCC_TimeGet#
uint32_t RTCC_TimeGet (void )
Get the TIME register value.
N/A |
Returns
Current TIME register value.
932
of file platform/emlib/inc/em_rtcc.h
RTCC_TimeSet#
void RTCC_TimeSet (uint32_t time)
Set the RTCC TIME register.
[in] | time | TIME value. |
944
of file platform/emlib/inc/em_rtcc.h
RTCC_Unlock#
void RTCC_Unlock (void )
Unlock RTCC registers.
N/A |
Note
When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.
959
of file platform/emlib/inc/em_rtcc.h
Macro Definition Documentation#
RTCC_INIT_DEFAULT#
#define RTCC_INIT_DEFAULTValue:
Default RTCC initialization structure.
315
of file platform/emlib/inc/em_rtcc.h
RTCC_CH_INIT_COMPARE_DEFAULT#
#define RTCC_CH_INIT_COMPARE_DEFAULTValue:
Default RTCC channel output compare initialization structure.
354
of file platform/emlib/inc/em_rtcc.h
RTCC_CH_INIT_CAPTURE_DEFAULT#
#define RTCC_CH_INIT_CAPTURE_DEFAULTValue:
Default RTCC channel input capture initialization structure.
366
of file platform/emlib/inc/em_rtcc.h
RTCC_CC_NUM#
#define RTCC_CC_NUMValue:
3UL
Number of RTCC capture/compare channels.
381
of file platform/emlib/inc/em_rtcc.h
RTCC_CH_VALID#
#define RTCC_CH_VALIDValue:
(ch)
Validation of valid RTCC channel for assert statements.
385
of file platform/emlib/inc/em_rtcc.h