Sleep Timer#
Sleep Timer can be used for creating timers which are tightly integrated with power management. The Power Manager requires precision timing to have all clocks ready on time, so that wakeup happens a little bit earlier to prepare the system to be ready at the right time. Sleep Timer uses one Hardware Timer and creates multiple software timer instances. It is important to note that when sleeptimer is used with WTIMER/TIMER, the MCU cannot go to EM2 energy mode because WTIMER/TIMER uses a high frequency clock source which is not retained in low energy mode.
The sleeptimer.c and sleeptimer.h source files for the SLEEPTIMER device driver library are in the service/sleeptimer folder.
Introduction#
The Sleeptimer driver provides software timers, delays, timekeeping and date functionalities using a low-frequency real-time clock peripheral.
All Silicon Labs microcontrollers equipped with the RTC or RTCC peripheral are currently supported. Only one instance of this driver can be initialized by the application.
Functionalities overview#
Software Timers#
This functionality allows the user to create periodic and one shot timers. A user callback can be associated with a timer and is called when the timer expires.
Timer structures must be allocated by the user. The function is called from within an interrupt handler with interrupts enabled.
Timekeeping#
A 64-bits tick counter is accessible through the
uint64_t sl_sleeptimer_get_tick_count64(void) API. It keeps the tick count since the initialization of the driver
The SL_SLEEPTIMER_WALLCLOCK_CONFIG configuration enables a UNIX timestamp (seconds count since January 1, 1970, 00:00:00).
This timestamp can be retrieved/modified using the following API:
sl_sleeptimer_timestamp_t sl_sleeptimer_get_time(void);
sl_status_t sl_sleeptimer_set_time(sl_sleeptimer_timestamp_t time);
Convenience conversion functions are provided to convert UNIX timestamp to/from NTP and Zigbee cluster format :
sl_status_t sl_sleeptimer_convert_unix_time_to_ntp(sl_sleeptimer_timestamp_t time, uint32_t *ntp_time);
sl_status_t sl_sleeptimer_convert_ntp_time_to_unix(uint32_t ntp_time, sl_sleeptimer_timestamp_t *time);
sl_status_t sl_sleeptimer_convert_unix_time_to_zigbee(sl_sleeptimer_timestamp_t time, uint32_t *zigbee_time);
sl_status_t sl_sleeptimer_convert_zigbee_time_to_unix(uint32_t zigbee_time, sl_sleeptimer_timestamp_t *time);
Date#
The previously described internal timestamp can also be retrieved/modified in a date format sl_sleeptimer_date_t.
API :
sl_status_t sl_sleeptimer_get_datetime(sl_sleeptimer_date_t *date);
sl_status_t sl_sleeptimer_set_datetime(sl_sleeptimer_date_t *date);
Frequency Setup and Tick Count#
This driver works with a configurable time unit called tick.
The frequency of the ticks is based on the clock source and the internal frequency divider.
WTIMER/TIMER peripherals uses high frequency oscillator. To have a reasonable tick frequency, divider is set to maximum value (1024).
One of the following clock sources must be enabled before initializing the sleeptimer:
LFXO: external crystal oscillator. Typically running at 32.768 kHz.
LFRCO: internal oscillator running at 32.768 kHz
ULFRCO: Ultra low-frequency oscillator running at 1.000 kHz
HFXO: High Frequency Crystal Oscillator at 39 Mhz. HFXO is only needed when Sleeptimer runs on TIMER or WTIMER.
The frequency divider is selected with the SL_SLEEPTIMER_FREQ_DIVIDER configuration. Its value must be a power of two within the range of 1 to 32. The number of ticks per second (sleeptimer frequency) is dictated by the following formula:
Tick (seconds) = 1 / (clock_frequency / frequency_divider)
The highest resolution for a tick is 30.5 us. It is achieved with a 32.768 kHz clock and a divider of 1.
Getting Started#
Clock Selection#
The sleeptimer relies on the hardware timer to operate. The hardware timer peripheral must be properly clocked from the application. Selecting the appropriate timer is crucial for design considerations. Each timer can potentially be used as a sleeptimer and is also available to the user. However, note that if a timer is used by the sleeptimer, it can't be used by the application and vice versa.
For WTIMER/TIMER peripherals, the user must select the appropriate oscillator if it is not the default wanted clock source.
When WTIMER/TIMER is selected, sleeptimer uses channel 0 and it is not possible to use other channels of the same instance for other purposes.
Selection in a Project without Micrium OS#
When RTC, RTCC, or BURTC is selected, the clock source for the peripheral must be configured and enabled in the application before initializing the sleeptimer module or any communication stacks. Most of the time, it consists in enabling the desired oscillators and setting up the clock source for the peripheral, like in the following example:
CMU_ClockSelectSet(cmuClock_LFE, cmuSelect_LFRCO);
CMU_ClockEnable(cmuClock_RTCC, true);
Clock Branch Select#
Clock | Enum | Description | Frequency |
|---|---|---|---|
LFXO | cmuSelect_LFXO | Low-frequency crystal oscillator | 32.768 Khz |
LFRCO | cmuSelect_LFRCO | Low-frequency RC oscillator | 32.768 Khz |
ULFRCO | cmuSelect_ULFRCO | Ultra low-frequency RC oscillator | 1 Khz |
Timer Clock Enable#
Module | Enum | Description |
|---|---|---|
RTCC | cmuClock_RTCC | Real-time counter and calendar clock (LF E branch) |
RTC | cmuClock_RTC | Real time counter clock (LF A branch) |
BURTC | cmuClock_BURTC | BURTC clock (EM4 Group A branch) |
When the Radio internal RTC (PRORTC) is selected, it is not necessary to configure the clock source for the peripheral. However, it is important to enable the desired oscillator before initializing the sleeptimer module or any communication stacks. The best oscillator available (LFXO being the first choice) will be used by the sleeptimer at initalization. The following example shows how the desired oscilator should be enabled:
CMU_OscillatorEnable(cmuSelect_LFXO, true, true);
Clock Selection in a Project with Micrium OS#
When Micrium OS is used, a BSP (all instances) is provided that sets up some parts of the clock tree. The sleeptimer clock source will be enabled by this bsp. However, the desired oscillator remains configurable from the file bsp_cfg.h.
The configuration BSP_LF_CLK_SEL determines which oscillator will be used by the sleeptimer's hardware timer peripheral. It can take the following values:
Config | Description | Frequency |
|---|---|---|
BSP_LF_CLK_LFXO | Low-frequency crystal oscillator | 32.768 Khz |
BSP_LF_CLK_LFRCO | Low-frequency RC oscillator | 32.768 Khz |
BSP_LF_CLK_ULFRCO | Ultra low-frequency RC oscillator | 1 Khz |
Configuration Options#
SL_SLEEPTIMER_PERIPHERAL can be set to one of the following values:
Config | Description |
|---|---|
| Selects either RTC or RTCC, depending of what is available on the platform. |
| Selects RTCC |
| Selects RTC |
| Selects Internal radio RTC. Available only on EFR32XG13, EFR32XG14, EFR32XG21 and EFR32XG22 families. |
| Selects BURTC. Not available on Series 0 devices. |
SL_SLEEPTIMER_WALLCLOCK_CONFIG must be set to 1 to enable timestamp and date functionnalities.
SL_SLEEPTIMER_FREQ_DIVIDER must be a power of 2 within the range 1 to 32. When SL_SLEEPTIMER_PERIPHERAL is set to SL_SLEEPTIMER_PERIPHERAL_PRORTC, SL_SLEEPTIMER_FREQ_DIVIDER must be set to 1.
SL_SLEEPTIMER_PRORTC_HAL_OWNS_IRQ_HANDLER is only meaningful when SL_SLEEPTIMER_PERIPHERAL is set to SL_SLEEPTIMER_PERIPHERAL_PRORTC. Set to 1 if no communication stack is used in your project. Otherwise, must be set to 0.
The API#
This section contains brief descriptions of the API functions. For more information about input and output parameters and return values, click on the hyperlinked function names. Most functions return an error code, SL_STATUS_OK is returned on success, see sl_status.h for other error codes.
The application code must include the sl_sleeptimer.h header file.
All API functions can be called from within interrupt handlers.
sl_sleeptimer_init() These functions initialize the sleeptimer driver. Typically, sl_sleeptimer_init() is called once in the startup code.
sl_sleeptimer_start_timer() Start a one shot 32 bits timer. When a timer expires, a user-supplied callback function is called. A pointer to this function is passed to sl_sleeptimer_start_timer(). See callback for details of the callback prototype.
sl_sleeptimer_restart_timer() Restart a one shot 32 bits timer. When a timer expires, a user-supplied callback function is called. A pointer to this function is passed to sl_sleeptimer_start_timer(). See callback for details of the callback prototype.
sl_sleeptimer_start_periodic_timer() Start a periodic 32 bits timer. When a timer expires, a user-supplied callback function is called. A pointer to this function is passed to sl_sleeptimer_start_timer(). See callback for details of the callback prototype.
sl_sleeptimer_restart_periodic_timer() Restart a periodic 32 bits timer. When a timer expires, a user-supplied callback function is called. A pointer to this function is passed to sl_sleeptimer_start_timer(). See callback for details of the callback prototype.
sl_sleeptimer_stop_timer() Stop a timer.
sl_sleeptimer_get_timer_time_remaining() Get the time remaining before the timer expires.
sl_sleeptimer_delay_millisecond() Delay for the given number of milliseconds. This is an "active wait" delay function.
sl_sleeptimer_is_timer_running() Check if a timer is running.
sl_sleeptimer_get_time(), sl_sleeptimer_set_time() Get or set wallclock time.
sl_sleeptimer_ms_to_tick(), sl_sleeptimer_ms32_to_tick(), sl_sleeptimer_tick_to_ms(), sl_sleeptimer_tick64_to_ms() Convert between milliseconds and RTC/RTCC counter ticks.
The timer expiry callback function: The callback function, prototyped as sl_sleeptimer_timer_callback_t(), is called from within the RTC peripheral interrupt handler on timer expiration. sl_sleeptimer_timer_callback_t(sl_sleeptimer_timer_handle_t *handle, void *data)
Example#
#include "sl_sleeptimer.h"
void my_timer_callback(sl_sleeptimer_timer_handle_t *handle, void *data)
{
//Code executed when the timer expire.
}
int start_timer(void)
{
sl_status_t status;
sl_sleeptimer_timer_handle_t my_timer;
uint32_t timer_timeout = 300;
// We assume the sleeptimer is initialized properly
status = sl_sleeptimer_start_timer(&my_timer,
timer_timeout,
my_timer_callback,
(void *)NULL,
0,
0);
if(status != SL_STATUS_OK) {
return -1;
}
return 1;
}
Modules#
Typedefs#
Timestamp, wall clock time in seconds.
Time zone offset from UTC(second).
Typedef for the user supplied callback function which is called when a timer expires.
Functions#
Month enum.
Week Day enum.
Initializes the Sleeptimer.
Starts a 32 bits timer.
Restarts a 32 bits timer.
Starts a 32 bits periodic timer.
Restarts a 32 bits periodic timer.
Stops a timer.
Gets the status of a timer.
Gets remaining time until timer expires.
Gets the time remaining until the first timer with the matching set of flags expires.
Gets current 32 bits global tick count.
Gets current 64 bits global tick count.
Get timer frequency.
Converts a Unix timestamp into a date.
Converts a 64 bit Unix timestamp into a date.
Converts a date into a Unix timestamp.
Converts a date into a 64 bit timestamp.
Convert date to string.
Sets time zone offset.
Gets time zone offset.
Retrieves current 32 bit time.
Retrieves current 64 bit time.
Sets current time.
Sets current time.
Gets current date.
Sets current time, in date format.
Builds a date time structure based on the provided parameters, where the maximum supported date is 10:14:07 PM 01/18/2038.
Builds a date time structure based on the provided parameters, where the maximum supported date is 11:59:59 PM 12/31/11899.
Converts Unix timestamp into NTP timestamp.
Converts NTP timestamp into Unix timestamp.
Converts Unix timestamp into Zigbee timestamp.
Converts Zigbee timestamp into Unix timestamp.
Calculates offset for time zone after UTC-0.
Calculates offset for time zone before UTC-0.
Active delay.
Converts milliseconds in ticks.
Converts 32-bits milliseconds in ticks.
Gets the maximum value that can be passed to the functions that have a 32-bits time or timeout argument expressed in milliseconds.
Converts ticks in milliseconds.
Converts 64-bit ticks in milliseconds.
Allow sleep after ISR exit.
Starts a 32 bits timer.
Restarts a 32 bits timer.
Starts a 32 bits periodic timer.
Restarts a 32 bits periodic timer.
Gets the precision (in PPM) of the sleeptimer's clock.
Typedef Documentation#
sl_sleeptimer_timestamp_t#
typedef uint32_t sl_sleeptimer_timestamp_t
Timestamp, wall clock time in seconds.
sl_sleeptimer_time_zone_offset_t#
typedef int32_t sl_sleeptimer_time_zone_offset_t
Time zone offset from UTC(second).
sl_sleeptimer_timer_callback_t#
typedef void(* sl_sleeptimer_timer_callback_t) (sl_sleeptimer_timer_handle_t *handle, void *data) )(sl_sleeptimer_timer_handle_t *handle, void *data)
Typedef for the user supplied callback function which is called when a timer expires.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| N/A | handle | The timer handle. | |
| N/A | data | An extra parameter for the user application. |
Function Documentation#
SLEEPTIMER_ENUM#
SLEEPTIMER_ENUM (sl_sleeptimer_month_t )
Month enum.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_month_t | N/A |
SLEEPTIMER_ENUM#
SLEEPTIMER_ENUM (sl_sleeptimer_weekDay_t )
Week Day enum.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_weekDay_t | N/A |
sl_sleeptimer_init#
sl_status_t sl_sleeptimer_init (void )
Initializes the Sleeptimer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_start_timer#
sl_status_t sl_sleeptimer_start_timer (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Starts a 32 bits timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout | Timer timeout, in timer ticks. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_restart_timer#
sl_status_t sl_sleeptimer_restart_timer (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Restarts a 32 bits timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout | Timer timeout, in timer ticks. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_start_periodic_timer#
sl_status_t sl_sleeptimer_start_periodic_timer (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Starts a 32 bits periodic timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout | Timer periodic timeout, in timer ticks. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_restart_periodic_timer#
sl_status_t sl_sleeptimer_restart_periodic_timer (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Restarts a 32 bits periodic timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout | Timer periodic timeout, in timer ticks. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_stop_timer#
sl_status_t sl_sleeptimer_stop_timer (sl_sleeptimer_timer_handle_t * handle)
Stops a timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
Returns
sl_sleeptimer_is_timer_running#
sl_status_t sl_sleeptimer_is_timer_running (sl_sleeptimer_timer_handle_t * handle, bool * running)
Gets the status of a timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| bool * | N/A | running | Pointer to the status of the timer. |
Note
A non periodic timer is considered not running during its callback.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_get_timer_time_remaining#
sl_status_t sl_sleeptimer_get_timer_time_remaining (sl_sleeptimer_timer_handle_t * handle, uint32_t * time)
Gets remaining time until timer expires.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t * | N/A | time | Time left in timer ticks. |
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_get_remaining_time_of_first_timer#
sl_status_t sl_sleeptimer_get_remaining_time_of_first_timer (uint16_t option_flags, uint32_t * time_remaining)
Gets the time remaining until the first timer with the matching set of flags expires.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | option_flags | Set of flags to match. |
| uint32_t * | N/A | time_remaining | Time left in timer ticks. |
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_get_tick_count#
uint32_t sl_sleeptimer_get_tick_count (void )
Gets current 32 bits global tick count.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current tick count.
sl_sleeptimer_get_tick_count64#
uint64_t sl_sleeptimer_get_tick_count64 (void )
Gets current 64 bits global tick count.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Current tick count.
sl_sleeptimer_get_timer_frequency#
uint32_t sl_sleeptimer_get_timer_frequency (void )
Get timer frequency.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_time_to_date#
sl_status_t sl_sleeptimer_convert_time_to_date (sl_sleeptimer_timestamp_t time, sl_sleeptimer_time_zone_offset_t time_zone, sl_sleeptimer_date_t * date)
Converts a Unix timestamp into a date.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_t | N/A | time | 32 bit Unix timestamp to convert. |
| sl_sleeptimer_time_zone_offset_t | N/A | time_zone | Offset from UTC in second. |
| sl_sleeptimer_date_t * | N/A | date | Pointer to converted date. |
Note
Time is in Standard Time.
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_time_to_date_64#
sl_status_t sl_sleeptimer_convert_time_to_date_64 (sl_sleeptimer_timestamp_64_t time, sl_sleeptimer_time_zone_offset_t time_zone, sl_sleeptimer_date_t * date)
Converts a 64 bit Unix timestamp into a date.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_64_t | N/A | time | 64 bit Unix timestamp to convert. |
| sl_sleeptimer_time_zone_offset_t | N/A | time_zone | Offset from UTC in second. |
| sl_sleeptimer_date_t * | N/A | date | Pointer to converted date. |
Note
Time is in Standard Time.
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_date_to_time#
sl_status_t sl_sleeptimer_convert_date_to_time (sl_sleeptimer_date_t * date, sl_sleeptimer_timestamp_t * time)
Converts a date into a Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to date to convert. |
| sl_sleeptimer_timestamp_t * | N/A | time | Pointer to converted 32 bit Unix timestamp. |
Returns
0 if successful. Error code otherwise.
Note
Dates are based on the Unix time representation. Range of dates supported :
January 1, 1970, 00:00:00 to January 19, 2038, 03:14:00
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
sl_sleeptimer_convert_date_to_time_64#
sl_status_t sl_sleeptimer_convert_date_to_time_64 (sl_sleeptimer_date_t * date, sl_sleeptimer_timestamp_64_t * time)
Converts a date into a 64 bit timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to date to convert. |
| sl_sleeptimer_timestamp_64_t * | N/A | time | Pointer to converted 64 bit Unix timestamp. |
Returns
0 if successful. Error code otherwise.
Note
Dates are based on the 64 bit Unix time representation. Range of dates supported :
January 1, 1900, 00:00:00 to December 31, 11899 23:59:59.
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
sl_sleeptimer_convert_date_to_str#
uint32_t sl_sleeptimer_convert_date_to_str (char * str, size_t size, const uint8_t * format, sl_sleeptimer_date_t * date)
Convert date to string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| char * | N/A | str | Output string. |
| size_t | N/A | size | Size of the input array. |
| const uint8_t * | N/A | format | The format specification character. |
| sl_sleeptimer_date_t * | N/A | date | Pointer to date structure. |
Returns
0 if error. Number of character in the output string.
Note
Refer strftime() from UNIX. http://man7.org/linux/man-pages/man3/strftime.3.html
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
sl_sleeptimer_set_tz#
void sl_sleeptimer_set_tz (sl_sleeptimer_time_zone_offset_t offset)
Sets time zone offset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_time_zone_offset_t | N/A | offset | Time zone offset, in seconds. |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
sl_sleeptimer_get_tz#
sl_sleeptimer_time_zone_offset_t sl_sleeptimer_get_tz (void )
Gets time zone offset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Time zone offset, in seconds.
sl_sleeptimer_get_time#
sl_sleeptimer_timestamp_t sl_sleeptimer_get_time (void )
Retrieves current 32 bit time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
Current timestamps in Unix format.
sl_sleeptimer_get_time_64#
sl_sleeptimer_timestamp_64_t sl_sleeptimer_get_time_64 (void )
Retrieves current 64 bit time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
Current timestamps in Unix format.
sl_sleeptimer_set_time#
sl_status_t sl_sleeptimer_set_time (sl_sleeptimer_timestamp_t time)
Sets current time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_t | N/A | time | bit time to set. |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_set_time_64#
sl_status_t sl_sleeptimer_set_time_64 (sl_sleeptimer_timestamp_64_t time)
Sets current time.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_64_t | N/A | time | bit time to set. |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_get_datetime#
sl_status_t sl_sleeptimer_get_datetime (sl_sleeptimer_date_t * date)
Gets current date.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to a sl_sleeptimer_date_t structure. |
Note
Time is in Standard Time.
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_set_datetime#
sl_status_t sl_sleeptimer_set_datetime (sl_sleeptimer_date_t * date)
Sets current time, in date format.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to current date. |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_build_datetime#
sl_status_t sl_sleeptimer_build_datetime (sl_sleeptimer_date_t * date, uint16_t year, sl_sleeptimer_month_t month, uint8_t month_day, uint8_t hour, uint8_t min, uint8_t sec, sl_sleeptimer_time_zone_offset_t tzOffset)
Builds a date time structure based on the provided parameters, where the maximum supported date is 10:14:07 PM 01/18/2038.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to the structure to be populated. |
| uint16_t | N/A | year | Current year. May be provided based on a 0 Epoch or a 1900 Epoch. |
| sl_sleeptimer_month_t | N/A | month | Months since January. Expected value: 0-11. |
| uint8_t | N/A | month_day | Day of the month. Expected value: 1-31. |
| uint8_t | N/A | hour | Hours since midnight. Expected value: 0-23. |
| uint8_t | N/A | min | Minutes after the hour. Expected value: 0-59. |
| uint8_t | N/A | sec | Seconds after the minute. Expected value: 0-59. |
| sl_sleeptimer_time_zone_offset_t | N/A | tzOffset | Offset, in seconds, from UTC. |
Note
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_build_datetime_64#
sl_status_t sl_sleeptimer_build_datetime_64 (sl_sleeptimer_date_t * date, uint16_t year, sl_sleeptimer_month_t month, uint8_t month_day, uint8_t hour, uint8_t min, uint8_t sec, sl_sleeptimer_time_zone_offset_t tzOffset)
Builds a date time structure based on the provided parameters, where the maximum supported date is 11:59:59 PM 12/31/11899.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_date_t * | N/A | date | Pointer to the structure to be populated. |
| uint16_t | N/A | year | Current year based on 0 Epoch. |
| sl_sleeptimer_month_t | N/A | month | Months since January. Expected value: 0-11. |
| uint8_t | N/A | month_day | Day of the month. Expected value: 1-31. |
| uint8_t | N/A | hour | Hours since midnight. Expected value: 0-23. |
| uint8_t | N/A | min | Minutes after the hour. Expected value: 0-59. |
| uint8_t | N/A | sec | Seconds after the minute. Expected value: 0-59. |
| sl_sleeptimer_time_zone_offset_t | N/A | tzOffset | Offset, in seconds, from UTC. |
Note
Resulting date structure's year will be based on 1900 epoch
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_unix_time_to_ntp#
sl_status_t sl_sleeptimer_convert_unix_time_to_ntp (sl_sleeptimer_timestamp_t time, uint32_t * ntp_time)
Converts Unix timestamp into NTP timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_t | N/A | time | Unix timestamp. |
| uint32_t * | N/A | ntp_time | Pointer to NTP Timestamp. |
Note
Unix timestamp range supported : 0x0 to 0x7C55 817F ie. January 1, 1970, 00:00:00 to February 07, 2036, 06:28:15
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_ntp_time_to_unix#
sl_status_t sl_sleeptimer_convert_ntp_time_to_unix (uint32_t ntp_time, sl_sleeptimer_timestamp_t * time)
Converts NTP timestamp into Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | ntp_time | NTP Timestamp. |
| sl_sleeptimer_timestamp_t * | N/A | time | Pointer to Unix timestamp. |
Note
NTP timestamp range supported : 0x83AA 7E80 to 0xFFFF FFFF ie. January 1, 1970, 00:00:00 to February 07, 2036, 06:28:15
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_unix_time_to_zigbee#
sl_status_t sl_sleeptimer_convert_unix_time_to_zigbee (sl_sleeptimer_timestamp_t time, uint32_t * zigbee_time)
Converts Unix timestamp into Zigbee timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timestamp_t | N/A | time | Unix timestamp. |
| uint32_t * | N/A | zigbee_time | Pointer to NTP Timestamp. |
Note
Unix timestamp range supported : 0x386D 4380 to 0x7FFF FFFF ie. January 1, 2000, 00:00:0 to January 19, 2038, 03:14:00
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_convert_zigbee_time_to_unix#
sl_status_t sl_sleeptimer_convert_zigbee_time_to_unix (uint32_t zigbee_time, sl_sleeptimer_timestamp_t * time)
Converts Zigbee timestamp into Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | zigbee_time | NTP Timestamp. |
| sl_sleeptimer_timestamp_t * | N/A | time | Pointer to Unix timestamp. |
Note
ZIGBEE timestamp range supported : 0x0 to 0x4792 BC7F ie. January 1, 2000, 00:00:00 to January 19, 2038, 03:14:00
Function definition is accessible only when SL_SLEEPTIMER_WALLCLOCK_CONFIG is set to 1.
Returns
0 if successful. Error code otherwise.
sl_sleeptimer_set_tz_ahead_utc#
sl_sleeptimer_time_zone_offset_t sl_sleeptimer_set_tz_ahead_utc (uint8_t hours, uint8_t minutes)
Calculates offset for time zone after UTC-0.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | hours | Number of hours from UTC-0. |
| uint8_t | N/A | minutes | Number of minutes from UTC-0. |
Returns
The time zone offset in seconds.
sl_sleeptimer_set_tz_behind_utc#
sl_sleeptimer_time_zone_offset_t sl_sleeptimer_set_tz_behind_utc (uint8_t hours, uint8_t minutes)
Calculates offset for time zone before UTC-0.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | hours | Number of hours to UTC-0. |
| uint8_t | N/A | minutes | Number of minutes to UTC-0. |
Returns
The time zone offset in seconds.
sl_sleeptimer_delay_millisecond#
void sl_sleeptimer_delay_millisecond (uint16_t time_ms)
Active delay.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | time_ms | Delay duration in milliseconds. |
sl_sleeptimer_ms_to_tick#
uint32_t sl_sleeptimer_ms_to_tick (uint16_t time_ms)
Converts milliseconds in ticks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | N/A | time_ms | Number of milliseconds. |
Returns
Corresponding ticks number.
Note
The result is "rounded" to the superior tick number. This function is light and cannot fail so it should be privilegied to perform a millisecond to tick conversion.
sl_sleeptimer_ms32_to_tick#
sl_status_t sl_sleeptimer_ms32_to_tick (uint32_t time_ms, uint32_t * tick)
Converts 32-bits milliseconds in ticks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | time_ms | Number of milliseconds. |
| uint32_t * | N/A | tick | Pointer to the converted tick number. |
Returns
0 if successful. Error code otherwise.
Note
The result is "rounded" to the superior tick number. If possible the sl_sleeptimer_ms_to_tick() function should be used.
This function converts the delay expressed in milliseconds to timer ticks (represented on 32 bits). This means that the value that can be passed to the argument 'time_ms' is limited. The maximum timeout value that can be passed to this function can be retrieved by calling sl_sleeptimer_get_max_ms32_conversion(). If the value passed to 'time_ms' is too large, SL_STATUS_INVALID_PARAMETER will be returned.
sl_sleeptimer_get_max_ms32_conversion#
uint32_t sl_sleeptimer_get_max_ms32_conversion (void )
Gets the maximum value that can be passed to the functions that have a 32-bits time or timeout argument expressed in milliseconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Maximum time or timeout value in milliseconds.
sl_sleeptimer_tick_to_ms#
uint32_t sl_sleeptimer_tick_to_ms (uint32_t tick)
Converts ticks in milliseconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | N/A | tick | Number of tick. |
Returns
Corresponding milliseconds number.
Note
The result is rounded to the inferior millisecond.
sl_sleeptimer_tick64_to_ms#
sl_status_t sl_sleeptimer_tick64_to_ms (uint64_t tick, uint64_t * ms)
Converts 64-bit ticks in milliseconds.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint64_t | N/A | tick | Number of tick. |
| uint64_t * | N/A | ms | Pointer to the converted milliseconds number. |
Returns
0 if successful. Error code otherwise.
Note
The result is rounded to the inferior millisecond.
sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire#
bool sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire (void )
Allow sleep after ISR exit.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if sleep is allowed after ISR exit. False otherwise.
sl_sleeptimer_start_timer_ms#
sl_status_t sl_sleeptimer_start_timer_ms (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout_ms, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Starts a 32 bits timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout_ms | Timer timeout, in milliseconds. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
Note
This function converts the delay expressed in milliseconds to timer ticks (represented on 32 bits). This means that the value that can be passed to the argument 'timeout_ms' is limited. The maximum timeout value that can be passed to this function can be retrieved by calling sl_sleeptimer_get_max_ms32_conversion(). If the value passed to 'timeout_ms' is too large, SL_STATUS_INVALID_PARAMETER will be returned.
sl_sleeptimer_restart_timer_ms#
sl_status_t sl_sleeptimer_restart_timer_ms (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout_ms, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Restarts a 32 bits timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout_ms | Timer timeout, in milliseconds. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
Note
This function converts the delay expressed in milliseconds to timer ticks (represented on 32 bits). This means that the value that can be passed to the argument 'timeout_ms' is limited. The maximum timeout value that can be passed to this function can be retrieved by calling sl_sleeptimer_get_max_ms32_conversion(). If the value passed to 'timeout_ms' is too large, SL_STATUS_INVALID_PARAMETER will be returned.
sl_sleeptimer_start_periodic_timer_ms#
sl_status_t sl_sleeptimer_start_periodic_timer_ms (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout_ms, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Starts a 32 bits periodic timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout_ms | Timer periodic timeout, in milliseconds. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
Note
This function converts the delay expressed in milliseconds to timer ticks (represented on 32 bits). This means that the value that can be passed to the argument 'timeout_ms' is limited. The maximum timeout value that can be passed to this function can be retrieved by calling sl_sleeptimer_get_max_ms32_conversion(). If the value passed to 'timeout_ms' is too large, SL_STATUS_INVALID_PARAMETER will be returned.
sl_sleeptimer_restart_periodic_timer_ms#
sl_status_t sl_sleeptimer_restart_periodic_timer_ms (sl_sleeptimer_timer_handle_t * handle, uint32_t timeout_ms, sl_sleeptimer_timer_callback_t callback, void * callback_data, uint8_t priority, uint16_t option_flags)
Restarts a 32 bits periodic timer.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_sleeptimer_timer_handle_t * | N/A | handle | Pointer to handle to timer. |
| uint32_t | N/A | timeout_ms | Timer periodic timeout, in milliseconds. |
| sl_sleeptimer_timer_callback_t | N/A | callback | Callback function that will be called when initial/periodic timeout expires. |
| void * | N/A | callback_data | Pointer to user data that will be passed to callback. |
| uint8_t | N/A | priority | Priority of callback. Useful in case multiple timer expire at the same time. 0 = highest priority. |
| uint16_t | N/A | option_flags | Bit array of option flags for the timer. Valid bit-wise OR of one or more of the following:
|
Returns
0 if successful. Error code otherwise.
Note
This function converts the delay expressed in milliseconds to timer ticks (represented on 32 bits). This means that the value that can be passed to the argument 'timeout_ms' is limited. The maximum timeout value that can be passed to this function can be retrieved by calling sl_sleeptimer_get_max_ms32_conversion(). If the value passed to 'timeout_ms' is too large, SL_STATUS_INVALID_PARAMETER will be returned.
sl_sleeptimer_get_clock_accuracy#
uint16_t sl_sleeptimer_get_clock_accuracy (void )
Gets the precision (in PPM) of the sleeptimer's clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Clock accuracy, in PPM.