Public Attribute Documentation#

mac_address#

uint8_t mac_address[6]

Incoming MAC address in payload


Definition at line 1751 of file include/rsi_wlan_apis.h

reserved#

uint8_t reserved[2]

Definition at line 1752 of file include/rsi_wlan_apis.h

tsf#

uint32_t tsf

Incoming TSF of frame in payload


Definition at line 1754 of file include/rsi_wlan_apis.h

rsi_rsp_csi_record#

rsi_rsp_csi_record_t rsi_rsp_csi_record[CSI_MAX_NUM_RECORDS]

Incoming CSI data in payload. Refer to rsi_rsp_csi_record_s


Definition at line 1757 of file include/rsi_wlan_apis.h