Public Attribute Documentation#

wake_duration#

uint8_t wake_duration

Definition at line 1638 of file include/rsi_wlan_apis.h

wake_duration_tol#

uint8_t wake_duration_tol

Definition at line 1640 of file include/rsi_wlan_apis.h

wake_int_exp#

uint8_t wake_int_exp

Definition at line 1642 of file include/rsi_wlan_apis.h

wake_int_exp_tol#

uint8_t wake_int_exp_tol

Definition at line 1644 of file include/rsi_wlan_apis.h

wake_int_mantissa#

uint16_t wake_int_mantissa

Definition at line 1646 of file include/rsi_wlan_apis.h

wake_int_mantissa_tol#

uint16_t wake_int_mantissa_tol

Definition at line 1648 of file include/rsi_wlan_apis.h

implicit_twt#

uint8_t implicit_twt

Definition at line 1650 of file include/rsi_wlan_apis.h

un_announced_twt#

uint8_t un_announced_twt

Definition at line 1652 of file include/rsi_wlan_apis.h

triggered_twt#

uint8_t triggered_twt

Definition at line 1654 of file include/rsi_wlan_apis.h

wake_duration_unit#

uint8_t wake_duration_unit

Definition at line 1656 of file include/rsi_wlan_apis.h

twt_channel#

uint8_t twt_channel

Definition at line 1658 of file include/rsi_wlan_apis.h

twt_protection#

uint8_t twt_protection

Definition at line 1660 of file include/rsi_wlan_apis.h

restrict_tx_outside_tsp#

uint8_t restrict_tx_outside_tsp

Definition at line 1662 of file include/rsi_wlan_apis.h

twt_retry_limit#

uint8_t twt_retry_limit

Definition at line 1664 of file include/rsi_wlan_apis.h

twt_retry_interval#

uint8_t twt_retry_interval

Definition at line 1666 of file include/rsi_wlan_apis.h

req_type#

uint8_t req_type

Definition at line 1668 of file include/rsi_wlan_apis.h