Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[6]

Device address of the remote device


Definition at line 290 of file include/rsi_ble_apis.h

conn_interval#

uint16_t conn_interval

Connection Interval


Definition at line 292 of file include/rsi_ble_apis.h

conn_latency#

uint16_t conn_latency

Connection Latency


Definition at line 294 of file include/rsi_ble_apis.h

timeout#

uint16_t timeout

Supervision Timeout


Definition at line 296 of file include/rsi_ble_apis.h