Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[6]
Device address of the remote device.
Definition at line
272
of file include/rsi_ble_apis.h
TxPhy#
uint8_t TxPhy
Transmitission phy rate(1 byte)
BIT(0) - The Host prefers to use the LE 1M transmitter PHY (possibly among others)
BIT(1) - The Host prefers to use the LE 2M transmitter PHY (possibly among others)
BIT(2) - The Host prefers to use the LE Coded transmitter PHY (possibly among others)
BIT(3) - BIT(7) Reserved for future use
Definition at line
278
of file include/rsi_ble_apis.h
RxPhy#
uint8_t RxPhy
Reception phy rate(1 byte)
BIT(0) - The Host prefers to use the LE 1M transmitter PHY (possibly among others)
BIT(1) - The Host prefers to use the LE 2M transmitter PHY (possibly among others)
BIT(2) - The Host prefers to use the LE Coded transmitter PHY (possibly among others)
BIT(3) - BIT(7) Reserved for future use
Definition at line
284
of file include/rsi_ble_apis.h