Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
remote device address
Definition at line
683
of file include/rsi_ble_apis.h
pkt_type#
uint8_t pkt_type
Type of the event received from the remote device
RSI_BLE_WRITE_CMD_EVENT 0x01
RSI_BLE_WRITE_REQUEST_EVENT 0x02
RSI_BLE_NOTIFICATION_EVENT 0x03
RSI_BLE_INDICATION_EVENT 0x04
Definition at line
694
of file include/rsi_ble_apis.h
length#
uint8_t length
length of attribute value
Definition at line
698
of file include/rsi_ble_apis.h
att_value#
uint8_t att_value[RSI_DEV_ATT_LEN]
This contains the attribute value. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro
Definition at line
700
of file include/rsi_ble_apis.h