Public Attributes#
Public Attribute Documentation#
cmd_ix#
uint8_t cmd_ix
Command ID Takes per BLE_TRANSMIT_CMD_ID of value 0x13
905
of file include/rsi_ble_apis.h
transmit_enable#
uint8_t transmit_enable
Enables/disables the ble per transmit mode 1 PER Transmit Enable 0 PER Transmit Disable
909
of file include/rsi_ble_apis.h
access_addr#
uint8_t access_addr[4]
Access address with which packets are transmitted
911
of file include/rsi_ble_apis.h
phy_rate#
uint8_t phy_rate
Phy rate at which packets are transmitted 1 1Mbps 2 2 Mbps 4 125 Kbps Coded 8 500 Kbps Coded
917
of file include/rsi_ble_apis.h
rx_chnl_num#
uint8_t rx_chnl_num
Rx channel number (0 - 39)
919
of file include/rsi_ble_apis.h
tx_chnl_num#
uint8_t tx_chnl_num
Tx channel number (0 - 39)
921
of file include/rsi_ble_apis.h
scrambler_seed#
uint8_t scrambler_seed
Initial seed to be used for whitening. It should be set to �0� in order to disable whitening. In order to enable, one should give the scrambler seed value which is used on the receive side
924
of file include/rsi_ble_apis.h
le_chnl_type#
uint8_t le_chnl_type
LE channel type (data or advertise channel) 0x00 Advertise Channel 0x01 Data Channel (to be used by Default)
928
of file include/rsi_ble_apis.h
freq_hop_en#
uint8_t freq_hop_en
Frequency hopping type to be used 0 No Hopping 1 Fixed Hopping 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)
933
of file include/rsi_ble_apis.h
ant_sel#
uint8_t ant_sel
Select the antenna to be used. Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna. 2 ONBOARD_ANT_SEL 3 EXT_ANT_SEL
937
of file include/rsi_ble_apis.h
pll_mode#
uint8_t pll_mode
pll_mode type to be used 0 PLL_MODE0 (to be used by Default) 1 PLL_MODE1
941
of file include/rsi_ble_apis.h
rf_type#
uint8_t rf_type
Selection of RF type (internal/external) BIT[7:6] - RECT selection for BLR (Default value -> 0b00) BIT[5:4] - RECT selection for BLE 2 Mbps (Default value -> 0b00) BIT[3:2] - RECT selection for BLE 1 Mbps (Default value -> 0b00) BIT[1:0] - for rf_type(external - 0/internal - 1) (Default value -> 0b01) Note
The above macros are applicable for BLE
948
of file include/rsi_ble_apis.h
rf_chain#
uint8_t rf_chain
Selection of RF Chain (HP/LP) to be used 2 BT_HP_CHAIN 3 BT_LP_CHAIN Note
The above macros are applicable for both BT and BLE
953
of file include/rsi_ble_apis.h
pkt_len#
uint8_t pkt_len[2]
Length of the packet to be transmitted Max pkt_len to be transmitted is 255
955
of file include/rsi_ble_apis.h
payload_type#
uint8_t payload_type
Type of payload data sequence 0x00 PRBS9 sequence �11111111100000111101... 0x01 Repeated �11110000� 0x02 Repeated �10101010� 0x03 PRBS15 0x04 Repeated �11111111� 0x05 Repeated �00000000� 0x06 Repeated '00001111' 0x07 Repeated '01010101'
965
of file include/rsi_ble_apis.h
tx_power#
uint8_t tx_power
Transmit Power This field corresponds to the transmit power. The range for the Tx Power Index is 1 to 63 (0 and 32 are invalid.) If rf chain is BT_HP_CHAIN 1 - 12 BLE - HP Mode 127 magic number for selecting maximum possible power output If rf chain is BT_LP_CHAIN 1 - 31 BLE - 0 dBm Mode 33 - 63 BLE- 10 dBm Mode
974
of file include/rsi_ble_apis.h
transmit_mode#
uint8_t transmit_mode
Transmit mode to be used either Burst/Continuous 0 BURST_MODE 1 CONTINUOUS_MODE 2 CONTINUOUS_WAVE_MODE (CW_MODE)
979
of file include/rsi_ble_apis.h
inter_pkt_gap#
uint8_t inter_pkt_gap
This field takes the value of inter packet gap. Number of slots to be skipped between two packets - Each slot will be 1250usec
982
of file include/rsi_ble_apis.h
num_pkts#
uint8_t num_pkts[4]
This field defines the number of packets to be transmitted, default to zero for continuous transmission
984
of file include/rsi_ble_apis.h