Public Attributes#

int32_t
rsi_mutex_handle_t
rsi_semaphore_handle_t
uint8_t *

Public Attribute Documentation#

status#

volatile int32_t status

Definition at line 829 of file include/rsi_common.h

crypto_mutex#

rsi_mutex_handle_t crypto_mutex

Definition at line 832 of file include/rsi_common.h

crypto_sem#

rsi_semaphore_handle_t crypto_sem

Definition at line 835 of file include/rsi_common.h

crypto_tx_pool#

rsi_pkt_pool_t crypto_tx_pool

Definition at line 838 of file include/rsi_common.h

crypto_hold_power_save#

uint8_t crypto_hold_power_save

Definition at line 841 of file include/rsi_common.h

crypto_buffer#

uint8_t* crypto_buffer

Definition at line 844 of file include/rsi_common.h

crypto_buffer_length#

uint32_t crypto_buffer_length

Definition at line 847 of file include/rsi_common.h