Public Attribute Documentation#

wake_duration#

uint8_t wake_duration

Definition at line 1637 of file include/rsi_wlan_apis.h

wake_duration_tol#

uint8_t wake_duration_tol

Definition at line 1639 of file include/rsi_wlan_apis.h

wake_int_exp#

uint8_t wake_int_exp

Definition at line 1641 of file include/rsi_wlan_apis.h

wake_int_exp_tol#

uint8_t wake_int_exp_tol

Definition at line 1643 of file include/rsi_wlan_apis.h

wake_int_mantissa#

uint16_t wake_int_mantissa

Definition at line 1645 of file include/rsi_wlan_apis.h

wake_int_mantissa_tol#

uint16_t wake_int_mantissa_tol

Definition at line 1647 of file include/rsi_wlan_apis.h

implicit_twt#

uint8_t implicit_twt

Definition at line 1649 of file include/rsi_wlan_apis.h

un_announced_twt#

uint8_t un_announced_twt

Definition at line 1651 of file include/rsi_wlan_apis.h

triggered_twt#

uint8_t triggered_twt

Definition at line 1653 of file include/rsi_wlan_apis.h

wake_duration_unit#

uint8_t wake_duration_unit

Definition at line 1655 of file include/rsi_wlan_apis.h

twt_channel#

uint8_t twt_channel

Definition at line 1657 of file include/rsi_wlan_apis.h

twt_protection#

uint8_t twt_protection

Definition at line 1659 of file include/rsi_wlan_apis.h

restrict_tx_outside_tsp#

uint8_t restrict_tx_outside_tsp

Definition at line 1661 of file include/rsi_wlan_apis.h

twt_retry_limit#

uint8_t twt_retry_limit

Definition at line 1663 of file include/rsi_wlan_apis.h

twt_retry_interval#

uint8_t twt_retry_interval

Definition at line 1665 of file include/rsi_wlan_apis.h

req_type#

uint8_t req_type

Definition at line 1667 of file include/rsi_wlan_apis.h