Public Attribute Documentation#
wlan_state#
uint16_t wlan_state
Definition at line 1069
of file include/rsi_wlan_apis.h
channel_number#
uint16_t channel_number
Definition at line 1072
of file include/rsi_wlan_apis.h
ssid#
uint8_t ssid[RSI_SSID_LEN]
Definition at line 1075
of file include/rsi_wlan_apis.h
mac_address#
uint8_t mac_address[6]
Definition at line 1078
of file include/rsi_wlan_apis.h
sec_type#
uint8_t sec_type
Definition at line 1081
of file include/rsi_wlan_apis.h
pmk#
uint8_t pmk[64]
Definition at line 1084
of file include/rsi_wlan_apis.h
ipv4_address#
uint8_t ipv4_address[4]
Definition at line 1087
of file include/rsi_wlan_apis.h
ipv6_address#
uint8_t ipv6_address[16]
Definition at line 1090
of file include/rsi_wlan_apis.h
reserved1#
uint8_t reserved1[2]
Definition at line 1093
of file include/rsi_wlan_apis.h
reserved2#
uint8_t reserved2[2]
Definition at line 1096
of file include/rsi_wlan_apis.h