Public Attributes#

Public Attribute Documentation#

dynamic_power_enable#

uint8_t dynamic_power_enable

Definition at line 977 of file include/rsi_bt.h

pwr_index_br#

uint8_t pwr_index_br

Definition at line 978 of file include/rsi_bt.h

pwr_index_2m#

uint8_t pwr_index_2m

Definition at line 979 of file include/rsi_bt.h

pwr_index_3m#

uint8_t pwr_index_3m

Definition at line 980 of file include/rsi_bt.h