RTC time from host

Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

tm_sec#

uint8_t tm_sec[4]

Definition at line 482 of file include/rsi_wlan_non_rom.h

tm_min#

uint8_t tm_min[4]

Definition at line 483 of file include/rsi_wlan_non_rom.h

tm_hour#

uint8_t tm_hour[4]

Definition at line 484 of file include/rsi_wlan_non_rom.h

tm_mday#

uint8_t tm_mday[4]

Definition at line 485 of file include/rsi_wlan_non_rom.h

tm_mon#

uint8_t tm_mon[4]

Definition at line 486 of file include/rsi_wlan_non_rom.h

tm_year#

uint8_t tm_year[4]

Definition at line 487 of file include/rsi_wlan_non_rom.h

tm_wday#

uint8_t tm_wday[4]

Definition at line 488 of file include/rsi_wlan_non_rom.h