Public Attribute Documentation#
tcp_stack_used#
uint8_t tcp_stack_used
Definition at line 1089
of file include/rsi_wlan_apis.h
dhcp_enable#
uint8_t dhcp_enable
Definition at line 1091
of file include/rsi_wlan_apis.h
ip_address#
uint8_t ip_address[4]
Definition at line 1092
of file include/rsi_wlan_apis.h
sn_mask#
uint8_t sn_mask[4]
Definition at line 1093
of file include/rsi_wlan_apis.h
default_gw#
uint8_t default_gw[4]
Definition at line 1094
of file include/rsi_wlan_apis.h
dhcp6_enable#
uint8_t dhcp6_enable
Definition at line 1096
of file include/rsi_wlan_apis.h
prefix_length#
uint8_t prefix_length[2]
Definition at line 1097
of file include/rsi_wlan_apis.h
ip6_address#
uint8_t ip6_address[16]
Definition at line 1098
of file include/rsi_wlan_apis.h
deafault_gw#
uint8_t deafault_gw[16]
Definition at line 1099
of file include/rsi_wlan_apis.h