Public Attribute Documentation#
serv_handler#
void* serv_handler
service handler
Definition at line
438
of file include/rsi_ble_apis.h
config_bitmap#
uint16_t config_bitmap
If this variable is 1, Host has to maintain attributes and records in the application. If 0, Stack will maintain the attributes and records
Definition at line
443
of file include/rsi_ble_apis.h
data_len#
uint16_t data_len
Attribute data length
Definition at line
449
of file include/rsi_ble_apis.h
data#
uint8_t data[RSI_DEV_ATT_LEN]
Attribute data. The maximum value is 240, please refer RSI_DEV_ATT_LEN Macro
Definition at line
451
of file include/rsi_ble_apis.h