Public Attribute Documentation#
dev_addr#
uint8_t dev_addr[RSI_DEV_ADDR_LEN]
remote device address
Definition at line
299
of file include/rsi_bt_apis.h
max_tx_latency#
uint16_t max_tx_latency
Maximum latency for data being transmitted from the local device to the remote device
Definition at line
302
of file include/rsi_bt_apis.h
min_remote_timeout#
uint16_t min_remote_timeout
Base sniff subrate timeout in baseband slots that the remote device use
Definition at line
305
of file include/rsi_bt_apis.h
min_local_timeout#
uint16_t min_local_timeout
Base sniff subrate timeout in baseband slots that the local device use
Definition at line
308
of file include/rsi_bt_apis.h