Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t dev_addr[RSI_DEV_ADDR_LEN]

remote device address


Definition at line 154 of file include/rsi_bt_apis.h

reserved#

uint8_t reserved[2]

Reserved field for future use


Definition at line 157 of file include/rsi_bt_apis.h

confirmation_value#

uint8_t confirmation_value[4]

This is the passkey to be confirmed


Definition at line 160 of file include/rsi_bt_apis.h