Public Attributes#
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
uint16_t
int8_t
uint16_t
uint16_t
Public Attribute Documentation#
crc_fail_cnt#
uint16_t crc_fail_cnt
Packet count of CRC fails (Cyclic Redundancy Check (CRC))
Definition at line
325
of file include/rsi_bt_common.h
crc_pass_cnt#
uint16_t crc_pass_cnt
Packet count of CRC fails (Cyclic Redundancy Check (CRC))
Definition at line
327
of file include/rsi_bt_common.h
tx_abort_cnt#
uint16_t tx_abort_cnt
Packet count of aborted Tx
Definition at line
329
of file include/rsi_bt_common.h
rx_drop_cnt#
uint16_t rx_drop_cnt
Packet count of dropped Rx
Definition at line
331
of file include/rsi_bt_common.h
rx_cca_idle_cnt#
uint16_t rx_cca_idle_cnt
Packet count of CCA Idle (Clear Channel Assessment (CCA))
Definition at line
333
of file include/rsi_bt_common.h
rx_start_idle_cnt#
uint16_t rx_start_idle_cnt
Packet count of Rx start
Definition at line
335
of file include/rsi_bt_common.h
rx_abrt_cnt#
uint16_t rx_abrt_cnt
Packet count of aborted Rx
Definition at line
337
of file include/rsi_bt_common.h
tx_dones#
uint16_t tx_dones
Packet count of successful transmissions
Definition at line
339
of file include/rsi_bt_common.h
rssi#
int8_t rssi
Received Signal Strength Indicator of the packet
Definition at line
341
of file include/rsi_bt_common.h
id_pkts_rcvd#
uint16_t id_pkts_rcvd
Packet count of ID packets received
Definition at line
343
of file include/rsi_bt_common.h
dummy#
uint16_t dummy[5]
Dummy array of length 5
Definition at line
345
of file include/rsi_bt_common.h