Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
union rsi_rsp_socket_recv_s::@10

Public Attribute Documentation#

ip_version#

uint8_t ip_version[2]

Definition at line 1279 of file include/rsi_wlan.h

socket_id#

uint8_t socket_id[2]

Definition at line 1282 of file include/rsi_wlan.h

length#

uint8_t length[4]

Definition at line 1285 of file include/rsi_wlan.h

offset#

uint8_t offset[2]

Definition at line 1288 of file include/rsi_wlan.h

dest_port#

uint8_t dest_port[2]

Definition at line 1291 of file include/rsi_wlan.h

ipv4_address#

uint8_t ipv4_address[4]

Definition at line 1296 of file include/rsi_wlan.h

ipv6_address#

uint8_t ipv6_address[16]

Definition at line 1299 of file include/rsi_wlan.h

dest_ip_addr#

union rsi_rsp_socket_recv_s::@10 dest_ip_addr

Definition at line 1300 of file include/rsi_wlan.h

end_of_the_data#

uint8_t end_of_the_data

Definition at line 1302 of file include/rsi_wlan.h

more_data_pending#

uint8_t more_data_pending

Definition at line 1303 of file include/rsi_wlan.h